Public Attributes#
TaskFunction_t
The function of the task (Invalid parameter if NULL)
char *
The name of the task. (Max characters = configMAX_TASK_NAME_LEN). NULL allowed.
void *
Any parameter variable of own choice that is casted as (void*). Can be NULL.
The desired priority of the task.
The buffer collection for the task.
Public Attribute Documentation#
pTaskFunc#
TaskFunction_t ZW_UserTask_t::pTaskFunc
The function of the task (Invalid parameter if NULL)
Definition at line
49
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_UserTask.h
pTaskName#
char* ZW_UserTask_t::pTaskName
The name of the task. (Max characters = configMAX_TASK_NAME_LEN). NULL allowed.
Definition at line
50
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_UserTask.h
pUserTaskParam#
void* ZW_UserTask_t::pUserTaskParam
Any parameter variable of own choice that is casted as (void*). Can be NULL.
Definition at line
51
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_UserTask.h
priority#
ZW_UserTask_Priority_t ZW_UserTask_t::priority
The desired priority of the task.
Definition at line
52
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_UserTask.h
taskBuffer#
ZW_UserTask_Buffer_t* ZW_UserTask_t::taskBuffer
The buffer collection for the task.
See Also
ZW_UserTask_Buffer_t for more info.
Definition at line
53
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_UserTask.h