Public Attribute Documentation#
sof#
uint8_t tx_beam_start_frame_t::sof
Definition at line
94
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h
type#
uint8_t tx_beam_start_frame_t::type
Definition at line
95
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h
timestamp1#
uint8_t tx_beam_start_frame_t::timestamp1
Definition at line
96
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h
timestamp2#
uint8_t tx_beam_start_frame_t::timestamp2
Definition at line
97
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h
ch_speed#
uint8_t tx_beam_start_frame_t::ch_speed
Definition at line
98
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h
freq_no#
uint8_t tx_beam_start_frame_t::freq_no
Definition at line
99
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h
rssi#
uint8_t tx_beam_start_frame_t::rssi
Definition at line
100
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h
payload#
uint8_t tx_beam_start_frame_t::payload[4]
Definition at line
101
of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h