Node info stored within the non-volatile memory This are the first (protocol part) payload bytes from the Node Infomation frame.
Public Attribute Documentation#
capability#
uint8_t _NODEINFO_::capability
Network capabilities.
Definition at line
58
of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_basis_api.h
security#
uint8_t _NODEINFO_::security
Network security.
Definition at line
59
of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_basis_api.h
reserved#
uint8_t _NODEINFO_::reserved
Definition at line
60
of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_basis_api.h
nodeType#
NODE_TYPE _NODEINFO_::nodeType
Basic, Generic and Specific Device types - Basic is generated...
Definition at line
61
of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_basis_api.h