Structure that holds the attributes of a sensor type.
Public Attributes#
uint8_t
Sensor type id from SDS13812.
uint8_t
Supported bitmask byte number from SDS13812.
uint8_t
Supported bitmask bit number from SDS13812.
uint8_t
Maximum supported scale number from SDS13812.
Public Attribute Documentation#
value#
uint8_t _sensor_type::value
Sensor type id from SDS13812.
Definition at line
67
of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h
byte_offset#
uint8_t _sensor_type::byte_offset
Supported bitmask byte number from SDS13812.
Definition at line
68
of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h
bit_mask#
uint8_t _sensor_type::bit_mask
Supported bitmask bit number from SDS13812.
Definition at line
69
of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h
max_scale_value#
uint8_t _sensor_type::max_scale_value
Maximum supported scale number from SDS13812.
Definition at line
70
of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h