Transmit options for ZW_SendDataEx.
Public Attributes#
Options for enabling specific Security scheme functionality.
uint8_t
Security key to use for sending.
enum SECURITY_KEY
More transmit options.
uint8_t
Public Attribute Documentation#
destNode#
node_id_t _TRANSMIT_OPTIONS_TYPE::destNode
< Destination node ID - 0xFF == all nodes
Reserved
Definition at line
217
of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
bSrcNode#
node_id_t _TRANSMIT_OPTIONS_TYPE::bSrcNode
Transmit options.
Definition at line
219
of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
txOptions#
TxOptions_t _TRANSMIT_OPTIONS_TYPE::txOptions
Options for enabling specific Security scheme functionality.
Definition at line
221
of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
txSecOptions#
uint8_t _TRANSMIT_OPTIONS_TYPE::txSecOptions
Security key to use for sending.
Definition at line
223
of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
securityKey#
enum SECURITY_KEY _TRANSMIT_OPTIONS_TYPE::securityKey
More transmit options.
Definition at line
225
of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
txOptions2#
uint8_t _TRANSMIT_OPTIONS_TYPE::txOptions2
Definition at line
227
of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h