Public Attribute Documentation#

rxOpt#

RECEIVE_OPTIONS_TYPE_EX _cc_notification_t::rxOpt

Definition at line 35 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/src/cc_notification_config_api.h

endpoint#

const uint8_t _cc_notification_t::endpoint

Definition at line 36 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/src/cc_notification_config_api.h

type#

const notification_type_t _cc_notification_t::type

Definition at line 37 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/src/cc_notification_config_api.h

agi_profile#

const agi_profile_t _cc_notification_t::agi_profile

Definition at line 38 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/src/cc_notification_config_api.h

events#

const notification_event_state* _cc_notification_t::events

Definition at line 39 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/src/cc_notification_config_api.h

event_count#

const uint8_t _cc_notification_t::event_count

Definition at line 40 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/src/cc_notification_config_api.h

current_event#

notification_event_state _cc_notification_t::current_event

Definition at line 41 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/src/cc_notification_config_api.h

status#

NOTIFICATION_STATUS _cc_notification_t::status

Current event state.


Definition at line 42 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/src/cc_notification_config_api.h