Structure used by supervision_event_handler() to process upcoming events Registered for CC Supervision.

Public Attributes#

zaf_tx_options_t
uint8_t

TX data to be used to send Supervision Report.

bool

Supervision session Id.

uint8_t

Status Update. True if more reports will follow.

Public Attribute Documentation#

tx_options#

zaf_tx_options_t _cc_supervision_report_event::tx_options

Definition at line 118 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h

session_id#

uint8_t _cc_supervision_report_event::session_id

TX data to be used to send Supervision Report.


Definition at line 119 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h

status_update#

bool _cc_supervision_report_event::status_update

Supervision session Id.


Definition at line 120 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h

duration#

uint8_t _cc_supervision_report_event::duration

Status Update. True if more reports will follow.


Definition at line 121 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h