Structure that holds Color Switch CC related data.
Public Attributes#
saves Rx values, including data about supervision.
Color Component ID.
uint8_t
Endpoint that supports colorId.
Actuator data.
void(*
pointer to app callback function that triggers driver changes
Public Attribute Documentation#
rxOpt#
RECEIVE_OPTIONS_TYPE_EX colorComponent_::rxOpt
saves Rx values, including data about supervision.
(Must be first member - required by TSE)
Definition at line
42
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/ColorSwitch/inc/CC_ColorSwitch.h
colorId#
EColorComponents colorComponent_::colorId
Color Component ID.
Definition at line
44
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/ColorSwitch/inc/CC_ColorSwitch.h
ep#
uint8_t colorComponent_::ep
Endpoint that supports colorId.
Definition at line
45
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/ColorSwitch/inc/CC_ColorSwitch.h
obj#
s_Actuator colorComponent_::obj
Actuator data.
Definition at line
46
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/ColorSwitch/inc/CC_ColorSwitch.h
cb#
void(* colorComponent_::cb) (struct colorComponent_ *color)
pointer to app callback function that triggers driver changes
Definition at line
47
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/ColorSwitch/inc/CC_ColorSwitch.h