Device type#
Device type.
Macros#
The generic type of a device.
The specific type of a device.
Macro Definition Documentation#
ZAF_CONFIG_GENERIC_TYPE#
#define ZAF_CONFIG_GENERIC_TYPEValue:
0
The generic type of a device.
The generic type of a device. A certain device type requires a generic type, e.g., the Lock device type requires the generic type to be Entry Control. Find more info in the Z-Wave Plus v2 Device Type specification.
Option | Value |
---|---|
AV Control Point | GENERIC_TYPE_AV_CONTROL_POINT |
Entry Control | GENERIC_TYPE_ENTRY_CONTROL |
Generic Controller | GENERIC_TYPE_GENERIC_CONTROLLER |
Meter | GENERIC_TYPE_METER |
Repeater End Device | GENERIC_TYPE_REPEATER_END_NODE |
Sensor Multilevel | GENERIC_TYPE_SENSOR_MULTILEVEL |
Switch Binary | GENERIC_TYPE_SWITCH_BINARY |
Switch Multilevel | GENERIC_TYPE_SWITCH_MULTILEVEL |
Thermostat | GENERIC_TYPE_THERMOSTAT |
Wall Controller | GENERIC_TYPE_WALL_CONTROLLER |
Sensor Notification | GENERIC_TYPE_SENSOR_NOTIFICATION |
429
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/configuration/config/zaf_config.h
ZAF_CONFIG_SPECIFIC_TYPE#
#define ZAF_CONFIG_SPECIFIC_TYPEValue:
SPECIFIC_TYPE_NOT_USED
The specific type of a device.
The specific type of a device. A certain device type requires a specific type, e.g., the Lock device type requires the specific type to be Door Lock. Find more info in the Z-Wave Plus v2 Device Type specification.
Option | Value |
---|---|
Specific type not used | SPECIFIC_TYPE_NOT_USED |
Door Lock | SPECIFIC_TYPE_DOOR_LOCK |
Secure Gate | SPECIFIC_TYPE_SECURE_GATE |
Secure Barrier (open only) | SPECIFIC_TYPE_SECURE_BARRIER_OPEN_ONLY |
Secure Barrier (close only) | SPECIFIC_TYPE_SECURE_BARRIER_CLOSE_ONLY |
Color Tunable Binary | SPECIFIC_TYPE_COLOR_TUNABLE_BINARY |
Color Tunable Multilevel | SPECIFIC_TYPE_COLOR_TUNABLE_MULTILEVEL |
Class A Motor Control | SPECIFIC_TYPE_CLASS_A_MOTOR_CONTROL |
Class B Motor Control | SPECIFIC_TYPE_CLASS_B_MOTOR_CONTROL |
Class C Motor Control | SPECIFIC_TYPE_CLASS_C_MOTOR_CONTROL |
Thermostat General Version 2 | SPECIFIC_TYPE_THERMOSTAT_GENERAL_V2 |
Sound Switch | SPECIFIC_TYPE_SOUND_SWITCH |
Secure Keypad | SPECIFIC_TYPE_SECURE_KEYPAD |
Routing Sensor Multilevel | SPECIFIC_TYPE_ROUTING_SENSOR_MULTILEVEL |
Notification Sensor | SPECIFIC_TYPE_NOTIFICATION_SENSOR |
Repeater End Device | SPECIFIC_TYPE_REPEATER_END_NODE |
Infrared Repeater | SPECIFIC_TYPE_IR_REPEATER |
460
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/configuration/config/zaf_config.h