Public Attributes#
uint8_t
uint8_t 1, bit 0-6 - Can represent endpoints from 1-127 unless used as a bitmask where endpoint 1-7 is represented.
uint8_t
uint8_t 1, bit 7 - Interprets the endpoint fields as a bitmask addressing only the first 7 endpoints in destination.
Public Attribute Documentation#
nodeId#
node_id_t _MULTICHAN_DEST_NODE_ID_::nodeId
The ID of the destination node.
Definition at line
37
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h
endpoint#
uint8_t _MULTICHAN_DEST_NODE_ID_::endpoint
uint8_t 1, bit 0-6 - Can represent endpoints from 1-127 unless used as a bitmask where endpoint 1-7 is represented.
Definition at line
40
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h
BitAddress#
uint8_t _MULTICHAN_DEST_NODE_ID_::BitAddress
uint8_t 1, bit 7 - Interprets the endpoint fields as a bitmask addressing only the first 7 endpoints in destination.
Definition at line
43
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h