Notifying Queue object.
All content is public.
Public Attributes#
void *
FreeRTOS Queue handle.
uint8_t
which bit to use when notifying receiver task of pending queue item (range 0 - 31)
void *
Handle to queue receiver task where notifications are sent to.
Public Attribute Documentation#
Queue#
void* SQueueNotifying::Queue
FreeRTOS Queue handle.
Definition at line
47
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/Components/QueueNotifying/QueueNotifying.h
iTaskNotificationBitNumber#
uint8_t SQueueNotifying::iTaskNotificationBitNumber
which bit to use when notifying receiver task of pending queue item (range 0 - 31)
Definition at line
49
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/Components/QueueNotifying/QueueNotifying.h
ReceiverTask#
void* SQueueNotifying::ReceiverTask
Handle to queue receiver task where notifications are sent to.
Definition at line
52
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/Components/QueueNotifying/QueueNotifying.h