Zpal-bootloader#
Defines a platform abstraction layer for the Z-Wave bootloader.
How to use the bootloader API
The ZPAL bootloader API is required if an application would like to store and use a new firmware image.
zpal_bootloader_init() and zpal_bootloader_get_info() must be implemented as Z-Wave always invokes these. The remaining API functions are optional in case a bootloader is not present in the ZPAL implementation.
The following outlines an example of use:
To enable the bootloader functionality, invoke zpal_bootloader_init().
zpal_bootloader_get_info() must be invoked to check whether a bootloader is present.
For every received fragment, zpal_bootloader_write_data() must be invoked to store the new firmware image.
When all fragments are received, zpal_bootloader_verify_image() must be invoked to verify the integrity of the received firmware image.
If the received firmware image is valid, invoke zpal_bootloader_reboot_and_install() install and boot from the new firmware image.
Requirements:
The ZPAL bootloader requires that a storage is available for storing a received firmware image. Z-Wave has no requirements on how and where the image is stored.
Modules#
Enumerations#
Type of bootloader.
Functions#
//zpal-bootloader-info-version
Initialize components of the bootloader so the app can use the interface.
Reboot into the bootloader to install something.
Verify that the image is valid.
Writes a fragment of a firmware image to the bootloader storage.
Returns whether the software is running on the first boot after a new firmware image was written.
Resets the bootloader page counters.
Macros#
Bootloader has the capability of storing data in an internal or external storage medium.
Enumeration Documentation#
zpal_bootloader_type_t#
zpal_bootloader_type_t
Type of bootloader.
Enumerator | |
---|---|
ZPAL_BOOTLOADER_NOT_PRESENT | No bootloader present. |
ZPAL_BOOTLOADER_PRESENT | Bootloader present. |
56
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_bootloader.h
Function Documentation#
zpal_bootloader_get_info#
void zpal_bootloader_get_info (zpal_bootloader_info_t * info)
//zpal-bootloader-info-version
[out] | info | Pointer to the bootloader information struct. |
Get information about the bootloader on this device. The information returned is fetched from the main bootloader information table.
116
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_bootloader.h
zpal_bootloader_init#
zpal_status_t zpal_bootloader_init (void )
Initialize components of the bootloader so the app can use the interface.
N/A |
This typically includes initializing serial peripherals for communication with external SPI flashes, and so on.
Returns
Error code. ZPAL_STATUS_OK on success, else ZPAL_STATUS_FAIL
125
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_bootloader.h
zpal_bootloader_reboot_and_install#
void zpal_bootloader_reboot_and_install (void )
Reboot into the bootloader to install something.
N/A |
If there is a storage component and a slot is marked for bootload, install the image in that slot after verifying it. If a communication component is present, open the communication channel and receive an image to be installed.
134
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_bootloader.h
zpal_bootloader_verify_image#
zpal_status_t zpal_bootloader_verify_image (void )
Verify that the image is valid.
N/A |
Returns
ZPAL_STATUS_OK if the image is valid, else ZPAL_STATUS_FAIL.
141
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_bootloader.h
zpal_bootloader_write_data#
zpal_status_t zpal_bootloader_write_data (uint32_t offset, uint8_t * data, uint16_t length)
Writes a fragment of a firmware image to the bootloader storage.
[in] | offset | Offset from the storage start. |
[in] | data | Pointer to fragment of firmware image. |
[in] | length | Length of firmware image fragment. |
Returns
ZPAL_STATUS_OK on success, and ZPAL_STATUS_FAIL otherwise.
151
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_bootloader.h
zpal_bootloader_is_first_boot#
bool zpal_bootloader_is_first_boot (bool * updated_successfully)
Returns whether the software is running on the first boot after a new firmware image was written.
[in] | updated_successfully | Set to true if update was successful, false otherwise. Valid only when it's the first boot. |
Returns
True if it's the first boot, false otherwise.
159
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_bootloader.h
zpal_bootloader_reset_page_counters#
void zpal_bootloader_reset_page_counters (void )
Resets the bootloader page counters.
N/A |
Used when initiating an upgrade to jump back to the start of the storage slot.
165
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_bootloader.h
Macro Definition Documentation#
ZPAL_BOOTLOADER_CAPABILITY_STORAGE#
#define ZPAL_BOOTLOADER_CAPABILITY_STORAGEValue:
(1 << 0)
Bootloader has the capability of storing data in an internal or external storage medium.
75
of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_bootloader.h