Devices Menu
When you click the Devices menu, the Devices page displays with a list of your connected devices. You can expand each device to view any components associated with by clicking the right arrowhead at the left of the device name. The arrowhead points downward when the components display.
Refresh your list of devices by clicking Refresh at the top of the page.
A Configure button and ellipsis display on the right of each connected device in the list. Click the Configure button to display the Device Overview page with options that let you configure the settings on your device. If you click the ellipsis instead, a shortcut menu drops down with these options:
Detailed Overview: Takes you to the Device Overview page
Flash Target: Takes you to the Flash Target Application page
Update Adapter: Takes you to the Update Adapter page
Set Nickname: Takes you to the Device Hardware page
One or more Open <name of terminal> options, depending on how many terminals are connected to your device. Each option takes you to the associated terminal page.
To return, click < Devices on the upper left corner of your screen.
On the Device Overview page, you can view general information about your device and work with a variety of configuration settings.
Also, when this page is open, these options display on the left under the Devices menu:
Info menu options
Click Overview to display the Device Overview page, which shows:
The name of the connected device you selected
The status of the device – In the example above, the device is online.
The serial number for the device
How the device is connected: In the example above, the device is connected with a USB.
A row of tiles with information about the adapter firmware, secure firmware, debug mode, serial number of the device, and host. Some tiles have either Read or Change in blue letters. Click these words to either read or change the information in the tile.
Note: The secure firmware information is not shown by default. Click Read to see it.
The terminals available for the device: Hover over each terminal name to see whether it is open or not, or click a terminal name to open it.
A list of the hardware for the device
Firmware menu options
Flash Target Application: Click to display the Flash Target Application page, where you can flash your device. On the right of the page name, the serial number of the adapter displays. Drag and drop or browse for an application file to upload to flash from your device.
Update Adapter: Click to display the Update Adapter page, where you can update the firmware for your adapter. On the right of the page name, the serial number of the adapter displays. The version number of the firmware for your adapter displays under the page title, as well as a message on whether a new version of the firmware has been detected. If a new version of the firmware is available, a button displays where you can update it.
You can also install custom firmware by dragging and dropping or browsing for a custom adapter firmware image file using the Install Custom Firmware box.
Configuration menu options
Device Hardware: Click to display these options:
Nickname: Enter a unique name for your device in the field on the right.
Adapter Debug Mode: Select the adapter connection mode from the dropdown list on the right.
MCU: The debug adapter is connected to the target part on a connected radio board for main boards or the built-in target part for other development kits.
OUT: The debug adapter connects to an offboard target part through the debug connectors.
IN: The target part on a connected radio board for main boards or the built-in target part for other development kits are connected to the debug connectors, so a connection can be made from a different debug adapter. Mainly used to simulate a connection to a custom board.
MINI: Only available on the Wireless Pro Kit (WPK - BRD4002). Similiar to OUT mode, but the connection is made to the mini-simplicity connector on the board instead of the debug connectors.
OFF: Turns off all connections to target parts. Not useful for development. The debug adapter goes into this mode if it is in it's bootloader mode. If the debug mode cannot be changed from OFF then the debug adapter firmware needs to be updated.
Target Interface: Select the interface connection mode from the dropdown list on the right.
Configured Hardware: Displays how other tools will see your device when it is connected. Remove a piece of hardware or component by clicking Remove on the right of its name. A Restore All button then displays in case you want to restore the items you removed.
Physical Hardware: Displays the physical hardware detected by Device Manager.
Hardware Override: Search for and add boards and devices to your configuration. Find a board or part by entering a keyword in the field under the Board or Part heading. Your search results display under the field. Add a board or part by clicking Add on the right of its name. The Hardware Override option is is helpful when working with custom hardware designs.
Packet Trace: Click to display these options:
Enable Packet Trace: Check this box to enable the packet trace interface on the debug adapter.
Interface Number: Select the packet trace interface number from the dropdown list on the right.
Mode: Select a mode from the dropdown list on the right.
Bitrate: Enter a bitrate value.
Terminals menu options: The number of options vary, depending on the adapter firmware capability of the development board. In the example below, there are four terminals. Click the name of a terminal to view it and enter commands to communicate with it. For the Admin console, enter
help
to get a list of supported commands.help
also normally works on the Serial0 and Serial1 consoles, if the application has command line support.
To return to the main Devices page, click < Devices at the top left corner of your screen.