GPIOs
GPIO commands allow control of the function and direction of the GPIOs.
- get gp u - List GPIO usage, direction and initialization
- set gp u - Set the format of the GPIO usage list
- gfu - Configure GPIO function
-
gdi
- Set GPIO direction for a GPIO functioning as
stdio(Standard Input/Output) -
gdis
- Set
stdiofunction and GPIO direction for multiple GPIOs -
gge
- Get GPIO value for a GPIO functioning as
stdio -
gges
- Get multiple values for GPIOs functioning as
stdio -
gse
- Set GPIO value for a GPIO functioning as
stdio -
gses
- Set multiple values for GPIOs functioning as
stdio
Typically, particular GPIOs are hard-wired to components such as LEDs and buttons. Other GPIOs are configurable for input and output.
GPIOs can be used for special system functions, including (but not limited to):
- assigning a LED as a BLE connection indicator
- selecting between serial bus modes: COMMAND or STREAM
- blink on BLE activity
- general standard IO function
GPIO Functions and Pins
In the following examples, the BGX EXP evaluation board is used to demonstrate GPIO functions.
Viewing GPIO Usage
To see the current GPIO usage, read the GPIO usage variable. The default BGX EXP usage is:
> get gp u
! # Description
# 0 none
# 1 none
# 2 none
# 3 none
# 4 none
# 5 none
# 6 none
# 7 none
Setting GPIO Function
Use the GPIO function command to set a single GPIO to a specific function.
After using gfu , it may be necessary to save then reboot depending on the alternate function (some functions are only configured at boot up).
Use
gdis
command to set
stdio
function and direction
for multiple GPIOs. See
Setting and Getting Multiple STDIO GPIO
Values
below.
Available functions are listed in the gfu command documentation.
The
gfu
command fails if the GPIO is already configured
for an alternate function. Disable the alternate function first by using
gfu <GPIO#> none
.
For example, to enable GPIO 5 to operate as
stdio
:
> gfu 5 stdio
Success
To use LED0 to indicate when stream mode is on:
> gfu 0 str_activity_led
Success
Setting and Getting a Single STDIO GPIO Value
To set and get the value of a single GPIO, use the gse and gge commands.
Note that to set a GPIO, the GPIO must have
stdio
function and the output
direction. To get the value, the GPIO must have
stdio
function. See
Setting GPIO Function
.
For example, set and clear GPIO 1 to turn LED1 on and off:
> gfu 1 stdio
Success
> gdi 1 olo
Success
> gge 1
0
> gse 1 1
Success
> gge 1
1
Setting and Getting Multiple STDIO GPIO Values
To set and get multiple
stdio
GPIO values, use the
gses
and
gges
commands.
For example, set GPIO 0 (LED0) and GPIO 1 (LED1) as
stdio
open-drain outputs
with no pull-ups, and GPIO 2 (BTN0) and GPIO 3 (BTN1) as
stdio
inputs with
pull-ups.
> gdis 4400XXXX
Success
With no buttons pressed, get the values of the
stdio
GPIOs:
> gges
1111XXXX
Now turn the LED0 on:
> gses 0111XXXX
Success
Press both buttons and get the values of the
stdio
GPIOs:
> gges
0100XXXX
Version Notes
For versions previous to
1.1.1229.0
, calling 'gdis' with any value other than
6
or
X
for a pin configured as
none
results in an error. The pin must
first be configured as
stdio
with the
gfu
command. The configuration
sequence in the
Setting and Getting Multiple STDIO GPIO
Values
section must be:
> gfu 0 stdio
Success
> gfu 1 stdio
Success
> gfu 2 stdio
Success
> gfu 3 stdio
Success
> gdis 4400XXXX
Success