BGX13 Variable Reference
This page provides a list of Bluetooth Xpress (BGX) BLE variables with a full description of the function of each variable together with example usage.
Variables are cached in volatile RAM and must be saved to non-volatile flash memory to persist between reboots. To save variables to flash, use the save command.
NOTE! Don't forget to check out command navigation tips to make it easier to find and type specific variable names.
Documentation Format
Many of the Bluetooth Xpress responses shown in the examples on this page were captured with the highest system print level ( sy p ) = 4, and system command header enabled ( sy c h ) = 1. These settings are provided to make it easy for a host microcontroller to parse responses by examining response headers.
Version Availability
Variables that were not available in the original product release but that have been added since are indicated with Version Notes . If the variable has no version notes, it means it was available since the original release.
List of Variables
-
All Variables
- al --- all variables
-
BLE Peripheral
- bl a --- BLE address
- bl c c --- connection count
- bl c i --- BLE connection interval
- bl c t --- BLE connection supervision timeout
- bl d a --- BLE device appearance
- bl e b --- encryption bondable mode
- bl e k --- encryption key
- bl e p --- encryption pairing mode
- bl p m --- BLE PHY multiplex
- bl p p --- BLE PHY preference
- bl t c --- transmit power
- bl v h d --- advertising high duration
- bl v h i --- advertising high interval
- bl v l d --- advertising low duration
- bl v l i --- advertising low interval
- bl v m --- advertising mode
- bl v p --- advertising preference
- bl v x d --- advertising xpress mode duration
- bl v x i --- advertising xpress mode interval
- Bus
- BLE Central
-
GPIO
- gp u --- GPIO usage
-
I2C
- i2 b s --- I2C bus speed
-
System
- sy c e --- command echo
- sy c h --- command header
- sy c m --- command mode
- sy c p --- command prompt enabled
- sy d n --- device name
- sy i m --- info string manufacturer
- sy i p --- info string product
- sy i s --- system indicator status LED blink behavior
- sy o e --- OTA enabled
- sy o p --- OTA password
- sy p --- print level
- sy r e --- remote command enabled
- sy r p --- remote command password
- sy s m --- sleep mode
- sy u -- system UUID
- sy v -- firmware version
- sy w c -- wake on CTS
-
Test Mode
- tm n p -- Test mode number of packets
- UART
- User Function
Variable Description
All
al
All (variables)
Description
Returns a list of all variables. This includes the list of GPIO settings returned by gp u .
| Attribute | Description |
|---|---|
| access | get |
Get example
> get al
bl a : D0CF5E828DC6
bl c c : 0
bl c i : 12
bl c t : 400
bl d a : 512
bl e b : 1
bl e k : none
bl e p : any
bl p m : 0
bl p p : 1m
bl t c : 8
bl v h d : 30
bl v h i : 32
bl v l d : 0
bl v l i : 874
bl v m : low
bl v p : high
bl v x d : 30
bl v x i : 32
bu i : command
bu s c : level
bu s s : 242424
ce c c : 0
ce s h d : 30
ce s h i : 96
ce s l d : 300
ce s l i : 2048
ce s m : off
ce w m : ack
gp u :
! # Description
# 0 none
# 1 none
# 2 none
# 3 none
# 4 none
# 5 none
# 6 none
# 7 none
i2 b s : 92
sy c e : 0
sy c h : 0
sy c p : 1
sy d n : BGX-8DC6
sy i m : Silicon Labs
sy i p : Bluetooth Xpress
sy i s : 04047F000404
sy o e : 1
sy o p : none
sy p : 4
sy r e : 1
sy r p : none
sy s m : deep
sy u : 4C892A6AB30335045E0374CAD0CF5EFFFE828DC6
sy v : BGX13P.1.2.2045.0-1524-2045
sy w c : 1
tm n p : 0
ua b : 115200
ua f : 0
uf l p : 20
uf u :
! # Description
# 0 none ()
# 1 none ()
# 2 none ()
# 3 none ()
# 4 none ()
# 5 none ()
# 6 none ()
# 7 none ()
BLE Peripheral
bl a
BLE Address
Description
Returns the BLE device address.
| Attribute | Description |
|---|---|
| format | 6-byte hex string, big-endian |
| default | unique per device |
| access | get |
| save | n/a |
Get example
> get bl a
D0CF5E35E0D8
bl c c
BLE Connection Count
Description
Returns the number of centrals that are connected when acting as a peripheral. Will return 0 or 1.
| Attribute | Description |
|---|---|
| format | integer |
| units | count |
| min | 0 |
| max | 1 |
| default | 0 |
| access | get |
| save | n/a |
Get example
> get bl c c
0
bl c i
BLE Connection Interval
Description
BLE connection interval. See Bluetooth specification : Important Connection Parameters : Connection Interval, Supervision Timeout
Notes:
-
For BGX-to-BGX use cases, the recommended configuration is to set
bl c ito the same value for both devices.
| Attribute | Description |
|---|---|
| format | integer |
| units | 1.25 ms |
| min | 6 (7.5 ms) |
| max | 3200 (4000 ms) |
| default | 12 (15 ms) |
| access | get/set |
| save | yes |
Get example
> get bl c i
12
Set example
> set bl c i 10
Success
bl c t
BLE Connection Timeout
Description
BLE connection supervision timeout. See Bluetooth specification : Important Connection Parameters : Connection Interval, Supervision Timeout .
| Attribute | Description |
|---|---|
| format | integer |
| units | 10 ms |
| min | 10 (100 ms) |
| max | 3200 (32000 ms) |
| default | 400 (4000 ms) |
| access | get/set |
| save | yes |
Get example
> get bl c t
400
Set example
> set bl c t 500
Success
bl d a
BLE Device Appearance
Description
BLE device appearance is a 16 bit integer that describes how the device
appears to other devices. It is part of the GAP database. The default value of
512
corresponds to Generic tag, Generic category.
For other appearance values, see Bluetooth GAP Appearance .
| Attribute | Description |
|---|---|
| format | integer |
| units | n/a |
| min | 0 |
| max | 65535 |
| default | 512 |
| access | get/set |
| save | yes |
Get example
get bl d a
512
Set example
set bl d a 512
Success
bl e b
BLE Encryption Bondable (mode)
Description
Enables or disable bonding. Encryption is always enabled for the Bluetooth Xpress module.
Note: The Bluetooth Xpress device can remember up to 14 devices in its internal bonding table. As new devices are added (beyond 14), older less used devices are forgotten.
| Attribute | Description |
|---|---|
| format | integer |
| units | 1=true/enabled, 0=false/disabled |
| min | 0 |
| max | 1 |
| default | 1 |
| access | get/set |
| save | yes |
Get example
> get bl e b
1
Set example
> set bl e b 1
Success
bl e k
BLE Encryption Key
Description
The BLE encryption key can be set to
none
or to a 6 digit pin. Entering more
or less than 6 digits, or entering a pin with non-numeric characters other
than 'none' will cause the command to fail. Encryption is always enabled on
the Bluetooth Xpress module.
The key type determines the pairing procedure and security mode and level. See Security .
Note
: if the key is set to
none
, and an Android phone requests a pin, use
000000
.
| Attribute | Description |
|---|---|
| format | 6-digit integer or 'none' |
| units | n/a |
| min | 000000 |
| max | 999999 |
| default | 'none' |
| access | get/set |
| save | yes |
Get example
> get bl e k
none
Set example
> set bl e k 123456
Success
bl e p
BLE Encryption Pairing (mode)
Version Notes
Starting at
1.1.1229.0
added new option "off" and changed the default from
"secure" to "any".
Description
Determines the policy for new pairing requests. When set to
off
, all new pairing
requests are rejected. Selecting
secure
enables pairing with LE Secure Connections
(BLE 4.2 or newer) only, while
any
enables pairing with either secure or legacy
methods. When
any
is selected LE Secure Connections will be used by default if
supported by the connecting device. Encryption is always enabled on Bluetooth Xpress
modules.
Note : This setting only applies to new pairing requests and does not affect devices that were previously bonded.
| Attribute | Description |
|---|---|
| format | string enumeration |
| units |
'secure'=secure only
'any'=secure or legacy 'off'=disabled |
| default | any |
| access | get/set |
| save | yes |
Get example
> get bl e p
secure
Set example
> set bl e p off
Success
bl p m
BLE PHY Multiplex
Version Notes
Added in
1.1.1229.0
Description
Selects whether the peripheral advertises on one or multiple PHY's. When enabled the peripheral will advertise on both the LE 1M and LE Coded PHY's. When disabled the peripheral will advertise on one PHY determined by PHY preference setting bl p p .
Note : The BGX only supports one connection at a time. Once a connection is established on any PHY, advertising is automatically disabled on all enabled PHY's.
| Attribute | Description |
|---|---|
| format | integer |
| units | 1=true/enabled, 0=false/disabled |
| min | 0 |
| max | 1 |
| default | 0 |
| access | get/set |
| save | yes |
Get example
> get bl p m
0
Set example
> set bl p m 1
Success
bl p p
BLE PHY Preference
Version Notes
Beginning with version
1.1.1229.0
, added new options
125k
and
500k
. Also
changed the preferred PHY requester from the BGX peripheral to the central
device (phone or BGX).
Description
Specifies the PHY preference for BLE GAP procedures. When either
1m
or
2m
is
selected the device will advertise, scan and initiate connections using the BLE
1M PHY. If the central device (phone or BGX) has been configured to prefer the
BLE 2M PHY, it will start a procedure to switch PHY's once a connection is
established.
When either
125k
or
500k
is selected the device will advertise, scan and initiate
connections using the BLE Coded PHY (S=8). For both central and peripheral devices,
selecting
500k
only affects the transmit direction. After a connection is established
using the BLE Coded PHY (S=8), the transmit PHY will switch to the BLE Coded PHY (S=2).
It is possible to advertise on both the 1M and Coded PHY's at the same time. Use bl p m to enable this feature.
Notes:
-
For BGX-to-BGX use cases, the recommended configuration is to set
bl p pto the same value for both devices. -
For BGX-to-phone use cases,
bl p ponly affects advertising as the selection of preferred PHY is made by the phone.
| Attribute | Description |
|---|---|
| format | string enumeration |
| units |
'1m'=1M PHY
'2m'=2M PHY '125k'=Coded PHY(S=8) '500k'=Coded PHY(S=2) |
| default | 1m |
| access | get/set |
| save | yes |
Get example
> get bl p p
1m
Set example
> set bl p p 2m
Success
bl t c
BLE Transmit Connected (power)
Description
Configures the RF transmit power when connected.
| Attribute | Description |
|---|---|
| format | integer |
| units | dBm |
| min | -25 |
| max | 8 |
| default | 8 |
| access | get/set |
| save | yes |
Note: The BGX uses its low power amplifier when the transmit power setting is below 0 dBm. The low power amplifier only supports several discrete power settings below 0 dBm. For this reason, negative output power values will result in an actual output power that does not exactly match the value specified.
Get example
> get bl t c
8
Set example
> set bl t c 4
Success
bl v h d
BLE adVertising High Duration
Description
Configures high mode advertising duration. This is the duration in seconds for which advertising continues after issuing the adv high command. See BLE Advertising .
| Attribute | Description |
|---|---|
| format | integer |
| units | seconds |
| min | 0 (advertise forever) |
| max | 1000 |
| default | 30 |
| access | get/set |
| save | yes |
Get example
> get bl v h d
30
Set example
> set bl v h d 40
Success
bl v h i
BLE adVertising High Interval
Description
Configures high mode advertising interval, used for the
adv
command
high
option. The interval is measured in slots. For example, an
interval of 32 means advertise in slot 0, then 32, then 64 and so on. Valid
range: 32 - 16384 slots inclusive.
| Attribute | Description |
|---|---|
| format | integer |
| units | slots |
| min | 32 |
| max | 16384 |
| default | 32 |
| access | get/set |
| save | yes |
Get example
> get bl v h i
32
Set example
> set bl v h i 50
Success
bl v l d
BLE adVertising Low Duration
Description
Configures low mode advertising duration. This is the duration in seconds for which advertising continues after issuing the adv low command. See BLE Advertising .
| Attribute | Description |
|---|---|
| format | integer |
| units | seconds |
| min | 0 (advertise forever) |
| max | 1000 |
| default | 0 (forever) |
| access | get/set |
| save | yes |
Get example
> get bl v l d
0
Set example
> set bl v l d 350
Success
bl v l i
BLE adVertising Low Interval
Description
Configures low mode advertising interval, used for the
adv
command
low
option. The interval is measured in slots. For example, an
interval of 32 means advertise in slot 0, then 32, then 64 and so on. Valid
range: 32 - 16384 slots inclusive.
| Attribute | Description |
|---|---|
| format | integer |
| units | slots |
| min | 32 |
| max | 16384 |
| default | 874 |
| access | get/set |
| save | yes |
Get example
> get bl v l i
874
Set example
> set bl v l i 64
Success
!-- structElement:varHeading -->
bl v x d
BLE adVertising Xpress Duration
Version Notes
Added in
1.2.2045.0
Description
Configures Xpress mode advertising duration. This is the duration in seconds for which advertising continues after issuing the adv xpr command. See BLE Advertising .
| Attribute | Description |
|---|---|
| format | integer |
| units | seconds |
| min | 1 |
| max | 180 |
| default | 30 |
| access | get/set |
| save | yes |
Get example
> get bl v x d
30
Set example
> set bl v x d 40
Success
bl v x i
BLE adVertising Xpress Interval
Version Notes
Added in
1.2.2045.0
Description
Configures Xpress mode advertising interval, used for the
adv
command
xpr
option. The interval is measured in slots. For example, an
interval of 32 means advertise in slot 0, then 32, then 64 and so on. Valid
range: 32 - 16384 slots inclusive.
| Attribute | Description |
|---|---|
| format | integer |
| units | slots |
| min | 32 |
| max | 16384 |
| default | 32 |
| access | get/set |
| save | yes |
Get example
> get bl v x i
32
Set example
> set bl v x i 64
Success
bl v m
BLE adVertising Mode
Version Notes
xpr
value added in
1.2.2045.0
.
Description
Get peripheral advertising mode, as set by the adv command.
| Attribute | Description |
|---|---|
| format | string enumeration |
| units |
'high'=adv high mode
'low'=adv low mode 'xpr'=adv xpress mode 'off'=no advertising |
| default | 'high' |
| access | get |
| save | n/a |
Get example
> get bl v m
high
bl v p
BLE adVertising Preference
Version Notes
Added in
1.1.1229.0
xpr
argument added in
1.2.2045.0
.
Description
Selects which advertising mode is entered whenever exiting a non-advertising mode (sleep, connection, scan, etc.).
| Attribute | Description |
|---|---|
| format | string enumeration |
| units |
'high'=adv high mode
'low'=adv low mode 'xpr'=adv xpress mode 'off'=no advertising |
| default | 'high' |
| access | get/set |
| save | yes |
Get example
> get bl v p
low
Set example
> set bl v p off
Success
Bus
bu i
Bus Initialization (mode)
Description
Serial bus initialization mode for
str_select
. If GPIO option
str_select
is used, and it is configured for edge mode (see
bu s c
), then this
option determines the initial mode of the serial bus (COMMAND or STREAM).
Notes :
-
For more information about bus modes and
str_select, see Manual and Automatic Bus Mode Selection .
| Attribute | Description |
|---|---|
| format | string enumeration |
| units |
'stream'=stream mode
'command'=command mode (remote command mode locked out) |
| default | 'command' |
| access | get/set |
| save | yes |
Get example
> get bu i
command
Set example
> set bu i stream
Success
> save
Success
bu s c
Bus Serial Control
Description
Serial bus switch control mode for
str_select
. If GPIO option
str_select
is used, then this option is used to determine whether the pin switching is
edge or level mode for selecting serial bus STREAM or COMMAND mode.
If
bu s c
is set to
edge
, a rising edge on the
str_select
pin toggles
the mode. The initial bus mode after reset can be configured
(see
bu i
).
If
bu s c
is set to
level
, the serial bus mode is selected by
driving a constant high or low logic level onto the
str_select
pin. In
level mode a low level selects COMMAND mode and a high level selects
STREAM mode.
Note:
The
str_select
pin is configured with the
GPIO function
command.
| Attribute | Description |
|---|---|
| format | string enumeration |
| units |
'edge'=rising edge toggle on
str_select
'level'=mode selected by logic level |
| default | 'level' |
| access | get/set |
| save | yes |
Get example
> get bu s c
level
Set example
> set bu s c edge
Success
bu s s
Bus Stream (breakout) Sequence
Description
Set a new bus stream breakout sequence. Sending the breakout sequence when in
STREAM mode places the device in local COMMAND mode. To disable the breakout
sequence, set to
none
. See
Serial Bus Modes
.
In order to be seen as a breakout condition, the breakout sequence must be preceded and followed by idle periods of at least 500 milliseconds on the BGX UART's Rx line. The amount of time between each character in the breakout sequence must be less than 255 bit times or 4 milliseconds, whichever is shorter.
Due to these timing constraints, it is generally not possible to send the breakout sequence by manually typing it into a terminal. Instead, a terminal program with the capability to send macros should be used.
Note
: Setting to
00
sets the breakout sequence to the hexadecimal
0x00
,
corresponding to the ASCII NULL character.
Note : The breakout sequence does not work reliably for serial data rates less than 5000 bits per second .
| Attribute | Description |
|---|---|
| format | up to 4-byte hex string |
| default | 242424 ('$$$') |
| access | get/set |
| save | yes |
Get example
> get bu s s
242424
Set example
Set breakout sequence to ASCII characters "BRK"
> set bu s s 42524b
Success
Disable breakout sequence:
> set bu s s none
Central
ce c c
Central Connection Count
Description
Returns the number of peripherals connected when acting as a central. Will return 0 if not connected, and 1 if connected.
| Attribute | Description |
|---|---|
| format | integer |
| units | count |
| min | 0 |
| max | 1 |
| default | 0 |
| access | get |
| save | n/a |
Get example
> get ce c c
0
ce s h d
Central Scan High Duration
Description
Configures central scan high mode duration. This is the duration in seconds for which scan continues after issuing the scan high command.
| Attribute | Description |
|---|---|
| format | integer |
| units | seconds |
| min | 0 (scan forever) |
| max | 1000 |
| default | 30 |
| access | get/set |
| save | yes |
Get example
> get ce s h d
30
Set example
> set ce s h d 40
Success
ce s h i
Central Scan High Interval
Version Notes
Starting with version
1.1.1229.0
, if scanning is configured to use
the BLE Coded PHY, the configured scan interval values are automatically
tripled.
Description
Configures central high mode scanning interval, used for the
scan
command
high
option.
| Attribute | Description |
|---|---|
| format | integer |
| units | slots |
| min | 4 |
| max | 16384 |
| default | 96 |
| access | get/set |
| save | yes |
Get example
> get ce s h i
96
Set example
> set ce s h i 1000
Success
ce s l d
Central Scan Low Duration
Description
Configures central low mode scanning duration. This is the duration in seconds for which scanning continues after issuing the scan low command.
| Attribute | Description |
|---|---|
| format | integer |
| units | seconds |
| min | 0 (scan forever) |
| max | 1000 |
| default | 300 |
| access | get/set |
| save | yes |
Get example
> get ce s l d
300
Set example
> set ce s l d 350
Success
ce s l i
Central Scan Low Interval
Version Notes
Starting with version
1.1.1229.0
, if scanning is configured to use
the BLE Coded PHY, the configured scan interval values are automatically
tripled.
Description
Configures low mode scanning interval, used for the
scan
command
low
option.
| Attribute | Description |
|---|---|
| format | integer |
| units | slots |
| min | 4 |
| max | 16384 |
| default | 2048 |
| access | get/set |
| save | yes |
Get example
> get ce s l i
2048
Set example
> set ce s l i 64
Success
ce s m
Central Scan Mode
Description
With this device acting as a Central, returns scan mode, as set by the scan command.
| Attribute | Description |
|---|---|
| format | string enumeration |
| units |
'high'=scan high mode
'low'=scan low mode 'off'=no scanning |
| default | 'off' |
| access | get |
| save | n/a |
Get example
> get ce s m
off
ce w m
Central Write Mode
Version Notes
Starting with version
1.2.2045.0
, the
ack
setting uses Fast-Ack Flow Control
instead of Legacy Flow Control (see
Xpress Streaming Service Flow Control
).
The
noack
setting is not recommended, because the
ack
setting guarantees
data integrity while still achieving high throughput rates.
The
noack
setting is still available to maintain backwards-compatibility with
existing BGX applications.
Description
This variable controls whether the connection requires acknowledgement on writes.
| Attribute | Description |
|---|---|
| format | string enumeration |
| units |
'ack'=use write acknowledgement
'noack'=do not use acknowledgment |
| default | 'ack' |
| access | get/set |
| save | yes |
Get example
> get ce w m
ack
Get example
> set ce w m noack
Success
GPIO
gp u
GPIO Usage
Description
Get GPIO usage. See the GPIO function command for a description of configurable and automatically assigned GPIO functions.
By default
get gp u
displays the function and the direction set by the
gdi
or
gdis
commands. For example:
> gfu 5 stdio
Success
> gdi 5 ipu
Success
> gfu 6 stdio
Success
> gdi 6 ohi
Success
> get gp u
! # Description
...
# 5 stdio,ipu
# 6 stdio,ohi
...
To view the pin mode and extra options set by the
gdi
command
set this variable to
verbose
. To change back to the shorter display, set this
variable to
default
.
> set gp u verbose
Success
> get gp u
! # Description
...
# 5 stdio,ipu (ioz)
# 6 stdio,ohi (ioz,pp,drvst)
...
| Attribute | Description |
|---|---|
| format | table list |
| units |
'default'=abbreviated display
'verbose'=detailed display |
| default | 'default' |
| access | get/set |
| save | no |
Get example
> get gp u
! # Description
# 0 stdio
# 1 stdio
# 2 none
# 3 none
# 4 none
# 5 none
# 6 none
# 7 none
I2C
i2 b s
I2C Bus Speed
Version Notes
Added in
1.2.2045.0
Description
I2C Master bus speed in kHz. This is the bus speed that will be used for the i2crd and i2cwr commands.
| Attribute | Description |
|---|---|
| format | integer |
| units | kHz |
| min | 10 |
| max | 1000 |
| default | 92 (BGX13), 100 (BGX220) |
| access | get/set |
| save | yes |
Note:
The ratio between the low period and high period of the clock pulses
on
i2cm_scl
(
Tlow:Thigh
) varies at different I2C bus speed settings as shown
in the table below:
| i2 b s | Tlow:Thigh |
|---|---|
| i2 b s <= 92 | 1 : 1 |
| 93 <= i2 b s <= 392 | 2 : 1 |
| i2 b s >= 393 | 3.67 : 1 |
Note: : SCL and SDA pins should be defined using gfu command before setting I2C bus speed.
Get example
> get i2 b s
92
Set example
> set i2 b s 1000
Success
System
sy c e
System Command Echo
Description
Enable/disable character echo.
Note! If character echo is turned off, keystrokes that are subsequently typed are not echoed to the serial interface (or terminal). This mode is primarily intended for machine control.
| Attribute | Description |
|---|---|
| format | integer |
| units | 1=true/enabled, 0=false/disabled |
| min | 0 |
| max | 1 |
| default | 1 |
| access | get/set |
| save | yes |
Get example
> get sy c e
1
Set example
> set sy c e 0
Success
sy c h
System Command Header
Description
Enable/disable a response header for commands. Only applies to command mode. Response headers make it easy to parse responses with a host MCU.
See Serial Interface, Response Format for the reponse header format.
| Attribute | Description |
|---|---|
| format | integer |
| units | 1=true/enabled, 0=false/disabled |
| min | 0 |
| max | 1 |
| default | 0 |
| access | get/set |
| save | yes |
Get example
> get sy c h
0
Set example
> set sy c h 1
Success
sy c m
System Command Mode
Description
Puts the Bluetooth Xpress command interface into human or machine mode. See Serial Interface, Configuration . Note! This variable is NOT readable.
| Attribute | Description |
|---|---|
| format | string enumeration |
| units |
'machine'=machine mode
'human'=human mode |
| default | 'human' |
| access | set |
| save | yes |
Set example
> set sy c m machine
Success
sy c p
System Command Prompt
Description
Enable/disable terminal command prompt. Only applies to command mode. A prompt makes it easy for humans to interact with Bluetooth Xpress module.
| Attribute | Description |
|---|---|
| format | integer |
| units | 1=true/enabled, 0=false/disabled |
| min | 0 |
| max | 1 |
| default | 1 |
| access | get/set |
| save | yes |
Get example
> get sy c p
1
Set example
> set sy c p 1
Success
sy d n
System Device Name
Description
Bluetooth device name, up to 16 characters in length. Up to all 12 digits
of the Bluetooth address from
BD_ADDR
may be substituted
by hash
#
wildcard characters. The wildcard characters must be contiguous
and the BD address will be right-justified within the field. See the examples
below.
| Attribute | Description |
|---|---|
| format | string |
| min | -- |
| max | 16 characters length |
| default | 'BGX-####' |
| access | get/set |
| save | yes |
Get example
> get bl a
4C55CCABCDEF
> get sy d n
BGX-CDEF
Set example
In the following examples the BD_ADDR address is
4C55CCABCDEF
(see
bl a
)
> set sy d n ACK-##
Success
> get sy d n
ACK-EF
> set sy d n BGX###
Success
> get sy d n
BGXDEF
> set sy d n my######
Success
> get sy d n
myABCDEF
> set sy d n ###-DEV
Success
> get sy d n
DEF-DEV
sy i m
System Info Manufacturer
Description
Manufacturer string, up to 32 characters in length. Use double quotes to enter a name containing a space.
| Attribute | Description |
|---|---|
| format | string |
| min | -- |
| max | 32 characters length |
| default | 'Silicon Labs' |
| access | get/set |
| save | yes |
Get example
> get sy i m
Silicon Labs
Set example
> set sy i m "Placeholder Name"
Success
> get sy i m
Placeholder Name
sy i p
System Info Product
Version Notes
Prior to
1.1.1229.0
the default value was "Blue Gecko Xpress"
Description
Product information string, up to 32 characters in length. Use double quotes to enter a name containing a space.
| Attribute | Description |
|---|---|
| format | string |
| min | -- |
| max | 32 characters length |
| default | 'Bluetooth Xpress' |
| access | get/set |
| save | yes |
Get example
> get sy i p
Bluetooth Xpress
Set example
> set sy i p "Placeholder Product"
Success
> get sy i p
Placeholder Product
sy i s
System Indicator Status (setting)
Version Notes
Starting with version
1.2.2045.0
an additional blink pattern was added for
attempting to connect/advertising.
Description
Set the blink pattern for the
con_status_led
pin function. The command takes
6 hexadecimal values AABBCCDDEEFF, where AA, BB, CC and DD are hex numbers in
the range
00
to
FF
.
AABB sets the LED blink pattern when not connected. CCDD sets the LED blink pattern when connected. EEFF sets the blink pattern when attempting to connect (i.e. adv or con command is executing).
Note
: For backwards compatibility, the EEFF portion of the variable can
be omitted. When the variable is set using AABBCCDD, the connecting blink
pattern will match the
not
connected blink pattern. For versions prior to
1.2.2045.0
the EEFF portion will not be accepted.
The low part of the blink pattern is set with AA when not connected (CC when connected, EE when attempting to connect).
The high period of the blink pattern is set with BB when not connected (DD when connected, FF when attempting to connect).
Each pattern tick equals 0.1 sec (100 msec).
Some examples:
| Low = AA/CC/EE | High = BB/DD/FF | Period | Duty Cycle | Notes |
|---|---|---|---|---|
04
|
04
|
0.80s | 50% | 1.25 Hz --- default blink pattern when not connected or attempting to connect |
7f
|
00
|
--- | 0% | Always low --- default blink pattern when connected |
01
|
01
|
0.20s | 50% | Fastest possible blink. Duty cycle = 50% |
ff
|
ff
|
51.0s | 50% | Slowest possible blink. Duty cycle = 50% |
1c
|
04
|
3.20s | 12.5% | Period = (28 + 4) x 0.1s, Duty cycle = 4/(28 + 4) x 100% |
| Attribute | Description |
|---|---|
| format | 6-byte hex string (4 bytes for legacy behavior) |
| units | 0.1 sec resolution per byte |
| min | '00' per byte (inactive) |
| max | 'FF' per byte |
| default | '04047F000404' (1.25 Hz blink when not connected or attempting to connect, always low when connected) |
| access | get/set |
| save | yes |
Get example
> get sy i s
04047F000404
Set example
Set to fastest blink when not connected, slower blink when connected.
> set sy i s 0101ffff0202
Success
sy o e
System OTA Enable
Description
Enable or disable OTA upgrades.
| Attribute | Description |
|---|---|
| format | integer |
| units | 1=true/enabled, 0=false/disabled |
| min | 0 |
| max | 1 |
| default | 1 |
| access | get/set |
| save | yes |
Get example
> get sy o e
1
Set example
> set sy o e 1
Success
sy o p
System OTA Password
Version Notes
This variable was added in
1.2.2045.0
.
Description
Requires the remote device to provide a password to enable OTA firmware update.
If set to
none
, OTA is not protected by a password.
If set to a string, the remote device must provide a password when performing a firmware update.
| Attribute | Description |
|---|---|
| format | Up to 16-character string |
| default | none |
| access | get/set |
| save | yes |
Get example
> get sy o p
none
Set example
> set sy o p 123456
Success
sy p
System Print (level)
Description
System print level.
| Attribute | Description |
|---|---|
| format | integer |
| units |
0 = no messages
1 = synchronous system messages 2 = synchronous logging messages 3 = asynchronous system messages 4 = all/asynchronous logging messages |
| min | 0 |
| max | 4 |
| default | 4 |
| access | get/set |
| save | yes |
Get example
> get sy p
0
Set example
> set sy p 0
Success
sy r e
System Remote (commanding) Enabled
Version Notes
Restricted mode was added in version
1.2.2045.0
.
Description
Enables/disables/restricts access to the Bluetooth Xpress module command interface from a remote terminal via the BLE interface (remote COMMAND mode).
If
sy r e
is set to 0, access to the command interface is restricted to the
UART interface (local COMMAND mode). See
Serial Interface
.
If
sy r e
is set to 1, access to the command interface is enabled for remote
COMMAND mode.
If
sy r e
is set to 2, access to the command interface is restricted to the
following set of commands.
Remote Commands Allowed in Restricted Mode
| Command | Usage |
|---|---|
| gdi | set GPIO direction and pin mode (stdio) |
| gdis | set direction for multiple GPIOs |
| gfu | select GPIO function |
| gge | get GPIO value (stdio) |
| gges | get multiple GPIO values |
| gse | set GPIO value (stdio) |
| gses | set multiple GPIO values |
| i2crd | I2C read |
| i2cwr | I2C write |
| rssi | display RSSI value for current connection |
| str | switch to stream mode |
| ver | show version |
| Attribute | Description |
|---|---|
| format | integer |
| units | 0=disabled, 1=unrestricted, 2=restricted (GPIO and I2C only) |
| min | 0 |
| max | 2 |
| default | 1 |
| access | get/set |
| save | yes |
Get example
> get sy r e
1
Set example
> set sy r e 1
Success
sy r p
System Remote (commanding) Password
Version Notes
This variable was added in
1.2.2045.0
.
Description
Requires that the remote device use a password to access the Bluetooth Xpress module's command interface from a remote terminal via the BLE interface (remote COMMAND mode).
If set to
none
, remote COMMAND mode is not protected by a password (although
is can still be disabled or restricted via
sy r e
).
If set to a string, specifies the password that the remote device must use when issuing the rbmode remote command to access the module's command interface remotely.
| Attribute | Description |
|---|---|
| format | up to 16-character string |
| default | none |
| access | get/set |
| save | yes |
Get example
> get sy r p
none
Set example
> set sy r p 123456
Success
sy s m
System Sleep Mode
Description
Sets the sleep mode to be entered by the Bluetooth Xpress module. See Power Management for more information.
| Attribute | Description |
|---|---|
| format | string enumeration |
| units |
'deep' = stop all active advertising and scanning operations when entering sleep mode
'radio' = continue all active advertising and scanning operations when entering sleep mode |
| default | 'deep' |
| access | get/set |
| save | yes |
Get example
> get sy s m
deep
Set example
> set sy s m radio
Success
sy u
System UUID
Description
Returns the hardware UUID of the module.
| Attribute | Description |
|---|---|
| format | 20-byte hex string |
| default | unique per device |
| access | get |
| save | n/a |
The first 8 digits of the UUID indicate the hardware revision, per the following table:
| UUID first 8 digits | Hardware version |
|---|---|
4C892A6A
|
BGX13P-V2 |
080447D0
|
BGX13S-V2 |
F65FD7F0
|
BGX13S-V3 |
Get example
> get sy u
4C892A6A68B925AC06E893B1D0CF5EFFFE828F33
Note:
In the above example, the hardware field value is
4C892A6A
which
indicates this device is BGX13P-V2.
sy v
System (firmware) Version
Description
Returns the Bluetooth Xpress firmware version.
| Attribute | Description |
|---|---|
| format | string |
| default | varies |
| access | get |
| save | n/a |
This is the variable equivalent of the ver command. Refer to the ver command for a description of the version fields.
Get example
> get sy v
BGX13.1.0.821.0-1229-821
sy w c
System Wake on CTS
Description
Enables/disables waking the device from sleep mode when a falling edge is detected on the UART CTS pin.
UART baud rate ( ua b ) must be greater than 9600 bps for the device to wake from sleep on a falling edge of CTS. If the baud rate is 9600 bps or less, the UART interface is operational in sleep mode, so CTS retains its normal function as a flow control signal and cannot be used as a wake pin. In this scenario, the user can issue the wake command ( wake ) to put the device into active mode.
See Power Management for more information on power modes.
| Attribute | Description |
|---|---|
| format | integer |
| units | 1=true/enabled, 0=false/disabled |
| min | 0 |
| max | 1 |
| default | 1 |
| access | get/set |
| save | yes |
Get example
> get sy w c
1
Set example
> set sy w c 0
Success
Test Mode
tm n p
Test Mode Number of Packets
Description
This variable reports the number of packets that were transmitted
or received between the
dtm start
and
dtm stop
commands. It is
set to 0 when
dtm start
runs and records total packets when
dtm stop
runs.
See Direct Test Mode (dtm) for more details.
| Attribute | Description |
|---|---|
| format | integer |
| units | count |
| min | 0 |
| max | 65535 |
| default | 0 |
| access | get |
| save | n/a |
Get example
> get tm n p
0
UART
ua b
UART Baud
Description
Sets the UART baud rate.
Note: The new data rate does not take effect until the user issues the uartu command.
| Attribute | Description |
|---|---|
| format | integer |
| units | bits per second |
| min | 0 |
| max | 2000000 |
| default | 115200 |
| access | get/set |
| save | yes |
Get example
> get ua b
115200
Set example
> set ua b 115200
Success
ua f
UART Flow control
Description
Turn on/off UART hardware flow control.
Note: The new flow control setting does not take effect until the user issues the uartu command.
| Attribute | Description |
|---|---|
| format | integer |
| units | 1=true/enabled, 0=false/disabled |
| min | 0 |
| max | 1 |
| default | 0 |
| access | get/set |
| save | yes |
Get example
> get ua f
1
Set example
> set ua f 0
Success
User Function
uf l p
User Function Long-Press Duration
Version Notes
Added in
1.2.2045.0
Description
Configures the minimum length of time a
ufu_level
pin configured to trigger a
hi_long
or
lo_long
user event (see
uevt
command) must
remain high (for
hi_long
) or low (for
lo_long
) in order for the event to be
seen as a long-press rather than a short-press.
| Attribute | Description |
|---|---|
| format | integer |
| units | 100 milliseconds |
| min | 1 (100 milliseconds) |
| max | 100 (10 seconds) |
| default | 20 (2 seconds) |
| access | get/set |
| save | yes |
Get example
> get uf l p
20
Set example
> set uf l p 30
Success
uf u
User Function Usage
Description
User functions and the events that trigger them are displayed using this read-only variable. This multi-line variable behaves similar to the gpio "gp u" variable.
| Attribute | Description |
|---|---|
| format | table list |
| access | get |
| save | n/a |
Get example
> get uf u
! # Description
# 0 lo,3 (con D0CF5E35E0D8 10)
# 1 hi,3 (dct)
# 2 none ()
# 3 none ()