BGXpressService

The Silicon Labs BGX device provides a bridge between Bluetooth Low Energy (BLE) and Serial communication. More...

Classes

enum com.silabs.bgxcommander.BGX_CONNECTION_STATUS
This enum is the Connection Status of the BGXpressService instance.
enum com.silabs.bgxcommander.OTA_Status
This is the OTA status that can be used to drive a user interface as part of the OTA_STATUS_MESSAGE.
class com.silabs.bgxcommander.BGXpressService
An intent service which is used to control and communicate with a BGX device. More...

Detailed Description

The Silicon Labs BGX device provides a bridge between Bluetooth Low Energy (BLE) and Serial communication.

BGXpressService is an Android Intent Service which makes it easier to write an Android app which interacts with BGX. It supports discovery of BGX devices, connecting and disconnecting, setting and detecting changes to the bus mode of the BGX, sending and receiving serial data, and OTA (Over The Air) Firmware Updates of the BGX accessed through the Silicon Labs DMS (Device Management Service).

Remarks
BGXpressService is designed to target Android SDK 27 and supports a minimum SDK version 23.
BGXpressService is currently designed for connecting to one BGX at a time.

Class Documentation

◆ com::silabs::bgxcommander::BGXpressService

class com::silabs::bgxcommander::BGXpressService

An intent service which is used to control and communicate with a BGX device.

Inherits IntentService.

Public Member Functions

BGXpressService ()
void onCreate ()
void onDestroy ()

Static Public Member Functions

static void startActionStartScan (Context context)
Starts this service to perform action Start Scan. More...
static void startActionStopScan (Context context)
Starts this service to perform action Stop Scan. More...
static void startActionBGXConnect (Context context, String deviceAddress)
startActionBGXConnect More...
static void startActionBGXCancelConnect (Context context)
startActionBGXCancelConnect More...
static void clearCancelFlag ()
clearCancelFlag More...
static void getBGXDeviceInfo (Context context)
getBGXDeviceInfo More...

Static Public Attributes

static final String ACTION_START_SCAN
The BGXpressService receives this intent and it begins scanning. More...
static final String ACTION_STOP_SCAN
The BGXpressService receives this intent and it stops scanning. More...
static final String ACTION_BGX_CONNECT
This is sent to cause the BGXpressService to connect to a BGX. More...
static final String ACTION_BGX_DISCONNECT
This is sent to cause the BGXpressService to disconnect from a connected BGX. More...
static final String ACTION_BGX_CANCEL_CONNECTION
Attempt to cancel an in-progress connection operation. More...
static final String ACTION_READ_BUS_MODE
Reads the bus mode. More...
static final String ACTION_WRITE_BUS_MODE
Writes the bus mode. More...
static final String ACTION_WRITE_SERIAL_DATA
Writes data to the BGX. More...
static final String ACTION_BGX_GET_INFO
This request causes the BGXpressService to read the device uuid and determine the part id. More...
static final String ACTION_DMS_GET_VERSIONS
Gets the firmware versions available from DMS. More...
static final String ACTION_DMS_REQUEST_VERSION
This request causes the specified DMS version to be loaded onto the phone. More...
static final String ACTION_OTA_WITH_IMAGE
image_path - String - path to the image file. More...
static final String ACTION_OTA_CANCEL
Attempts to cancel an OTA operation in progress. More...
static final String BGX_CONNECTION_STATUS_CHANGE
Extras: bgx-connection-status - a value from the BGX_CONNECTION_STATUS enum which is the new status. More...
static final String BGX_MODE_STATE_CHANGE
Broadcast Intent which indicates a state change in the bgxss mode. More...
static final String BGX_DATA_RECEIVED
Extras: data - String - contains the data that was received from the BGX. More...
static final String BGX_SCAN_MODE_CHANGE
This change is sent when scanning begins or ends. More...
static final String BGX_SCAN_DEVICE_DISCOVERED
This is sent as a broadcast intent when a BGX device is discovered during scanning. More...
static final String DMS_VERSION_LOADED
Notification that a specific version has been loaded and is attached to the intent as "file_path". More...
static final String OTA_STATUS_MESSAGE
This contains the following extras: ota_failed : boolean. More...
static final String BGX_DEVICE_INFO
This is sent when connection state becomes connected for the device. More...
static final String DMS_VERSIONS_AVAILABLE
Broadcast intent sent when the list of versions is retrieved from DMS. More...

Protected Member Functions

void onHandleIntent (Intent intent)

Constructor & Destructor Documentation

◆ BGXpressService()

com.silabs.bgxcommander.BGXpressService.BGXpressService ( )
inline

Member Function Documentation

◆ onCreate()

void com.silabs.bgxcommander.BGXpressService.onCreate ( )
inline

◆ onDestroy()

void com.silabs.bgxcommander.BGXpressService.onDestroy ( )
inline

◆ startActionStartScan()

static void com.silabs.bgxcommander.BGXpressService.startActionStartScan ( Context context )
inline static

Starts this service to perform action Start Scan.

If the service is already performing a task this action will be queued.

See also
IntentService

◆ startActionStopScan()

static void com.silabs.bgxcommander.BGXpressService.startActionStopScan ( Context context )
inline static

Starts this service to perform action Stop Scan.

If the service is already performing a task this action will be queued.

See also
IntentService

◆ startActionBGXConnect()

static void com.silabs.bgxcommander.BGXpressService.startActionBGXConnect ( Context context,
String deviceAddress
)
inline static

startActionBGXConnect

Attempt to connect to the specified device.

Parameters
context
deviceAddress the Bluetooth address of the device to which you wish to connect.

◆ startActionBGXCancelConnect()

static void com.silabs.bgxcommander.BGXpressService.startActionBGXCancelConnect ( Context context )
inline static

startActionBGXCancelConnect

Attempt to cancel an in-progress connection operation.

Parameters
context

◆ clearCancelFlag()

static void com.silabs.bgxcommander.BGXpressService.clearCancelFlag ( )
inline static

clearCancelFlag

Call this before initiating a connection in order to clear the connection cancel flag.

To Do: maybe we can clear this a better way (such as when the user calls connect?)

◆ getBGXDeviceInfo()

static void com.silabs.bgxcommander.BGXpressService.getBGXDeviceInfo ( Context context )
inline static

getBGXDeviceInfo

Starts an operation to get the device info which is the part id and the device uuid.

Parameters
context

◆ onHandleIntent()

void com.silabs.bgxcommander.BGXpressService.onHandleIntent ( Intent intent )
inline protected

Member Data Documentation

◆ ACTION_START_SCAN

final String com.silabs.bgxcommander.BGXpressService.ACTION_START_SCAN
static

The BGXpressService receives this intent and it begins scanning.

There is no need to directly send this. You can call startActionStartScan() instead.

◆ ACTION_STOP_SCAN

final String com.silabs.bgxcommander.BGXpressService.ACTION_STOP_SCAN
static

The BGXpressService receives this intent and it stops scanning.

There is no need to directly send this. You can call startActionStopScan() instead.

◆ ACTION_BGX_CONNECT

final String com.silabs.bgxcommander.BGXpressService.ACTION_BGX_CONNECT
static

This is sent to cause the BGXpressService to connect to a BGX.

Extras:

DeviceAddress - String - The bluetooth address of the device to which to connect.

There is no need to directly send this. You can call startActionBGXConnect() using the device address instead.

◆ ACTION_BGX_DISCONNECT

final String com.silabs.bgxcommander.BGXpressService.ACTION_BGX_DISCONNECT
static

This is sent to cause the BGXpressService to disconnect from a connected BGX.

TODO: Add a static method for this to send the intent.

◆ ACTION_BGX_CANCEL_CONNECTION

final String com.silabs.bgxcommander.BGXpressService.ACTION_BGX_CANCEL_CONNECTION
static

Attempt to cancel an in-progress connection operation.

There is no need to call this directly. Use startActionBGXCancelConnect() instead.

◆ ACTION_READ_BUS_MODE

final String com.silabs.bgxcommander.BGXpressService.ACTION_READ_BUS_MODE
static

Reads the bus mode.

When the read operation completes, a broadcast intent will be sent with the action BGX_MODE_STATE_CHANGE.

◆ ACTION_WRITE_BUS_MODE

final String com.silabs.bgxcommander.BGXpressService.ACTION_WRITE_BUS_MODE
static

Writes the bus mode.

The service will not send a notification to indicate that it succeeded at this time.

Extras: busmode - int - one of the values from BusMode : STREAM_MODE, LOCAL_COMMAND_MODE, or REMOTE_COMMAND_MODE.

◆ ACTION_WRITE_SERIAL_DATA

final String com.silabs.bgxcommander.BGXpressService.ACTION_WRITE_SERIAL_DATA
static

Writes data to the BGX.

value - String - the data to be written.

◆ ACTION_BGX_GET_INFO

final String com.silabs.bgxcommander.BGXpressService.ACTION_BGX_GET_INFO
static

This request causes the BGXpressService to read the device uuid and determine the part id.

The result is sent out as a broadcast intent BGX_DEVICE_INFO with the following extras: bgx-device-uuid - A string containing the device uuid. bgx-part-id - An enum value from BGXPartID .

◆ ACTION_DMS_GET_VERSIONS

final String com.silabs.bgxcommander.BGXpressService.ACTION_DMS_GET_VERSIONS
static

Gets the firmware versions available from DMS.

Extras: bgx-part-id - BGXPartID - one of the following values: BGX13S or BGX13P

◆ ACTION_DMS_REQUEST_VERSION

final String com.silabs.bgxcommander.BGXpressService.ACTION_DMS_REQUEST_VERSION
static

This request causes the specified DMS version to be loaded onto the phone.

When finished, the broadcast intent DMS_VERSION_LOADED is sent.

Extras: bgx-part-id - BGXPartID - one of the following values: BGX13S or BGX13P dms-version - String - the DMS version number you want to retrieve.

TO DO: Handle fail cases (e.g. specify a version number that doesn't exist as right now the calling app gets no reply.)

◆ ACTION_OTA_WITH_IMAGE

final String com.silabs.bgxcommander.BGXpressService.ACTION_OTA_WITH_IMAGE
static

image_path - String - path to the image file.

You could get this from a DMS_VERSION_LOADED broadcast intent.

◆ ACTION_OTA_CANCEL

final String com.silabs.bgxcommander.BGXpressService.ACTION_OTA_CANCEL
static

Attempts to cancel an OTA operation in progress.

If the cancellation is successful you will get an OTA_STATUS_MESSAGE where the ota_status is UserCanceled

◆ BGX_CONNECTION_STATUS_CHANGE

final String com.silabs.bgxcommander.BGXpressService.BGX_CONNECTION_STATUS_CHANGE
static

Extras: bgx-connection-status - a value from the BGX_CONNECTION_STATUS enum which is the new status.

device - a BluetoothDevice (not present for DISCONNECTED).

◆ BGX_MODE_STATE_CHANGE

final String com.silabs.bgxcommander.BGXpressService.BGX_MODE_STATE_CHANGE
static

Broadcast Intent which indicates a state change in the bgxss mode.

Extras: busmode - int - one of the values from BusMode : STREAM_MODE, LOCAL_COMMAND_MODE, or REMOTE_COMMAND_MODE.

◆ BGX_DATA_RECEIVED

final String com.silabs.bgxcommander.BGXpressService.BGX_DATA_RECEIVED
static

Extras: data - String - contains the data that was received from the BGX.

◆ BGX_SCAN_MODE_CHANGE

final String com.silabs.bgxcommander.BGXpressService.BGX_SCAN_MODE_CHANGE
static

This change is sent when scanning begins or ends.

It has one extra.

isscanning - boolean - indicates whether scanning is happening.

◆ BGX_SCAN_DEVICE_DISCOVERED

final String com.silabs.bgxcommander.BGXpressService.BGX_SCAN_DEVICE_DISCOVERED
static

This is sent as a broadcast intent when a BGX device is discovered during scanning.

◆ DMS_VERSION_LOADED

final String com.silabs.bgxcommander.BGXpressService.DMS_VERSION_LOADED
static

Notification that a specific version has been loaded and is attached to the intent as "file_path".

file_path - string of the path to the file containing the version.

◆ OTA_STATUS_MESSAGE

final String com.silabs.bgxcommander.BGXpressService.OTA_STATUS_MESSAGE
static

This contains the following extras: ota_failed : boolean.

True means it failed. Use false as the default. ota_status : OTA_Status enum. Tells the current status of the ota. Use Invalid as the default. bytes_sent : int - number of bytes transfered in the firmware image. Not always present.

◆ BGX_DEVICE_INFO

final String com.silabs.bgxcommander.BGXpressService.BGX_DEVICE_INFO
static

This is sent when connection state becomes connected for the device.

param: bgx-device-uuid - a String param: bgx-part-id - a BGXPartID

◆ DMS_VERSIONS_AVAILABLE

final String com.silabs.bgxcommander.BGXpressService.DMS_VERSIONS_AVAILABLE
static

Broadcast intent sent when the list of versions is retrieved from DMS.

Extras: versions-available-json - String - Contains JSON response from DMS with the list of firmware versions available.