BGXpress Service Usage
Using BGXpressService
Adding BGXpressService to your Android project
To use the BGXpressService in your Android app, follow these steps:
- Add the files BGXpressService.java and BusMode.java into your Android app.
-
Declare the BGXpressService in your AndroidManifest.xml file like this:
<service android:name=".BGXpressService" android:exported="false"> <meta-data android:name="DMS_API_KEY" android:value="<YOUR DMS API KEY HERE>"/> </service> -
If you do not yet have a
DMS_API_KEY, supply an empty string for now. -
Add the following declarations to your AndroidManifest.xml file:
<uses-feature android:name="android.hardware.bluetooth_le" android:required="true" /> <uses-permission android:name="android.permission.BLUETOOTH" /> <uses-permission android:name="android.permission.BLUETOOTH_ADMIN" /> <uses-permission android:name="android.permission.ACCESS_FINE_LOCATION" /> <uses-permission android:name="android.permission.ACCESS_COARSE_LOCATION" /> <uses-permission android:name="android.permission.INTERNET" /> <uses-permission android:name="android.permission.ACCESS_NETWORK_STATE" />
Setup Bluetooth in your main activty
In the onCreate method of the main activity of your app, you will need to perform the following operations:
-
Verify the system supports Bluetooth Low Energy:
getPackageManager().hasSystemFeature(PackageManager.FEATURE_BLUETOOTH_LE) -
Request permission to access device location (this is required in order to use BLE):
requestPermissions(new String[]{Manifest.permission.ACCESS_COARSE_LOCATION}, PERMISSION_REQUEST_COARSE_LOCATION); -
Start the BGXpressService:
startService(new Intent(this, BGXpressService.class));
You should register a BroadcastReceiver to receive broadcast intents for the following:
BGXpressService.BGX_SCAN_DEVICE_DISCOVERED
,
BGXpressService.BGX_CONNECTION_STATUS_CHANGE
, and
BGXpressService.BGX_SCAN_MODE_CHANGE
.
Do not scan for devices until onRequestPermissionsResult is called by the operating system to grant permission to access the device location.
In your onResume() method if you have been granted permission to acccess the device location and BluetoothAdapter.getDefaultAdapter() is not null, check to see if the default adapter is enabled by calling
BluetoothAdapter.getDefaultAdapter().isEnabled()
. If it is not enabled then create an Intent for
BluetoothAdapter.ACTION_REQUEST_ENABLE
and start an activity wth this Intent.
Device Discovery
When three conditions have been met: you determine the system supports Bluetooth Low Energy, onRequestPermissionsResult was called indicating you were granted permission to use the device location, and the default bluetooth adapter is enabled, then you can scan for BGX devices by calling:
`BGXpressService.startActionStartScan(Context)`
You will receive broadcast intents in your broadcast receiver with the action
BGXpressService.BGX_SCAN_DEVICE_DISCOVERED
as devices are discovered. This intent will contain an Extra which is a HashMap<String, String> containing the keys
name
,
uuid
, and
rssi
. The
name
key is the device name, the
uuid
key is the device uuid which you will use to connect to the device, and
rssi
contains the signal strength of the device.
Connecting to a BGX
To connect to a device, call
BGXpressService.startActionBGXConnect(context, deviceUUID)
where deviceUUID is the uuid you were given in the HashMap for the device. The app will receive broadcast intents of type
BGXpressService.BGX_CONNECTION_STATUS_CHANGE
as the connection occurs.
When the
bgx-connection-status
extra inside the
BGXpressService.BGX_CONNECTION_STATUS_CHANGE
Intent is
CONNECTED
, the device is connected.
Detecting device Changes
You should register to receive broadcast intents for the following actions:
| Action | Purpose | Extras |
|---|---|---|
BGXpressService.BGX_MODE_STATE_CHANGE
|
Indicates BusMode has been read or has changed | busmode |
BGXpressService.BGX_DATA_RECEIVED
|
Indicates data has been received | data |
BGXpressService.BGX_DEVICE_INFO
|
Contains information about the BGX which is needed for DMS/OTA | bgx-device-uuid, bgx-part-id |
Read/Write Serial data
When data is received from a connected BGX, the BGXpressService will send a broadcast intent of type BGXpressService.BGX_DATA_RECEIVED containing the data. To write data to the connected BGX, send a
BGXpressService.ACTION_WRITE_SERIAL_DATA
Intent like this:
Intent writeIntent = new Intent(BGXpressService.ACTION_WRITE_SERIAL_DATA);
writeIntent.putExtra("value", text2send);
writeIntent.setClass(mContext, BGXpressService.class);
startService(writeIntent);
Bus Mode
To change the BusMode, use the following method to send an Intent to BGXpressService:
Intent intent = new Intent(BGXpressService.ACTION_WRITE_BUS_MODE);
intent.setClass(this, BGXpressService.class);
intent.putExtra("busmode", busMode);
startService(intent);
Changes to the BusMode will be indicated by receiving a broadcast intent with the action
BGXpressService.BGX_MODE_STATE_CHANGE
containing the extra
busmode
.
Disconnecting from a BGX
To disconnect from the connected BGX:
Intent intent = new Intent(BGXpressService.ACTION_BGX_DISCONNECT); intent.setClass(mContext, BGXpressService.class); startService(intent);
When the BGX is disconnected, you will receive a broadcast Intent with the action
BGXpressService.BGX_CONNECTION_STATUS_CHANGE
where the
bgx-connection-status
will have the value DISCONNECTED.
Get available firmware using DMS
To request the list of available firmware, send the following Intent:
Intent intent = new Intent(BGXpressService.ACTION_DMS_GET_VERSIONS);
intent.setClass(this, BGXpressService.class);
intent.putExtra("bgx-part-id", mBGXPartID);
startService(intent);
When the list has been retrieved you will receive a broadcast intent with the action
BGXpressService.DMS_VERSIONS_AVAILABLE
which contains the list in the form of JSON under the extra
versions-available-json
. The JSON will parse into an array containing firmware version records with the following keys:
| key | type |
|---|---|
| version | string |
| tag | string (may be empty) |
| size | int (number of bytes) |
Get firmware image using DMS
To request a specific version of firmware be loaded, the following Intent should be sent:
Intent intent = new Intent(BGXpressService.ACTION_DMS_REQUEST_VERSION);
intent.putExtra("bgx-part-id", bgx_part_id); // This is the part ID that was provided in the BGXpressService.BGX_DEVICE_INFO intent as the extra *bgx-partd-id*
intent.putExtra("dms-version", dms_version); // This is the DMS version provided in the *version* field of the JSON record.
intent.setClass(mContext, BGXpressService.class);
When the firmware image is loaded onto your mobile device, you will receive a broadcast intent with the action
BGXpressService.DMS_VERSION_LOADED
containing an extra called
file_path
.
Updating a BGX using a firmware image
To install a firmware image onto the connected BGX, send the following Intent:
Intent updateIntent = new Intent(mContext, BGXpressService.class);
updateIntent.setAction(ACTION_OTA_WITH_IMAGE);
updateIntent.putExtra("image_path", firmwareImageFilePath);
startService(updateIntent);
As the update installs, you will receive a series of broadcast intents with the action
BGXpressService.OTA_STATUS_MESSAGE
with the following Extras:
| Extra | Type | Default Value | Meaning |
|---|---|---|---|
| ota_failed | boolean | false | If this value is true, it means that the OTA failed. |
| ota_status | OTA_STATUS | n/a | This is an enum indicating the status of the OTA. The values are described in the table below. |
| bytes_sent | int | -1 | Indicates the number of bytes that has been uploaded to the BGX device. This is only present when the OTA status is Installing. |
Canceling an OTA Update
To cancel an OTA Update in progress, send the following Intent:
Intent intent = new Intent(); intent.setAction(BGXpressService.ACTION_OTA_CANCEL); intent.setClass(mContext, BGXpressService.class); startService(intent);
OTA_Status Values
| OTA_Status Value | Meaning |
|---|---|
| Invalid | Should never see this. It indicates an error has occurred. |
| Idle | No OTA is happening |
| Downloading | The firmware image is being downloaded through DMS |
| Installing | The firmware iamge is being sent to the BGX device |
| Finishing | The firmware image has been written and the bgx is being commanded to load it |
| Finished | The BGX has acknowledged the command to load the firmware. The BGX is rebooting |
| UserCanceled | The intent ACTION_OTA_CACNCEL has been received and the OTA operation is being canceled |