Class List
Here are the classes, structs, unions and interfaces with brief descriptions:
| ▼ N com | |
| ▼ N silabs | |
| ▼ N bgxpress | |
| C BGX_CONNECTION_STATUS | The BGX_CONNECTION_STATUS datatype describes the connection status of a BGX Device |
| ▼ C BGXpressService | An intent service which is used to control and communicate with a BGX device |
| C BGXPartID | Value that indicates the type of part |
| C DeviceProperties | |
| C ScanProperties | |
| C BusMode | BusMode determines how the BGX interprets data it receives |
| C OTA_Status | This is the OTA status that can be used to drive a user interface as part of the OTA_STATUS_MESSAGE |