BGXpressService
The Silicon Labs BGX device provides a bridge between Bluetooth Low Energy (BLE) and Serial communication. More...
Classes |
|
| class | com.silabs.bgxpress.BGXpressService |
|
An intent service which is used to control and communicate with a BGX device.
More...
|
|
Detailed Description
The Silicon Labs BGX device provides a bridge between Bluetooth Low Energy (BLE) and Serial communication.
BGXpressService is an Android Intent Service which makes it easier to write an Android app which interacts with BGX. It supports discovery of BGX devices, connecting and disconnecting, setting and detecting changes to the bus mode of the BGX, sending and receiving serial data, and OTA (Over The Air) Firmware Updates of the BGX accessed through the Silicon Labs DMS (Device Management Service).
- Remarks
- BGXpressService is designed to target Android SDK 27 and supports a minimum SDK version 23.
- BGXpressService is currently designed for connecting to one BGX at a time.
Class Documentation
◆ com::silabs::bgxpress::BGXpressService
| class com::silabs::bgxpress::BGXpressService |
An intent service which is used to control and communicate with a BGX device.
Inherits IntentService.
Public Member Functions |
|
| BGXpressService () | |
| void | onCreate () |
| void | onDestroy () |
Static Public Member Functions |
|
| static void | startActionStartScan (Context context) |
|
Starts this service to perform action Start Scan.
More...
|
|
| static void | startActionStopScan (Context context) |
|
Starts this service to perform action Stop Scan.
More...
|
|
| static void | startActionBGXConnect (Context context, String deviceAddress) |
|
startActionBGXConnect
More...
|
|
| static void | startActionBGXCancelConnect (Context context, String deviceAddress) |
|
startActionBGXCancelConnect
More...
|
|
| static void | startActionBGXDisconnect (Context context, String deviceAddress) |
|
startActionBGXDisconnect
More...
|
|
| static void | getBGXDeviceInfo (Context context, String deviceAddress) |
|
getBGXDeviceInfo
More...
|
|
| static boolean | setBGXAcknowledgedWrites (String deviceAddress, boolean acknowledgedWrites) |
| static boolean | setBGXAcknowledgedReads (String deviceAddress, boolean acknowledgedReads) |
| static BGX_CONNECTION_STATUS | getBGXDeviceConnectionStatus (String deviceAddress) |
| static Integer | getBGXBootloaderVersion (String deviceAddress) |
|
getBGXBootloaderVersion
More...
|
|
| static String | getFirmwareRevision (String deviceAddress) |
|
getFirmwareRevision
More...
|
|
Static Public Attributes |
|
| static final String | ACTION_START_SCAN |
|
The
BGXpressService
receives this intent and it begins scanning.
More...
|
|
| static final String | ACTION_STOP_SCAN |
|
The
BGXpressService
receives this intent and it stops scanning.
More...
|
|
| static final String | ACTION_BGX_CONNECT |
|
This is sent to cause the
BGXpressService
to connect to a BGX.
More...
|
|
| static final String | ACTION_BGX_DISCONNECT |
|
This is sent to cause the
BGXpressService
to disconnect from a connected BGX.
More...
|
|
| static final String | ACTION_BGX_CANCEL_CONNECTION |
|
Attempt to cancel an in-progress connection operation.
More...
|
|
| static final String | ACTION_READ_BUS_MODE |
|
Reads the bus mode.
More...
|
|
| static final String | ACTION_WRITE_BUS_MODE |
|
Writes the bus mode.
More...
|
|
| static final String | ACTION_WRITE_SERIAL_DATA |
|
Writes data to the BGX.
More...
|
|
| static final String | ACTION_WRITE_SERIAL_BIN_DATA |
|
Writes byte data to the BGX.
More...
|
|
| static final String | ACTION_DMS_GET_VERSIONS |
|
Gets the firmware versions available from DMS.
More...
|
|
| static final String | ACTION_DMS_REQUEST_VERSION |
|
This request causes the specified DMS version to be loaded onto the phone.
More...
|
|
| static final String | ACTION_OTA_WITH_IMAGE |
|
Extras: image_path - String - path to the image file.
More...
|
|
| static final String | ACTION_OTA_CANCEL |
|
Attempts to cancel an OTA operation in progress.
More...
|
|
| static final String | BGX_CONNECTION_STATUS_CHANGE |
|
Extras: bgx-connection-status - a value from the
BGX_CONNECTION_STATUS
enum which is the new status.
More...
|
|
| static final String | BGX_MODE_STATE_CHANGE |
|
Broadcast Intent which indicates a state change in the bgxss mode.
More...
|
|
| static final String | BUS_MODE_ERROR_PASSWORD_REQUIRED |
|
This intent is sent when a password is required to change the bus mode to remote command mode.
More...
|
|
| static final String | BGX_DATA_RECEIVED |
|
Extras: data - String - contains the data that was received from the BGX.
More...
|
|
| static final String | BGX_SCAN_MODE_CHANGE |
|
This change is sent when scanning begins or ends.
More...
|
|
| static final String | BGX_MTU_CHANGE |
|
BGX_MTU_CHANGE.
More...
|
|
| static final String | BGX_SCAN_DEVICE_DISCOVERED |
|
This is sent as a broadcast intent when a BGX device is discovered during scanning.
More...
|
|
| static final String | DMS_VERSION_LOADED |
|
Notification that a specific version has been loaded and is attached to the intent as "file_path".
More...
|
|
| static final String | OTA_STATUS_MESSAGE |
|
This contains the following extras: ota_failed : boolean.
More...
|
|
| static final String | BGX_INVALID_GATT_HANDLES |
|
Notification message that is sent when invalid GATT handles are detected.
More...
|
|
| static final String | BGX_DEVICE_INFO |
|
This is sent when connection state becomes connected for the device.
More...
|
|
| static final String | BGX_CONNECTION_ERROR |
|
This is sent when the BGXConnectionState moves from Connecting to Disconnecting due to an error.
More...
|
|
| static final String | DMS_VERSIONS_AVAILABLE |
|
Broadcast intent sent when the list of versions is retrieved from DMS.
More...
|
|
| static Handler | mHandler |
Protected Member Functions |
|
| void | onHandleIntent (Intent intent) |
Constructor & Destructor Documentation
◆ BGXpressService()
|
inline |
Member Function Documentation
◆ onCreate()
|
inline |
◆ onDestroy()
|
inline |
◆ startActionStartScan()
|
inline static |
Starts this service to perform action Start Scan.
If the service is already performing a task this action will be queued.
- Parameters
-
contextInterface to global information about an Android application environment.
- See also
- IntentService
◆ startActionStopScan()
|
inline static |
Starts this service to perform action Stop Scan.
If the service is already performing a task this action will be queued.
- Parameters
-
contextInterface to global information about an Android application environment.
- See also
- IntentService
◆ startActionBGXConnect()
|
inline static |
startActionBGXConnect
Attempt to connect to the specified device. The process of the connection can be tracked by receiving a series of BGX_CONNECTION_STATUS_CHANGE intents.
- Parameters
-
contextInterface to global information about an Android application environment. deviceAddressthe Bluetooth address of the device to which to connect.
◆ startActionBGXCancelConnect()
|
inline static |
startActionBGXCancelConnect
Attempt to cancel an in-progress connection operation.
- Parameters
-
contextInterface to global information about an Android application environment. deviceAddressThe Bluetooth address of the device to which to cancel the connection in progress.
◆ startActionBGXDisconnect()
|
inline static |
startActionBGXDisconnect
Disconnect a BGX Device.
- Parameters
-
contextInterface to global information about an Android application environment. deviceAddressthe Bluetooth address of the device to which you wish to connect.
◆ getBGXDeviceInfo()
|
inline static |
getBGXDeviceInfo
Starts an operation to get the device info which is the part id and the device uuid.
- Parameters
-
contextInterface to global information about an Android application environment. deviceAddressThe device to which the operation pertains.
◆ setBGXAcknowledgedWrites()
|
inline static |
◆ setBGXAcknowledgedReads()
|
inline static |
◆ getBGXDeviceConnectionStatus()
|
inline static |
◆ getBGXBootloaderVersion()
|
inline static |
getBGXBootloaderVersion
Gets the BGXBootloader version if possible to do so. This value is available only after the device is connected.
- Parameters
-
deviceAddressAddress of the device to retrieve the bootloader version
- Returns
- -1 on error, or the bootloader version (a positive integer).
◆ getFirmwareRevision()
|
inline static |
getFirmwareRevision
- Parameters
-
deviceAddressAddress of the device to retrieve the firmware revision
- Returns
- String containing the firmware version if available, otherwise NULL.
◆ onHandleIntent()
|
inline protected |
Member Data Documentation
◆ ACTION_START_SCAN
|
static |
The BGXpressService receives this intent and it begins scanning.
There is no need to directly send this. You can call startActionStartScan() instead.
◆ ACTION_STOP_SCAN
|
static |
The BGXpressService receives this intent and it stops scanning.
There is no need to directly send this. You can call startActionStopScan() instead.
◆ ACTION_BGX_CONNECT
|
static |
This is sent to cause the BGXpressService to connect to a BGX.
Extras:
DeviceAddress - String - The bluetooth address of the device to which to connect.
There is no need to directly send this. You can call startActionBGXConnect() using the device address instead.
◆ ACTION_BGX_DISCONNECT
|
static |
This is sent to cause the BGXpressService to disconnect from a connected BGX.
◆ ACTION_BGX_CANCEL_CONNECTION
|
static |
Attempt to cancel an in-progress connection operation.
There is no need to call this directly. Use startActionBGXCancelConnect() instead.
◆ ACTION_READ_BUS_MODE
|
static |
Reads the bus mode.
When the read operation completes, a broadcast intent will be sent with the action BGX_MODE_STATE_CHANGE.
◆ ACTION_WRITE_BUS_MODE
|
static |
Writes the bus mode.
The service will not send a notification to indicate that it succeeded at this time.
Extras: busmode - int - one of the values from BusMode : STREAM_MODE, LOCAL_COMMAND_MODE, or REMOTE_COMMAND_MODE. DeviceAddress - String the address of the device on which to set the bus mode. password - String - If supplied, this value will be used as the password for REMOTE_COMMAND_MODE
◆ ACTION_WRITE_SERIAL_DATA
|
static |
Writes data to the BGX.
value - String - the data to be written.
◆ ACTION_WRITE_SERIAL_BIN_DATA
|
static |
Writes byte data to the BGX.
value - byte [] - the byte array to be written.
◆ ACTION_DMS_GET_VERSIONS
|
static |
Gets the firmware versions available from DMS.
Either bgx-part-id or bgx-part-identifier (preferred) must be specified. bgx-part-identifier is used if both are specified.
Extras: bgx-part-id - An enum value from BGXPartID . Preserved for compatibility. bgx-part-identifier - an 8 character string identifying the type of BGX (preferred).
◆ ACTION_DMS_REQUEST_VERSION
|
static |
This request causes the specified DMS version to be loaded onto the phone.
When finished, the broadcast intent DMS_VERSION_LOADED is sent. Either bgx-part-id or bgx-part-identifier (preferred) must be specified. bgx-part-identifier is used if both are specified.
Extras: bgx-part-id - BGXPartID - Optional one of the following values: BGX13S or BGX13P (Preserved for compatibility) bgx-part-identifier - String - an 8 character string identifying the kind of BGX (Preferred) dms-version - String - the DMS version number you want to retrieve.
◆ ACTION_OTA_WITH_IMAGE
|
static |
Extras: image_path - String - path to the image file.
You could get this from a DMS_VERSION_LOADED broadcast intent. DeviceAddress - String - The address of the device to update. password - String - the password to use for the OTA update if one is set.
◆ ACTION_OTA_CANCEL
|
static |
Attempts to cancel an OTA operation in progress.
If the cancellation is successful you will get an OTA_STATUS_MESSAGE where the ota_status is UserCanceled
◆ BGX_CONNECTION_STATUS_CHANGE
|
static |
Extras: bgx-connection-status - a value from the BGX_CONNECTION_STATUS enum which is the new status.
device - a BluetoothDevice (not present for DISCONNECTED). DeviceAddress - address of the BGX.
◆ BGX_MODE_STATE_CHANGE
|
static |
Broadcast Intent which indicates a state change in the bgxss mode.
Extras: busmode - int - one of the values from BusMode : STREAM_MODE, LOCAL_COMMAND_MODE, or REMOTE_COMMAND_MODE.
◆ BUS_MODE_ERROR_PASSWORD_REQUIRED
|
static |
This intent is sent when a password is required to change the bus mode to remote command mode.
This contains the following extras: DeviceAddress : the address of the device.
◆ BGX_DATA_RECEIVED
|
static |
Extras: data - String - contains the data that was received from the BGX.
DeviceAddress - string - the address of the BGX that received data.
◆ BGX_SCAN_MODE_CHANGE
|
static |
This change is sent when scanning begins or ends.
It has one extra.
isscanning - boolean - indicates whether scanning is happening.
◆ BGX_MTU_CHANGE
|
static |
BGX_MTU_CHANGE.
- Parameters
-
deviceAddressdevice address statusoperation status mtuthe new mtu size
◆ BGX_SCAN_DEVICE_DISCOVERED
|
static |
This is sent as a broadcast intent when a BGX device is discovered during scanning.
- Parameters
-
DeviceRecorda HashMap containing information about the device that was discovered. The HashMap contains the following keys: name - Device name uuid - Device address rssi - the device's current RSSI.
◆ DMS_VERSION_LOADED
|
static |
Notification that a specific version has been loaded and is attached to the intent as "file_path".
file_path - string of the path to the file containing the version.
◆ OTA_STATUS_MESSAGE
|
static |
This contains the following extras: ota_failed : boolean.
True means it failed. Use false as the default. ota_status : OTA_Status enum. Tells the current status of the OTA. Use Invalid as the default. bytes_sent : int - number of bytes transfered in the firmware image. Not always present.
◆ BGX_INVALID_GATT_HANDLES
|
static |
Notification message that is sent when invalid GATT handles are detected.
Invalid GATT handles result in operations failing to work correctly. Invalid GATT handles occur as a result of a firmware update that adds or removes Bluetooth characteristics and/or services to the BGX when you have an existing bond on your Android device. To fix this condition, you would need to go to the Bluetooth Settings on your Android device, select the BGX, and choose "Forget". The next time you connect, the bond will be reestablished. This broadcast intent will be sent when the BGXpressService is unable to read a valid part id or when it is unable to read a valid firmware version. Your app should respond to this broadcast intent by showing the user a message explaining the situation and telling them how to recover from it.
This broadcast intent contains the following extras: DeviceAddress: String - The address of the BGX device. DeviceName: String - The name of the BGX device.
◆ BGX_DEVICE_INFO
|
static |
This is sent when connection state becomes connected for the device.
param: bgx-device-uuid - a String param: bgx-part-id - a BGXPartID param: bgx-part-identifier - an 8 character String that identifies the type of BGX.
◆ BGX_CONNECTION_ERROR
|
static |
This is sent when the BGXConnectionState moves from Connecting to Disconnecting due to an error.
param: status - a GATT Status value as returned by the Android GATT API.
◆ DMS_VERSIONS_AVAILABLE
|
static |
Broadcast intent sent when the list of versions is retrieved from DMS.
Extras: versions-available-json - String - Contains JSON response from DMS with the list of firmware versions available.
◆ mHandler
|
static |