The
BGXDevice
class is used to represent the BGX device.
More...
The
BGXDevice
class is used to represent the BGX device.
It contains a group of properties as well as methods used to perform appropriate actions on a
BGXDevice
.
Supports two delegates, deviceDelegate and serialDelegate, as well as KVO.
◆
BGXSerialDelegate-p
|
protocol BGXSerialDelegate-p
|
BGXSerialDelegate
protocol.
The
BGXSerialDelegate
is used to perform serial read/write operations with the BGX.
◆
busModeChanged:forDevice:()
|
- (void) busModeChanged:
|
|
(
BusMode
)
|
newBusMode
|
|
forDevice:
|
|
(
BGXDevice
*)
|
device
|
|
|
|
|
|
|
required
|
Detect bus mode changes.
Delegate method called when the bus mode changes or is read. If you call the BGXpressManager method -(BOOL)readBusMode, this delegate will be called with the bus mode that was read whether or not it was different than the previous bus mode.
-
Parameters
-
newBusMode
|
the new bus mode for the connection
|
◆
dataRead:forDevice:()
|
- (void) dataRead:
|
|
(NSData *)
|
newData
|
|
forDevice:
|
|
(
BGXDevice
*)
|
device
|
|
|
|
|
|
|
required
|
Delegate method is called when data is received.
-
Parameters
-
◆
dataWrittenForDevice:()
|
- (void) dataWrittenForDevice:
|
|
(
BGXDevice
*)
|
device
|
|
|
required
|
Delegate method used to advise that the data has been written.
◆
BGXDeviceDelegate-p
|
protocol BGXDeviceDelegate-p
|
BGXDeviceDelegate
protocol is used to be notified of state changes and device-level events.
◆
connectionTimeoutForDevice:()
|
- (void) connectionTimeoutForDevice:
|
|
(
BGXDevice
*)
|
device
|
|
|
optional
|
The device was connecting but the connection operation failed to finish within the timeout period.
The device is probably disconnected as a result.
-
Parameters
-
device
|
The device whose connection timed out.
|
◆
stateChangedForDevice:()
|
- (void) stateChangedForDevice:
|
|
(
BGXDevice
*)
|
device
|
|
|
optional
|
The value of the deviceState variable changed.
This could mean that the device connected, disconnected, and so on. The typical flow is: Connect operation: Disconnected -> Connecting -> Interrogating -> Connected.
Disconnect operation: Connected -> Disconnecting -> Disconnected
-
Parameters
-
device
|
The device whose state changed.
|
◆
rssiChangedForDevice:()
|
- (void) rssiChangedForDevice:
|
|
(
BGXDevice
*)
|
device
|
|
|
optional
|
The RSSI value changed for the device.
-
Parameters
-
device
|
The device for which the RSSI changed.
|
◆
BGXDevice
Inherits NSObject, and <CBPeripheralDelegate>.
◆
connect()
Method to connect to the device.
Operation happens asynchronously. Observe the deviceState property to determine the outcome of the operation.
-
Returns
-
BOOL value to indicate if the connection operation started successfully.
◆
disconnect()
Method to disconnect to the device.
Operation happens asynchronously. Observe the deviceState property to determine the outcome of the operation.
-
Returns
-
BOOL value to indicate if the disconnection operation started successfully.
◆
readBusMode()
Method used to read the BusMode for a device e.g., Stream, Local or Remote commands.
This operation occurs asynchronously. Observe the changes to the busMode property.
-
Returns
-
BOOL value, YES to indicate that the read operation could be initiated. NO if the read operation could not be started.
◆
writeBusMode:()
|
- (BOOL) writeBusMode:
|
|
(
BusMode
)
|
newBusMode
|
|
Deprecated
Use
writeBusMode: password: completionHandler:
instead.
Method used to write new bus mode for device. Operation occurs asynchronously.
-
Parameters
-
newBusMode
|
The new BusMode for the device
|
-
Returns
-
BOOL value, YES if BusMode write operation could be started.
◆
writeBusMode:password:completionHandler:()
Method used to write new bus mode for device.
Operation occurs asynchronously. You may get an error if the password you pass is wrong.
-
Parameters
-
newBusMode
|
The new BusMode for the device
|
password
|
The password for the bus mode characteristic. Pass nil for no password.
|
completionHandler
|
This will be called when the operation completes. You will get an error as a parameter to the completionHandler if the password is wrong or if you pass nil when a password is required.
|
◆
canWrite()
Method to see if you can write to the device.
-
Returns
-
BOOL value, YES if device is connected and no data waiting to be written to the device, else NO.
◆
writeData:()
|
- (BOOL) writeData:
|
|
(NSData *)
|
data
|
|
Method used to write data to a device.
-
Parameters
-
data
|
Data to be written to device.
|
-
Returns
-
BOOL value advising if the data has been written to the device or not.
◆
writeString:()
|
- (BOOL) writeString:
|
|
(NSString *)
|
string
|
|
Method used to write a string to device.
-
Parameters
-
string
|
String value to be written to device.
|
-
Returns
-
BOOL value advising if the string has been written to the device or not.
◆
sendCommand:args:()
|
- (BOOL) sendCommand:
|
|
(NSString *)
|
command
|
|
args:
|
|
(NSString *)
|
args
|
|
|
|
|
|
Method used to send commands to the device.
-
Parameters
-
command
|
Command
|
args
|
Arguments
|
-
Returns
-
BOOL value advising if the command has been written to the device or not.
◆
device_unique_id()
|
- (nullable NSString *) device_unique_id
|
|
|
|
Returns the device unique id.
-
Returns
-
NSString with the unique id of the device. Nil on error.
◆
nameForDeviceState:()
Printable name for a device state value.
◆
peripheral()
|
- (CBPeripheral *) peripheral
|
|
|
|
Access to the CBPeripheral.
◆
_deviceState
◆
_busMode
◆
_writeWithResponse
|
- (BOOL) _writeWithResponse
|
|
protected
|
◆
deviceDelegate
|
|
read
write
nonatomic
weak
|
◆
serialDelegate
|
|
read
write
nonatomic
weak
|
◆
name
◆
rssi
◆
identifier
◆
deviceState
◆
busMode
◆
modelNumber
|
- (NSString*) modelNumber
|
|
read
write
nonatomic
strong
|
◆
firmwareRevision
|
- (NSString*) firmwareRevision
|
|
read
write
nonatomic
strong
|
◆
bootloaderVersion
|
- (NSString*) bootloaderVersion
|
|
read
write
nonatomic
strong
|
◆
fastAck
YES = The device supports fastAck and will operate in fastAck mode.
NO = The device does not support fastAck and will operate in legacy mode.
◆
writeWithResponse
|
- (BOOL) writeWithResponse
|
|
read
write
nonatomic
assign
|
YES = Writes occur using CBCharacteristicWriteWithResponse NO = Writes occur using CBCharacteristicWriteWithoutResponse = YES.
Note: If the device supports fastAck, writeWithoutResponse will always be used.
◆
busmode_write_completion_handler_t
|
typedef void(^ busmode_write_completion_handler_t) (
BGXDevice
*, NSError *err)
|
◆
DeviceState
DeviceState values.
|
Enumerator
|
|
Interrogating
|
The
BGXDevice
has connected and Bluetooth services and characteristics are being discovered.
|
|
Disconnected
|
The
BGXDevice
is not connected (to this iOS device).
|
|
Connecting
|
The
BGXDevice
is in the process of connecting.
|
|
Connected
|
The
BGXDevice
is connected.
|
|
Disconnecting
|
The
BGXDevice
is in the process of disconnecting.
|
◆
BusMode
Values of the bus mode.
|
Enumerator
|
|
UNKNOWN_MODE
|
an invalid mode used to indicate that the
mode has not been determined
|
|
STREAM_MODE
|
send and receive serial data to the device to
which the BGX is connected
|
|
LOCAL_COMMAND_MODE
|
data received over the serial lines is
processed as a command by the BGX and results returned over the serial lines
|
|
REMOTE_COMMAND_MODE
|
data received over Bluetooth is processed as
a command by the BGX and results returned over Bluetooth
|
|
UNSUPPORTED_MODE
|
an invalid mode state
|