Class List

Here are the classes, structs, unions and interfaces with brief descriptions:
▼ N com
▼ N silabs
▼ N bgxpress
C BGX_CONNECTION_STATUS The BGX_CONNECTION_STATUS datatype describes the connection status of a BGX Device
▼ C BGXpressService An intent service which is used to control and communicate with a BGX device
C BGXPartID Value that indicates the type of part
C DeviceProperties
C ScanProperties
C BusMode BusMode determines how the BGX interprets data it receives
C OTA_Status This is the OTA status that can be used to drive a user interface as part of the OTA_STATUS_MESSAGE