BGXpressScanner

BGXpressScanner is used to detect changes to the Bluetooth hardware and scan for devices. More...

Classes

protocol <BGXpressScanDelegate >
A protocol for keeping track of goings on with your BGXpressScanner . More...
class BGXpressScanner

Enumerations

enum ScanState : NSUInteger { CantScan , Idle , Scanning }

Detailed Description

BGXpressScanner is used to detect changes to the Bluetooth hardware and scan for devices.

It also contains a list of devices.

It has a delegate property using the BGXpressScanDelegate protocol.


Class Documentation

◆ BGXpressScanDelegate -p

protocol BGXpressScanDelegate -p

A protocol for keeping track of goings on with your BGXpressScanner .

Inherits <NSObject>.

Instance Methods

(void) - bluetoothStateChanged:
bluetoothStateChanged This is called to indicate that system state of Bluetooth changed. More...
(void) - deviceDiscovered:
This is called to indicate that the scanner has found a device. More...
(void) - scanStateChanged:
This method is called when the scanState has changed. More...

Method Documentation

◆ bluetoothStateChanged:()

- (void BGXpressScanDelegate) bluetoothStateChanged: (CBManagerState) state
optional

bluetoothStateChanged This is called to indicate that system state of Bluetooth changed.

◆ deviceDiscovered:()

- (void BGXpressScanDelegate) deviceDiscovered: ( BGXDevice *) device
optional

This is called to indicate that the scanner has found a device.

You can access each device as its discovered (via the parameter) or access them all using the devicesDiscovered property which is an array of BGXDevice objects.

◆ scanStateChanged:()

- (void BGXpressScanDelegate) scanStateChanged: ( ScanState ) scanState
optional

This method is called when the scanState has changed.

◆ BGXpressScanner

class BGXpressScanner

Inherits NSObject, and <CBCentralManagerDelegate>.

Instance Methods

(BOOL) - startScan
Call this method to start scanning for devices. More...
(BOOL) - stopScan
Call this method to stop scanning for devices. More...

Protected Attributes

ScanState _scanState

Properties

NSObject< BGXpressScanDelegate > * delegate
Assign this property to be your scan delegate. More...
NSMutableArray * devicesDiscovered
This is an array of BGXDevice objects discovered by the scanner. More...
ScanState scanState
The current state of the scanner. More...

Method Documentation

◆ startScan()

- (BOOL) startScan

Call this method to start scanning for devices.

Returns
Boolean value to indicate if scanning will start.
Remarks
Calling this method will clear the contents of the devicesDiscovered mutable array property.

◆ stopScan()

- (BOOL) stopScan

Call this method to stop scanning for devices.

Returns
Boolean value to indicate if scanning will stop.

Member Data Documentation

◆ _scanState

- ( ScanState ) _scanState
protected

Property Documentation

◆ delegate

- (NSObject<BGXpressScanDelegate>*) delegate
read write nonatomic strong

Assign this property to be your scan delegate.

◆ devicesDiscovered

- (NSMutableArray*) devicesDiscovered
read write nonatomic strong

This is an array of BGXDevice objects discovered by the scanner.

This property will be made read only and immutable in the future.

◆ scanState

- ( ScanState ) scanState
read nonatomic assign

The current state of the scanner.

Enumeration Type Documentation

◆ ScanState

enum ScanState : NSUInteger
Enumerator
CantScan

Scanning cannot occur. Calls to startScan will fail. Wait for Bluetooth to be enabled.

Idle

Not currently scanning.

Scanning

Currently scanning.