Controlling GPIOs and LEDs
This example demonstrates how to use GPIOs with Gecko OS in general, and how to use GPIOs to control LEDs on Silabs evaluation boards. For details of using GPIOs and peripherals, see Peripherals.
When a GPIO is configured with an alternative function, the standard IO function is NOT available and the gpio_dir, gpio_set, and gpio_get commands are disabled for that GPIO.
Before a GPIO can be used to control an LED, it is necessary to first check whether the GPIO is being used for an alternative function.
If a GPIO is not being used for an alternative function, but is already in use as a standard GPIO (for another purpose), the GPIO must first be freed up by setting the direction of the GPIO to none
using the gpio_dir command.
GPIO Usage
The gpio.usage variable makes it easy to get a list of GPIOs that are already in use. For example:
Gecko OS Session |
---|
|
LED Control
The following example is based on a setup that only has two LEDs connected to GPIO 21 & 22. These LEDs are factory configured as system indicators to dynamically indicate the state of the Wi-Fi and network connection (as shown in the table above). To repurpose the GPIOs as standard IOs for use with LEDs, try the Gecko OS command sequence shown in the table below.
Note! Don't forget to adjust the GPIO numbers to suit your specific board!
Gecko OS Commands | Command Description |
---|---|
|
|
To re-instate the system indicators, either factory reset the module, or use the following commands.
Gecko OS Commands | Command Description |
---|---|
|
|
Supporting Gecko OS Editions and Versions
- Gecko-OS-2.0+
Change Log
Modified | Changes |
---|---|
2014-05-08 | Created |