Network
network.default_interface
Abbreviation
ne f
Access
get/set
Description
The default network interface used by various network commands and variables.
Commands:
Variables:
Arguments
<wlan/softap>
Default
wlan
Properties
Supported Platforms
- AMW007
- AMW037
Get example
> get ne f
R000006
wlan
Set example
> set ne f softap
R000008
Set OK
network.tls.ca_cert
Abbreviation
ne t a
Access
get/set
Description
The default CA TLS certificate used with TLS network streams.
Note
: PEM file format requires Unix format line termination: LF (\n), not Windows format: CR-LF (\r\n). Some terminal applications may append unwanted end-of-line characters. Incorrect line termination may result in TLS connection failure.
Arguments
<CA TLS cert filename>
Default
geotrust_ca.pem
Properties
- available in Safe Mode
Supported Platforms
- AMW007
- AMW037
Get example
> get ne t a
R000017
geotrust_ca.pem
Set example
> set ne t a globalsign_ca.pem
R000008
Set OK
network.tls.client_cert
Abbreviation
ne t c
Access
get/set
Description
The filename of the TLS client cert.
Arguments
<TLS cert filename>
Default
null
Properties
Supported Platforms
- AMW007
- AMW037
Get example
> get ne t c
Set example
> set ne t c client_cert.pem
R000008
Set OK
network.tls.client_key
Abbreviation
ne t k
Access
get/set
Description
The filename of the TLS client cert key.
Arguments
<TLS cert key filename>
Default
null
Properties
Supported Platforms
- AMW007
- AMW037
Get example
> get ne t k
Set example
> set ne t k client_cert_key_filename
R000008
Set OK
network.tls.handshake_timeout
Abbreviation
ne t h
Access
get/set
Description
This specifies the maximum amount of time in seconds between handshake packets to wait before aborting the connection.
Arguments
<seconds>
where:
-
: Range: 3-600
Default
15
Properties
- takes effect immediately
Get example
> get ne t h
15
Set example
> set ne t v 20
R000008
Set OK
network.tls.version
Abbreviation
ne t v
Access
get/set
Description
Specifies the maximum TLS version used. By default the client/server negotiates which TLS version/cipher to use but sometimes it is necessary to force a maximum version.
Arguments
<10/12>
where:
-
10: indicates TLS1.0 -
12: indicates TLS1.2
Default
12
Properties
Supported Platforms
- AMW007
- AMW037
Get example
> get ne t v
12
Set example
> set ne t v 10
R000008
Set OK