Update and Recovery
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. The framework provides a hardened bootloader, read/write file system, safemode recovery mechanism, and secure over-the-air (OTA) capability.
Secure Update
Silabs manages a secure online OTA server that offers each Gecko OS device the ability to securely update individual files, applications or an entire firmware bundle. The OTA command is used to update device firmware.
The OTA process is secured by industry standard TLS/HTTPS using server and client certificates that forces
- Gecko OS devices to verify the identity of the Silabs OTA server; and
- the Silabs OTA server to verify the identity of each individual Gecko OS device.
Each Gecko OS device is uniquely identified by a 128-bit hardware universally unique identifier (UUID).
HTTPS is the same security your web browser uses to make secure transactions with your bank over the internet. Silabs adds an additional layer of security, since the Silabs OTA server checks the unique security certificate and hardware UUID of each Gecko OS device that requests an update.
If an OTA update fails to complete for some reason, you can resume it later. Rejoin the network and run the ota command again.
The Gecko OS OTA feature uses the Silabs Device Management Server (DMS).
Note: To update from ZentriOS WL to Gecko OS, see Updating to Gecko OS.
The Silabs Device Management Server (DMS)
To update a Gecko OS device using Gecko OS, you need to sign up for an account with the Silabs Device Management Server (DMS) and then you need to claim your device.
You may also need to activate your device to a Gecko OS product.
The terms claim and activate are used in a special sense with the DMS, and are defined as follows.
- claim - associate a particular device with your user account.
- activate - associate a device with a product.
To perform Gecko OS OTA update, the steps are:
Signing up with the DMS
To sign up for an account with the DMS, go to the Silabs DMS Sign up page:
During the sign up process, you will create a DMS username and password.
Claim Your Device
To claim your device, issue the dms_claim command:
dms_claim <dms_username> <dms_password>
After you have claimed the device, future OTA update requests are directed to the Silabs Device Management Service.
Update Gecko OS Using OTA
Once the device is claimed, update to the latest version of your Gecko OS product by issuing the ota command..
Note: OTA requires a memory-intensive TLS connection, and may fail if memory is low. See Networking and Security, Increasing Available Memory for TLS.
If the ota command fails with the message:
{"result":"fail","message":"device not claimed"}
then you need to claim the device before running the ota command. See The Silabs DMS above.
The Gecko OS dms Command
When using Gecko OS, the dms_claim and dms_activatecommands are used to claim and activate devices:
- dms_claim - claim a device. Use
claim
to claim a device that is already running Gecko OS. - dms_activate - activate a product. Use
activate
to activate a device as a different product, such as a custom product you have created.
Activate a Product by Product Code
To activate a device to a specific product, use the dms_activate command.
dms_activate <product code>
To update the device to the latest published firmware bundle for the product:
ota
When issued with no arguments, the OTA command updates to the most recent firmware bundle version for the product, or does nothing if the device already has the most recent version installed.
Safe Mode
Safe mode operation is guaranteed in the unlikely event the device is configured in a way that causes repeated and/or unexpected reboots. The bootloader automatically switches to safe mode after eight exceptions occur with the offending boot application. Safe mode is indicated by the system.safemode.status variable.
It is easy to return the device to normal operation when the device is in safe mode. Follow the command sequence in the following table and your device will be back to normal in no time.
Gecko OS Commands | Description |
---|---|
|
|
In some cases, a misconfigured device may quickly return to safe mode since the device may be inadvertently setup to invoke a fault. If this occurs, we recommend the device is returned to factory reset.
Once in safe mode, the device boots into the kernel. The kernel provides the ability to update the firmware, or switch back to Gecko OS using the faults_reset
command.
For a detailed discussion of recovery procedures, see the Recovery from Safemode application note.
Commands and Variables Available in Safe Mode
In safe mode a subset of the commands and variables is available.
Safe Mode Commands
Safe Mode Variables
- bus.mode
- network.tls.ca_cert
- system.cmd.buffered
- system.cmd.echo
- system.cmd.header_enabled
- system.cmd.prompt_enabled
- system.print_level
- system.safemode.disabled
- system.safemode.status
- system.uuid
- system.version
- tcp.client.connect_timeout
- tcp.client.local_port
- tcp.client.retries
- tcp.client.retry_period
- uart.baud
- uart.data
- uart.flow
- uart.parity
- uart.stop
- wlan.dhcp.enabled
- wlan.hide_passkey
- wlan.join.retries
- wlan.join.timeout
- wlan.mac
- wlan.network.dns
- wlan.network.gateway
- wlan.network.ip
- wlan.network.netmask
- wlan.network.status
- wlan.passkey
- wlan.rate.protocol
- wlan.ssid
- wlan.static.dns
- wlan.static.gateway
- wlan.static.ip
- wlan.static.netmask
- wlan.tx_power
Factory Reset
Factory reset returns the device to a known state.
The device may be factory reset by GPIO or by the Gecko OS factory_reset command.
After a successful factory reset, all variables are set to factory defaults and the device reboots.
See Configuration and Setup, Resetting Variable Values for details of reset types and the reset process.
Factory Reset GPIO
The factory reset GPIO is GPIO 0 on all Gecko OS devices. To perform a factory reset by GPIO:
- hold the factory reset pin high for more than 10 seconds through a hardware reset.
Button 1 is wired to GPIO 0 on Silabs evaluation boards. On a Silabs evaluation board, to factory reset:
- Press Button 1 and do not release it.
- Press and release the Reset button.
- Continue to press Button 1 for at least 10 seconds.
- Release Button 1.
Note: GPIO 0 always acts as the factory reset GPIO. GPIO 0 may be configured to initialize to another GPIO function, but the factory reset function takes priority over other functions.
Factory Reset Command
Use the factory_reset command to perform a factory reset. To avoid accidental factory reset, the device Wi-Fi MAC address must be provided:
- issue get wlan.mac to obtain the device MAC address
- then issue the factory_reset command with the returned MAC address as its argument:
factory_reset <MAC address>
Web App Recovery
In the event that the Web App does not work, due to a damaged file structure or misconfiguration, you can use the Web App Recovery system to regain access to the network and restore the Web App files. See the Web App Recovery application note.