UDP Client
udp.client.auto_interface
Abbreviation
ud c i
Access
get/set
Description
Interface to auto-start UDP client connection.
Arguments
default
Default
<default/wlan/softap>
Properties
- network_restart to apply change
Supported Platforms
- AMW007
- AMW037
Get example
> get udp.client.auto_interface
default
Set example
> set ud c i wlan
Set OK
udp.client.auto_start
Abbreviation
ud c a
Access
get/set
Description
Enable/disable UDP client auto-start feature. If enabled, UDP client automatically connects to remote server when interface is brought up.
Arguments
<0/1>
Default
0
Properties
- network_restart to apply change
Supported Platforms
- AMW007
- AMW037
Get example
> get udp.client.auto_start
0
Set example
> set ud c a 1
Set OK
udp.client.remote_host
Abbreviation
ud c h
Access
get/set
Description
Domain or IP address of remote udp server to auto connect.
Arguments
<domain/ip address>
Default
null
Properties
Supported Platforms
- AMW007
- AMW037
Get example
> get udp.client.remote_host
mydomain.com
Set example
> set ud c h mydomain.com
Set OK
udp.client.remote_port
Abbreviation
ud c p
Access
get/set
Description
Port of remote UDP server to auto connect.
Arguments
<port>
Default
3000
Properties
Supported Platforms
- AMW007
- AMW037
Get example
> get udp.client.remote_port
Set example
> set ud c p 5000
Set OK