Command API Quickstart
The fastest way to learn about the Gecko OS Command API is to use a desktop machine and a UART terminal application or a web browser over Wi-Fi.
To get your Gecko OS device onto a wireless network, you need to supply the device with network credentials: the wireless network name (SSID) and password.
Let's get started!
There are few steps involved:
- Factory Reset - this step is optional.
- Open a Gecko OS terminal . A Gecko OS terminal is necessary to enter commands via the serial interface.
- Set up Wi-Fi network credentials . There are several ways to do this.
- Verify the Network Connection .
When you have set up a Gecko OS terminal, verified your Wi-Fi network credentials and tested the connection, you can work with all the rich capabilities of Gecko OS. One of the most important Gecko OS features is over-the-air update (OTA). This lets you load the latest version of Gecko OS, or load specific Gecko OS products for development purposes. The steps are:
Performing a Factory Reset
You may optionally performing a factory reset to ensure the device is in a known state.
Performing a
factory_reset
returns variables to the default configuration.
You can factory reset with the factory_reset command, using a Gecko OS terminal .
With a Silabs evaluation board, you can perform a factory reset with the Reset button and Button 1:
- Press Button 1 and do not release it.
- Press and release the Reset button
- Continue to press Button 1 for at least 10 seconds
- Release Button 1.
Opening a Gecko OS Terminal
You can control your Gecko OS device using the Gecko OS Command API via a UART serial terminal or console application.
For a Gecko OS evaluation board, plug the computer USB port into the evaluation board micro USB port. USB provides power and UART serial connection.
For a device not on an evaluation board, connect the terminal to device UART 1 and provide power to the device. For pinout information, see Peripherals, GPIO Functions and Pins or the device datasheet.
With the device UART connected:
- Open a communication terminal application e.g. Teraterm
- Find the UART serial (COM) port associated with the eval board
- Set the communication parameters to 115200 8N1 with NO hardware flow control
- Press the enter key. Gecko OS responds with a ready message and command prompt:
Ready
>
-
At the Gecko OS prompt, type
version
and check for a response similar to the text below.
> version
SILABS-AMW007-2.1.5, Gecko OS-2.1.5, AMW007-W00001
If problems arise, see the Gecko OS Troubleshooting Guide .
Setting up Wi-Fi Network Credentials
Your network credentials are stored in the Gecko OS wlan.ssid and wlan.passkey variables.
There are several ways to set these values, including:
- Setting up with the Command API . See below .
- Setting up with the Web App . See below .
- See Configuration and Setup for more ways to configure a Gecko OS device.
Setting up with the Command API
To set up with the command API, open a Gecko OS terminal as described above.
Enter the following commands into a Gecko OS terminal:
Gecko OS Commands | Description |
---|---|
|
|
Substitute the appropriate values for the placeholders
YOUR_AP_NAME
and
YOUR_AP_PASSWORD
.
Now you can verify the network connection . See below .
Setting Up with the Web App
The Web App provides a graphical interface to configure the network credentials on the device using a web browser. Gecko OS runs a Soft AP and an HTTP server on the Gecko OS device. You connect to the soft AP with a mobile device or computer, and run the Web App in a web browser.
In a Gecko OS terminal, enter the command:
setup web
You can put Silabs evaluation boards into
setup_web
mode without connecting a Gecko OS terminal:
- Press Button 2 and do not release it
- Press and release the Reset button
- Continue to hold Button 2 for at least three seconds
- Release Button 2
For more details, see Web App, Setup Web Mode .
This starts the Gecko OS Soft AP. By default the Soft AP SSID is
Gecko OS Web Setup ###
, where
###
is the last three hex digits of the device WLAN MAC address, e.g.
Gecko OS Web Setup 2D6
. The default password is
password
.
Connect a mobile device or Wi-Fi enabled computer to this network. Open a web browser and navigate to
setup.com
or
Gecko OS.com
.
The Web App opens the Web App connect tab by default, and scans for Wi-Fi networks in range.
Select your preferred network, enter the network password and click
Connect
. The Web App verifies the password and connects to the WLAN. If you select the
Reconnect to device
option, the web app restarts your Gecko OS device, and attempts to reconnect to it via the WLAN. For more details, see
Web App, Setup Web Mode
.
Now you can verify the network connection . See below .
Verifying the Network Connection
When you issue any Gecko OS command that requires network access, Gecko OS attempts to bring the network up using the values set for wlan.ssid and wlan.passkey .
You can bring the network up with the network_up command.
In the
Gecko OS terminal
, at the
>
prompt, enter the command as shown. The response should be similar to the following:
Gecko OS Commands | Description |
---|---|
|
|
If your Gecko OS device successfully obtains an IP address, you are connected.
Silabs evaluation boards have a network indicator LED to help determine successful association. The network indicator LED changes its blink rate from fast (no IP address), to medium (DHCP in progress) to slow (DHCP successful, IP address obtained).
If your WLAN is connected to the Internet, you can try an Internet protocol command. For example, ping a known host:
Gecko OS Commands | Description |
---|---|
|
|
Claiming Your Device
The Silabs Device Management Service tracks Gecko OS devices, their owners, their firmware configuration and many other details. The DMS handles Over-the-Air (OTA) updates, providing a secure way to update devices in the field.
You need a free DMS account before using DMS features like OTA. To create an account go to the DMS Signup page. The DMS username (your email address) and password you register are used when you claim your device.
To claim your device, in the Gecko OS terminal , issue the dms_claim command:
Gecko OS Commands | Description |
---|---|
|
|
When you have successfully claimed your device, you can perform a Device Firmware Update (DFU) update. See below .
For full details of the DMS claim and OTA update process, see Update and Recovery .
Performing a DFU
Use DFU to update to the latest version of your device's Gecko OS product, or to load a development Gecko OS device with a specific Gecko OS product or version. You need to claim your device before performing a DFU. See above .
To OTA, in the Gecko OS terminal , issue the dfu_update command.
The DMS Claim and DFU (Device Firmware Update) process is discussed in detail in Update and Recovery .
Gecko OS Applications
Now that you have established control over your Gecko OS device, you can experiment with the rich set of Gecko OS features using the Gecko OS Command API.
There are many application notes demonstrating Gecko OS networking applications. See Application Examples .
Getting Help
As well as the Gecko OS documentation provided on this website, Gecko OS also provides interactive command line help. At the Gecko OS terminal prompt, issue the help command:
> help
Help options for the Gecko OS Command API ...
help all -> Print a list of all Commands and Variables
help commands -> Print a list of Commands
help variables -> Print a list of readable Variables
help <command> -> Print help for a specific Command
help <variable> -> Print help for a specific Variable
Additional help is available online at http://docs.silabs.com/gecko-os
- Enter help all for a full list of commands and variables .
- Enter help commands to list commands only, or help variables to list variables only.
- Enter help <command_or_variable_name> to show help for an individual command or variable.