Release Notes for Gecko OS Edition 2
Gecko OS 2 evolved from ZentriOS WL 1.5. To update from ZentriOS WL to Gecko OS, see Updating to Gecko OS . This page also lists differences between ZentriOS WL and Gecko OS 2 .
We recommend upgrading to the latest version of Gecko OS 2. See release notes for the latest version of Gecko OS 2 .
Version String
Note that the version string changes format in Gecko OS 2. The ZentriOS WL 1.5 version string is similar to:
ZENTRI-AMW007-1.5.0.13, 2018-09-03T06:06:14Z, ZentriOS-WL-1.5.0.13, Board:AMW007-E03.2
The Gecko OS 2 version string is similar to:
SILABS-AMW007-2.1.5, Gecko OS-2.1.5, AMW007-W00001
The version number in Gecko OS 2 contains major version, minor version, and patch version, e.g.
2.1.5
. It does not contain a release candidate version number.
Gecko OS 2.2.14 Release
Last Updated: October, 2019
This release contains the same set of features and fixes documented in Gecko OS 2.2.5 Beta below. Those release notes are duplicated here for the benefit of customers not involved in beta testing.
To update to this release from a previous release, use the following command:
ota -b 2.2.14
The
ota
command is deprecated in this release and will be phased out in future releases. It is replaced by DFU (Device Firmware Update) commands
dfu_query
and
dfu_update
.
This release contains a number of fixes and several features unavailable in previous releases.
The following changes are differences between Gecko OS 2.2 and Gecko OS 2.1 .
TLS records exceeding 4K are now supported. TLS connection, to a server that sends fragment sizes larger than 4K, now succeeds.
Auto-started TCP client, UDP client, TCP server and UDP server now restart after issuing the network_restart command.
STREAM mode is now fully supported for UDP client, for both RX and TX. See udp.client.auto_start . STREAM mode is also fully supported for UDP Server. See udp.server.auto_start .
Gecko OS now supports concurrent Wi-Fi AP ( SoftAP ) and STA ( WLAN ) modes.
The softap.ssid value is now generated correctly as documented.
Gecko OS supports up to 8 concurrent TCP client streams.
A new TCP keepalive feature has been added. See tcp.keepalive.enabled .
Deleting an open file automatically closes its stream. See the file_delete command.
The file_create now fails if a file of the same name already exists.
The
http_post
maximum request size has been increased to
5000
bytes. An
http_post
command with zero content now works as expected.
The http_download command now successfully downloads files larger than 64KB.
The dms_claim command now accepts a DMS token as an alternative to username and password.
The network indicator LED now returns to fast blinking when the network is down.
This version includes a security update to defeat the WPA2 KRACK exploit.
Issuing the
dfu_query
or
dfu_update
(previously the
ota
command) from the
webapp console
now works correctly.
Known Issues
Last Updated : October, 2019
| Topic | Description | Solution or Workaround |
|---|---|---|
| http_post data size 5000 byte limit | http_post data size is limited to 5000 bytes. | Break the http_post activity into multiple requests with sizes smaller than 5000 bytes. |
| system.indicator.state | system.indicator.state is read only. The variable cannot be set. | There is no workaround. |
| softap.idle_timeout | The variable softap.idle_timeout is listed in Gecko OS 2.2 but its function is not supported. | There is no workaround. |
| Unexpected SoftAP startup | A bare AMW0x7 module, as used in custom PCB designs, may leave GPIO5 floating. Because setup.gpio.control_gpio defaults to GPIO5, setup_web mode may be invoked on boot or reset, if the floating GPIO5 registers high. In this case, the SoftAP interface will be brought up. |
Disable
setup.gpio.control_gpio
by setting it to
-1
. Alternatively modify the hardware design so that GPIO5 is not floating.
|
Fixes and Improvements
| Topic | Description |
|---|---|
| SoftAp SSID | An intermittent issue, where softap.ssid was generated with an incorrect value, is now fixed. |
Commands Added
| Change | Description |
|---|---|
| dfu_query |
The
dfu_query
command is a new command to replace the
ota -q
command. The
ota
command remains in this version but will be removed in future versions.
|
| dfu_update |
The
dfu_update
command is a new command to replace the
ota [-f / b <bundle-id>]
command. The
ota
command remains in this version but will be removed in future versions.
|
| setup_web |
The
setup_web
command is a new command to replace the
setup web
command. The
setup
command remains in this version but the
web
option will be removed in future versions.
|
Commands Changed
| Change | Description |
|---|---|
| dms_claim | The dms_claim command now accepts a DMS token as an alternative to username and password. |
| http_add_header |
The
http_add_header
command now supports the
:extended
header option for headers up to
1024
bytes in length.
|
| network_lookup |
The
network_lookup
command now supports the
-i
option to specify network interface.
|
Commands Deprecated
| Change | Description |
|---|---|
ota
-q
|
The
ota
-q
command is deprecated. In Command API code, replace
ota -q
calls with
dfu_query
calls.
|
ota
[-f / b <bundle-id>]
|
The
ota
[-f / b <bundle-id>]
is deprecated. In Command API code, replace
ota
calls with
dfu_update
calls.
|
setup
web
|
The
setup
web
command is deprecated. In Command API code, replace
setup web
calls with
setup_web
calls.
|
Variables Added
| Change | Description |
|---|---|
| remote_terminal.interface | Interface for remote terminal. |
| tcp.client.auto_interface | Interface to auto-start TCP client connection. |
| tcp.keepalive.enabled | Enable/disable TCP keepalive feature of network stack. |
| tcp.keepalive.initial_timeout | Number of seconds for initial keepalive expiration. |
| tcp.keepalive.retry_count | Maximum number of times to retry keepalive. |
| tcp.keepalive.retry_timeout | After initial expiration, period of retries in seconds. |
| tcp.server.auto_interface | Wireless interface used for the TCP server if auto-start is enabled. |
| udp.server.auto_interface | Wireless interface used for the UDP server if auto-start is enabled. |
Gecko OS 2.2.5 Beta
Last Updated: May, 2019
To update to this beta release from previous release or beta versions, issue the command:
ota -b 2.2.5
This beta release contains a number of fixes and several features unavailable in previous versions.
The following changes are differences between Gecko OS 2.2 and Gecko OS 2.1 .
TLS records exceeding 4K are now supported. TLS connection, to a server that sends fragment sizes larger than 4K, now succeeds.
Auto-started TCP client, UDP client, TCP server and UDP server now restart after issuing the network_restart command.
STREAM mode is now fully supported for UDP client, for both RX and TX. See udp.client.auto_start . STREAM mode is also fully supported for UDP Server. See udp.server.auto_start .
Gecko OS now supports concurrent Wi-Fi AP ( SoftAP ) and STA ( WLAN ) modes.
The softap.ssid value is now generated correctly as documented.
Gecko OS supports up to 8 concurrent TCP client streams.
A new TCP keepalive feature has been added.
Deleting an open file automatically closes its stream. See the file_delete command.
The file_create now fails if a file of the same name already exists.
The
http_post
maximum request size has been increased to
5000
bytes. An
http_post
command with zero content now works as expected.
The http_download command now successfully downloads files larger than 64KB.
The dms_claim command now accepts a DMS token as an alternative to username and password.
The network indicator LED now returns to fast blinking when the network is down.
This version includes a security update to defeat the WPA2 KRACK exploit.
The
ota
command will be phased out in future releases, to be replaced by DFU (Device Firmware Update) commands
dfu_query
and
dfu_update
.
Issuing the
dfu_query
or
dfu_update
(previously the
ota
command) from the
webapp console
now works correctly.
Known Issues
Last Updated : May, 2019
| Topic | Description | Solution or Workaround |
|---|---|---|
| http_post data size 5000 byte limit | http_post data size is limited to 5000 bytes. | Break the http_post activity into multiple requests with sizes smaller than 5000 bytes. |
| system.indicator.state | system.indicator.state is read only. The variable cannot be set. | There is no workaround. |
| softap.idle_timeout | The variable softap.idle_timeout is listed in Gecko OS 2.2 but its function is not supported. | There is no workaround. |
Fixes and Improvements
| Topic | Description |
|---|---|
| SoftAp SSID | An intermittent issue, where softap.ssid was generated with an incorrect value, is now fixed. |
Commands Added
| Change | Description |
|---|---|
| dfu_query |
The
dfu_query
command is a new command to replace the
ota -q
command. The
ota
command remains in this version but will be removed in future versions.
|
| dfu_update |
The
dfu_update
command is a new command to replace the
ota [-f / b <bundle-id>]
command. The
ota
command remains in this version but will be removed in future versions.
|
| setup_web |
The
setup_web
command is a new command to replace the
setup web
command. The
setup
command remains in this version but the
web
option will be removed in future versions.
|
Commands Changed
| Change | Description |
|---|---|
| dms_claim | The dms_claim command now accepts a DMS token as an alternative to username and password. |
| http_add_header |
The
http_add_header
command now supports the
:extended
header option for headers up to
1024
bytes in length.
|
| network_lookup |
The
network_lookup
command now supports the
-i
option to specify network interface.
|
Commands Deprecated
| Change | Description |
|---|---|
ota
-q
|
The
ota
-q
command is deprecated. In Command API code, replace
ota -q
calls with
dfu_query
calls.
|
ota
[-f / b <bundle-id>]
|
The
ota
[-f / b <bundle-id>]
is deprecated. In Command API code, replace
ota
calls with
dfu_update
calls.
|
setup
web
|
The
setup
web
command is deprecated. In Command API code, replace
setup web
calls with
setup_web
calls.
|
Variables Added
| Change | Description |
|---|---|
| remote_terminal.interface | Interface for remote terminal. |
| tcp.client.auto_interface | Interface to auto-start TCP client connection. |
| tcp.keepalive.enabled | Enable/disable TCP keepalive feature of network stack. |
| tcp.keepalive.initial_timeout | Number of seconds for initial keepalive expiration. |
| tcp.keepalive.retry_count | Maximum number of times to retry keepalive. |
| tcp.keepalive.retry_timeout | After initial expiration, period of retries in seconds. |
| tcp.server.auto_interface | Wireless interface used for the TCP server if auto-start is enabled. |
| udp.server.auto_interface | Wireless interface used for the UDP server if auto-start is enabled. |