Measurement mode initialization structure.

Public Attributes#

Selects the conversion sample mode.

Selects the conversion trigger source.

bool

Enables DMA operation.

bool

Disables dividing the accumulated result.

Selects the number of samples to accumulate per conversion.

Selects the Exponential Moving Average sample weighting.

Enables the comparator and selects the comparison type.

uint16_t

Comparator threshold value.

Selects an APORT channel for a single conversion.

uint32_t

Mask selects inputs 0 to 31.

uint32_t

Mask selects inputs 32 to 63.

bool

Ground inactive inputs during a conversion.

Selects the converter type.

Selects the Successive Approximation (SAR) converter resolution.

Selects the Delta Modulation (DM) converter resolution.

uint8_t

Sets the number of DM iterations (comparisons) per cycle.

uint8_t

Sets number of DM converter cycles.

uint8_t

Sets the DM converter initial delta value.

bool

Disables DM automatic delta size reduction per cycle.

Selects the reset phase timing.

Selects the output drive strength.

Selects the converter gain.

Public Attribute Documentation#

sampleMode#

CSEN_SampleMode_TypeDef CSEN_InitMode_TypeDef::sampleMode

Selects the conversion sample mode.


trigSel#

CSEN_TrigSel_TypeDef CSEN_InitMode_TypeDef::trigSel

Selects the conversion trigger source.


enableDma#

bool CSEN_InitMode_TypeDef::enableDma

Enables DMA operation.


sumOnly#

bool CSEN_InitMode_TypeDef::sumOnly

Disables dividing the accumulated result.


accMode#

CSEN_AccMode_TypeDef CSEN_InitMode_TypeDef::accMode

Selects the number of samples to accumulate per conversion.


emaSample#

CSEN_EMASample_TypeDef CSEN_InitMode_TypeDef::emaSample

Selects the Exponential Moving Average sample weighting.


cmpMode#

CSEN_CmpMode_TypeDef CSEN_InitMode_TypeDef::cmpMode

Enables the comparator and selects the comparison type.


cmpThr#

uint16_t CSEN_InitMode_TypeDef::cmpThr

Comparator threshold value.

Meaning depends on cmpMode.


singleSel#

CSEN_SingleSel_TypeDef CSEN_InitMode_TypeDef::singleSel

Selects an APORT channel for a single conversion.


inputMask0#

uint32_t CSEN_InitMode_TypeDef::inputMask0

Mask selects inputs 0 to 31.

Effect depends on sampleMode. If sample mode is bonded, then mask selects inputs to short together. If sample mode is scan, then mask selects which inputs will be scanned. If sample mode is single and auto-ground is on (autoGnd is true), mask selects which pins are grounded.


inputMask1#

uint32_t CSEN_InitMode_TypeDef::inputMask1

Mask selects inputs 32 to 63.

See inputMask0 for more information.


autoGnd#

bool CSEN_InitMode_TypeDef::autoGnd

Ground inactive inputs during a conversion.


convSel#

CSEN_ConvSel_TypeDef CSEN_InitMode_TypeDef::convSel

Selects the converter type.


sarRes#

CSEN_SARRes_TypeDef CSEN_InitMode_TypeDef::sarRes

Selects the Successive Approximation (SAR) converter resolution.


dmRes#

CSEN_DMRes_TypeDef CSEN_InitMode_TypeDef::dmRes

Selects the Delta Modulation (DM) converter resolution.


dmIterPerCycle#

uint8_t CSEN_InitMode_TypeDef::dmIterPerCycle

Sets the number of DM iterations (comparisons) per cycle.

Only applies to the Delta Modulation converter.


dmCycles#

uint8_t CSEN_InitMode_TypeDef::dmCycles

Sets number of DM converter cycles.

Only applies to the Delta Modulation converter.


dmDelta#

uint8_t CSEN_InitMode_TypeDef::dmDelta

Sets the DM converter initial delta value.

Only applies to the Delta Modulation converter.


dmFixedDelta#

bool CSEN_InitMode_TypeDef::dmFixedDelta

Disables DM automatic delta size reduction per cycle.

Only applies to the Delta Modulation converter.


resetPhase#

CSEN_ResetPhaseSel_TypeDef CSEN_InitMode_TypeDef::resetPhase

Selects the reset phase timing.

Most measurements should use the default value. See reference manual for details on when to adjust.


driveSel#

CSEN_DriveSel_TypeDef CSEN_InitMode_TypeDef::driveSel

Selects the output drive strength.

Most measurements should use the default value. See reference manual for details on when to adjust.


gainSel#

CSEN_GainSel_TypeDef CSEN_InitMode_TypeDef::gainSel

Selects the converter gain.