Decoder state condition descriptor structure.

Public Attributes#

uint8_t

Configure compare value.

uint8_t

Configure compare mask.

uint8_t

Configure index of the current state when evaluation is done.

uint8_t

Configure index of state to be entered if the sensor state equals to compVal.

Configure which PRS action to perform when the sensor state equals to compVal.

bool

If enabled, interrupt flag is set when sensor state equals to compVal.

Public Attribute Documentation#

compVal#

uint8_t LESENSE_DecStCond_TypeDef::compVal

Configure compare value.

State transition is triggered when the sensor state equals to this value. Valid range: 0-15 (4 bits).


Definition at line 1307 of file platform/emlib/inc/em_lesense.h

compMask#

uint8_t LESENSE_DecStCond_TypeDef::compMask

Configure compare mask.

Set bit X to exclude sensor X from evaluation. Note: decoder can handle sensor inputs from up to 4 sensors; therefore, this mask is 4 bit long.


Definition at line 1312 of file platform/emlib/inc/em_lesense.h

curState#

uint8_t LESENSE_DecStCond_TypeDef::curState

Configure index of the current state when evaluation is done.

Valid range: 0-15 (4 bits).


Definition at line 1317 of file platform/emlib/inc/em_lesense.h

nextState#

uint8_t LESENSE_DecStCond_TypeDef::nextState

Configure index of state to be entered if the sensor state equals to compVal.

Valid range: 0-15 (4 bits).


Definition at line 1322 of file platform/emlib/inc/em_lesense.h

prsAct#

LESENSE_StTransAct_TypeDef LESENSE_DecStCond_TypeDef::prsAct

Configure which PRS action to perform when the sensor state equals to compVal.


Definition at line 1326 of file platform/emlib/inc/em_lesense.h

setInt#

bool LESENSE_DecStCond_TypeDef::setInt

If enabled, interrupt flag is set when sensor state equals to compVal.


Definition at line 1329 of file platform/emlib/inc/em_lesense.h