LESENSE timing control descriptor structure.

Public Attributes#

uint8_t

Set number of LFACLK cycles to delay sensor interaction on each channel.

bool

Set to true do delay startup of AUXHFRCO until the system enters excite phase.

Public Attribute Documentation#

startDelay#

uint8_t LESENSE_TimeCtrlDesc_TypeDef::startDelay

Set number of LFACLK cycles to delay sensor interaction on each channel.

Valid range: 0-3 (2 bit).


Definition at line 736 of file platform/emlib/inc/em_lesense.h

delayAuxStartup#

bool LESENSE_TimeCtrlDesc_TypeDef::delayAuxStartup

Set to true do delay startup of AUXHFRCO until the system enters excite phase.

This will reduce the time AUXHFRCO is enabled and reduce power usage.


Definition at line 742 of file platform/emlib/inc/em_lesense.h