You are viewing documentation for version:4.3Public Attributes#uint32_tVECTACTIVEuint32_t__pad0__uint32_tRETTOBASEuint32_tVECTPENDINGuint32_t__pad1__uint32_tISRPENDINGuint32_tISRPREEMPTuint32_t__pad2__uint32_tPENDSTCLRuint32_tPENDSTSETuint32_tPENDSVCLRuint32_tPENDSVSETuint32_t__pad3__uint32_tNMIPENDSETstruct HalCrashIcsrType::@4bitsuint32_twordPublic Attribute Documentation#VECTACTIVE#uint32_t HalCrashIcsrType::VECTACTIVE__pad0__#uint32_t HalCrashIcsrType::__pad0__RETTOBASE#uint32_t HalCrashIcsrType::RETTOBASEVECTPENDING#uint32_t HalCrashIcsrType::VECTPENDING__pad1__#uint32_t HalCrashIcsrType::__pad1__ISRPENDING#uint32_t HalCrashIcsrType::ISRPENDINGISRPREEMPT#uint32_t HalCrashIcsrType::ISRPREEMPT__pad2__#uint32_t HalCrashIcsrType::__pad2__PENDSTCLR#uint32_t HalCrashIcsrType::PENDSTCLRPENDSTSET#uint32_t HalCrashIcsrType::PENDSTSETPENDSVCLR#uint32_t HalCrashIcsrType::PENDSVCLRPENDSVSET#uint32_t HalCrashIcsrType::PENDSVSET__pad3__#uint32_t HalCrashIcsrType::__pad3__NMIPENDSET#uint32_t HalCrashIcsrType::NMIPENDSETbits#struct HalCrashIcsrType::@4 HalCrashIcsrType::bitsword#uint32_t HalCrashIcsrType::word