HFXO initialization structure.

Initialization values should be obtained from a configuration tool, application note or crystal data sheet.

Public Attributes#

uint8_t

HFXO Boost, 0=50% 1=70%, 2=80%, 3=100%.

uint8_t

Startup delay.

bool

Enable/disable glitch detector.

Oscillator mode.

Public Attribute Documentation#

boost#

uint8_t CMU_HFXOInit_TypeDef::boost

HFXO Boost, 0=50% 1=70%, 2=80%, 3=100%.


Definition at line 3172 of file platform/emlib/inc/em_cmu.h

timeout#

uint8_t CMU_HFXOInit_TypeDef::timeout

Startup delay.


Definition at line 3173 of file platform/emlib/inc/em_cmu.h

glitchDetector#

bool CMU_HFXOInit_TypeDef::glitchDetector

Enable/disable glitch detector.


Definition at line 3174 of file platform/emlib/inc/em_cmu.h

mode#

CMU_OscMode_TypeDef CMU_HFXOInit_TypeDef::mode

Oscillator mode.


Definition at line 3176 of file platform/emlib/inc/em_cmu.h