Initialization structure.

Public Attributes#

Specifies whether TX and/or RX will be enabled when initialization completes.

uint32_t

LEUART reference clock assumed when configuring baud rate setup.

uint32_t

Desired baud rate.

Number of data bits in frame.

Parity mode to use.

Number of stop bits to use.

Public Attribute Documentation#

enable#

LEUART_Enable_TypeDef LEUART_Init_TypeDef::enable

Specifies whether TX and/or RX will be enabled when initialization completes.


Definition at line 94 of file platform/emlib/inc/em_leuart.h

refFreq#

uint32_t LEUART_Init_TypeDef::refFreq

LEUART reference clock assumed when configuring baud rate setup.

Set to 0 if using currently configured reference clock.


Definition at line 100 of file platform/emlib/inc/em_leuart.h

baudrate#

uint32_t LEUART_Init_TypeDef::baudrate

Desired baud rate.


Definition at line 103 of file platform/emlib/inc/em_leuart.h

databits#

LEUART_Databits_TypeDef LEUART_Init_TypeDef::databits

Number of data bits in frame.


Definition at line 106 of file platform/emlib/inc/em_leuart.h

parity#

LEUART_Parity_TypeDef LEUART_Init_TypeDef::parity

Parity mode to use.


Definition at line 109 of file platform/emlib/inc/em_leuart.h

stopbits#

LEUART_Stopbits_TypeDef LEUART_Init_TypeDef::stopbits

Number of stop bits to use.


Definition at line 112 of file platform/emlib/inc/em_leuart.h