DPLL initialization structure.

Frequency will be Fref*(N+1)/(M+1).

Public Attributes#

uint32_t

PLL frequency value, max 40 MHz.

uint16_t

Factor N.

uint16_t

Factor M.

uint8_t

Spread spectrum update interval.

uint8_t

Spread spectrum amplitude.

Reference clock selector.

Reference clock edge detect selector.

DPLL lock mode selector.

bool

Enable automatic lock recovery.

Public Attribute Documentation#

frequency#

uint32_t CMU_DPLLInit_TypeDef::frequency

PLL frequency value, max 40 MHz.


Definition at line 3292 of file platform/emlib/inc/em_cmu.h

n#

uint16_t CMU_DPLLInit_TypeDef::n

Factor N.

300 <= N <= 4095


Definition at line 3293 of file platform/emlib/inc/em_cmu.h

m#

uint16_t CMU_DPLLInit_TypeDef::m

Factor M.

M <= 4095


Definition at line 3294 of file platform/emlib/inc/em_cmu.h

ssInterval#

uint8_t CMU_DPLLInit_TypeDef::ssInterval

Spread spectrum update interval.


Definition at line 3295 of file platform/emlib/inc/em_cmu.h

ssAmplitude#

uint8_t CMU_DPLLInit_TypeDef::ssAmplitude

Spread spectrum amplitude.


Definition at line 3296 of file platform/emlib/inc/em_cmu.h

refClk#

CMU_DPLLClkSel_TypeDef CMU_DPLLInit_TypeDef::refClk

Reference clock selector.


Definition at line 3297 of file platform/emlib/inc/em_cmu.h

edgeSel#

CMU_DPLLEdgeSel_TypeDef CMU_DPLLInit_TypeDef::edgeSel

Reference clock edge detect selector.


Definition at line 3298 of file platform/emlib/inc/em_cmu.h

lockMode#

CMU_DPLLLockMode_TypeDef CMU_DPLLInit_TypeDef::lockMode

DPLL lock mode selector.


Definition at line 3299 of file platform/emlib/inc/em_cmu.h

autoRecover#

bool CMU_DPLLInit_TypeDef::autoRecover

Enable automatic lock recovery.


Definition at line 3300 of file platform/emlib/inc/em_cmu.h