NVIC Initialization#

Initialize the NVIC Interrupt Handlers priority.

Set all interrupt priorities, except the Fault exceptions, to CORE_INTERRUPT_DEFAULT_PRIORITY value.

When the Device Init NVIC module is present and no configuration overwrites the em_core CORE_ATOMIC_METHOD define, the atomic method is automatically set to BASEPRI (CORE_ATOMIC_METHOD_BASEPRI).

Functions#

sl_status_t

Sets default priority for all configurable interrupts in NVIC.

Function Documentation#

sl_device_init_nvic#

sl_status_t sl_device_init_nvic (void )

Sets default priority for all configurable interrupts in NVIC.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Status code