Define crash registers as structs so a debugger can display their bit fields.

Public Attributes#

uint32_t
uint32_t
uint32_t
uint32_t
uint32_t
uint32_t
uint32_t
uint32_t
uint32_t
uint32_t
struct HalCrashxPsrType::@1

bits

uint32_t

word

Public Attribute Documentation#

EXCPT#

uint32_t HalCrashxPsrType::EXCPT

Definition at line 56 of file platform/service/legacy_hal/inc/cortexm3/diagnostic.h

ICIIT_LOW#

uint32_t HalCrashxPsrType::ICIIT_LOW

Definition at line 57 of file platform/service/legacy_hal/inc/cortexm3/diagnostic.h

__pad0__#

uint32_t HalCrashxPsrType::__pad0__

Definition at line 58 of file platform/service/legacy_hal/inc/cortexm3/diagnostic.h

T#

uint32_t HalCrashxPsrType::T

Definition at line 59 of file platform/service/legacy_hal/inc/cortexm3/diagnostic.h

ICIIT_HIGH#

uint32_t HalCrashxPsrType::ICIIT_HIGH

Definition at line 60 of file platform/service/legacy_hal/inc/cortexm3/diagnostic.h

Q#

uint32_t HalCrashxPsrType::Q

Definition at line 61 of file platform/service/legacy_hal/inc/cortexm3/diagnostic.h

V#

uint32_t HalCrashxPsrType::V

Definition at line 62 of file platform/service/legacy_hal/inc/cortexm3/diagnostic.h

C#

uint32_t HalCrashxPsrType::C

Definition at line 63 of file platform/service/legacy_hal/inc/cortexm3/diagnostic.h

Z#

uint32_t HalCrashxPsrType::Z

Definition at line 64 of file platform/service/legacy_hal/inc/cortexm3/diagnostic.h

N#

uint32_t HalCrashxPsrType::N

Definition at line 65 of file platform/service/legacy_hal/inc/cortexm3/diagnostic.h

bits#

struct HalCrashxPsrType::@1 HalCrashxPsrType::bits

bits


Definition at line 66 of file platform/service/legacy_hal/inc/cortexm3/diagnostic.h

word#

uint32_t HalCrashxPsrType::word

word


Definition at line 68 of file platform/service/legacy_hal/inc/cortexm3/diagnostic.h