Standard I/O#

Standard I/O allows to get and put characters on stdio stream that is the default in I/O Streams.

Functions#

sl_putchar(char c)

Put a character on the default stream.

sl_getchar(char *c)

Get a character on the default stream.

Macros#

#define
putchar (c)

Put a character on the default stream (match standard API).

#define
getchar sl_getchar_std_wrapper

Get a character on the default stream.

Function Documentation#

sl_putchar#

sl_status_t sl_putchar (char c)

Put a character on the default stream.

Parameters
TypeDirectionArgument NameDescription
char[in]c

Character to print

Returns

  • Status result


sl_getchar#

sl_status_t sl_getchar (char * c)

Get a character on the default stream.

Parameters
TypeDirectionArgument NameDescription
char *[out]c

Pointer to variable that will receive the character.

Returns

  • Status result