LETIMER initialization structure.

Public Attributes#

bool

Start counting when initialization completes.

bool

Counter shall keep running during debug halt.

bool

Start counting on RTC COMP0 match.

bool

Start counting on RTC COMP1 match.

bool

Load COMP0 register into CNT when counter underflows.

bool

Load COMP1 into COMP0 when REP0 reaches 0.

uint8_t

Idle value for output 0.

uint8_t

Idle value for output 1.

Underflow output 0 action.

Underflow output 1 action.

uint32_t

Top value.

Public Attribute Documentation#

enable#

bool LETIMER_Init_TypeDef::enable

Start counting when initialization completes.


debugRun#

bool LETIMER_Init_TypeDef::debugRun

Counter shall keep running during debug halt.


rtcComp0Enable#

bool LETIMER_Init_TypeDef::rtcComp0Enable

Start counting on RTC COMP0 match.


rtcComp1Enable#

bool LETIMER_Init_TypeDef::rtcComp1Enable

Start counting on RTC COMP1 match.


comp0Top#

bool LETIMER_Init_TypeDef::comp0Top

Load COMP0 register into CNT when counter underflows.


bufTop#

bool LETIMER_Init_TypeDef::bufTop

Load COMP1 into COMP0 when REP0 reaches 0.


out0Pol#

uint8_t LETIMER_Init_TypeDef::out0Pol

Idle value for output 0.


out1Pol#

uint8_t LETIMER_Init_TypeDef::out1Pol

Idle value for output 1.


ufoa0#

LETIMER_UFOA_TypeDef LETIMER_Init_TypeDef::ufoa0

Underflow output 0 action.


ufoa1#

LETIMER_UFOA_TypeDef LETIMER_Init_TypeDef::ufoa1

Underflow output 1 action.


repMode#

LETIMER_RepeatMode_TypeDef LETIMER_Init_TypeDef::repMode

Repeat mode.


topValue#

uint32_t LETIMER_Init_TypeDef::topValue

Top value.

Counter wraps when top value matches counter value is reached.