CORE - Core Interrupt#


Introduction#

CORE interrupt API provides a simple and safe means to disable and enable interrupts to protect sections of code.

This is often referred to as "critical sections". This module provides support for three types of critical sections, each with different interrupt blocking capabilities.

  • CRITICAL section: Inside a critical section, all interrupts are disabled (except for fault handlers). The PRIMASK register is always used for interrupt disable/enable.

  • ATOMIC section: This type of section is configurable and the default method is to use PRIMASK. With BASEPRI configuration, interrupts with priority equal to or lower than a given configurable level are disabled. The interrupt disable priority level is defined at compile time. The BASEPRI register is not available for all architectures.

  • NVIC mask section: Disable NVIC (external interrupts) on an individual manner.

em_core also has an API for manipulating RAM-based interrupt vector tables.


Compile-time Configuration#

The following #defines are used to configure em_core:

// The interrupt priority level used inside ATOMIC sections.
#define CORE_ATOMIC_BASE_PRIORITY_LEVEL    3

// A method used for interrupt disable/enable within ATOMIC sections.
#define CORE_ATOMIC_METHOD                 CORE_ATOMIC_METHOD_PRIMASK

If the default values do not support your needs, they can be overridden by supplying -D compiler flags on the compiler command line or by collecting all macro redefinitions in a file named emlib_config.h and then supplying -DEMLIB_USER_CONFIG on a compiler command line.

Note

  • The default emlib configuration for ATOMIC section interrupt disable method is using PRIMASK, i.e., ATOMIC sections are implemented as CRITICAL sections.

  • Due to architectural limitations Cortex-M0+ devices do not support ATOMIC type critical sections using the BASEPRI register. On M0+ devices ATOMIC section helper macros are available but they are implemented as CRITICAL sections using PRIMASK register.


Macro API#

The primary em_core API is the macro API. Macro API will map to correct CORE functions according to the selected CORE_ATOMIC_METHOD and similar configurations (the full CORE API is of course also available). The most useful macros are as follows:

CORE_DECLARE_IRQ_STATE
CORE_ENTER_ATOMIC()
@n Used together to implement an ATOMIC section.

{
  CORE_DECLARE_IRQ_STATE;           // Storage for saving IRQ state prior to
                                    // atomic section entry.

  CORE_ENTER_ATOMIC();              // Enter atomic section.

  ...
  ... your code goes here ...
  ...

  CORE_EXIT_ATOMIC();               // Exit atomic section, IRQ state is restored.
}


@n A concatenation of all three macros above.

{
  CORE_ATOMIC_SECTION(
    ...
    ... your code goes here ...
    ...
  )
}


CORE_DECLARE_IRQ_STATE
CORE_ENTER_CRITICAL()
CORE_EXIT_CRITICAL()
@n These macros implement CRITICAL sections in a similar fashion as described above for ATOMIC sections.


CORE_DECLARE_NVIC_STATE
CORE_ENTER_NVIC()
CORE_EXIT_NVIC()
@n These macros implement NVIC mask sections in a similar fashion as described above for ATOMIC sections. See Examples for an example.

Refer to Macros or Macro Definition Documentation below for a full list of macros.


API reimplementation#

Most of the functions in the API are implemented as weak functions. This means that it is easy to reimplement when special needs arise. Shown below is a reimplementation of CRITICAL sections suitable if FreeRTOS OS is used:

CORE_irqState_t CORE_EnterCritical(void)
{
  vPortEnterCritical();
  return 0;
}

void CORE_ExitCritical(CORE_irqState_t irqState)
{
  (void)irqState;
  vPortExitCritical();
}

Also note that CORE_Enter/ExitCritical() are not implemented as inline functions. As a result, reimplementations will be possible even when original implementations are inside a linked library.

Some RTOSes must be notified on interrupt handler entry and exit. Macros CORE_INTERRUPT_ENTRY() and CORE_INTERRUPT_EXIT() are suitable placeholders for inserting such code. Insert these macros in all your interrupt handlers and then override the default macro implementations. This is an example if uC/OS is used:

// In emlib_config.h:

#define CORE_INTERRUPT_ENTRY()   OSIntEnter()
#define CORE_INTERRUPT_EXIT()    OSIntExit()


Interrupt vector tables#

When using RAM based interrupt vector tables it is the user's responsibility to allocate the table space correctly. The tables must be aligned as specified in the CPU reference manual.

@n Initialize a RAM based vector table by copying table entries from a source vector table to a target table. VTOR is set to the address of the target vector table.


CORE_GetNvicRamTableHandler()
@n Use these functions to get or set the interrupt handler for a specific IRQn. They both use the interrupt vector table defined by the current VTOR register value.


Maximum Interrupt Disabled Time#

The maximum time spent (in cycles) in critical and atomic sections can be measured for performance and interrupt latency analysis. To enable the timings, use the SL_EMLIB_CORE_ENABLE_INTERRUPT_DISABLED_TIMING configuration option. When enabled, the functions
CORE_get_max_time_critical_section()
CORE_get_max_time_atomic_section()
can be used to get the max timings since startup.


Examples#

Implement an NVIC critical section:

{
  CORE_DECLARE_NVIC_ZEROMASK(mask); // A zero initialized NVIC disable mask

  // Set mask bits for IRQs to block in the NVIC critical section.
  // In many cases, you can create the disable mask once upon application
  // startup and use the mask globally throughout the application lifetime.
  CORE_NvicMaskSetIRQ(LEUART0_IRQn, &mask);
  CORE_NvicMaskSetIRQ(VCMP_IRQn,    &mask);

  // Enter NVIC critical section with the disable mask
  CORE_NVIC_SECTION(&mask,
    ...
    ... your code goes here ...
    ...
  )
}


Porting from em_int#

Existing code using INT_Enable() and INT_Disable() must be ported to the em_core API. While em_int used, a global counter to store the interrupt state, em_core uses a local variable. Any usage of INT_Disable(), therefore, needs to be replaced with a declaration of the interrupt state variable before entering the critical section.

Since the state variable is in local scope, the critical section exit needs to occur within the scope of the variable. If multiple nested critical sections are used, each needs to have its own state variable in its own scope.

In many cases, completely disabling all interrupts using CRITICAL sections might be more heavy-handed than needed. When porting, consider whether other types of sections, such as ATOMIC or NVIC mask, can be used to only disable a subset of the interrupts.

Replacing em_int calls with em_core function calls:

void func(void)
{
  // INT_Disable();
  CORE_DECLARE_IRQ_STATE;
  CORE_ENTER_ATOMIC();
    .
    .
    .
  // INT_Enable();
  CORE_EXIT_ATOMIC();
}

Modules#

dwt_cycle_counter_handle_t

CORE_nvicMask_t

Typedefs#

typedef uint32_t

Storage for PRIMASK or BASEPRI value.

typedef uint32_t

Storage for PRIMASK or BASEPRI value.

Functions#

void

Disable interrupts.

void

Enable interrupts.

void
CORE_ExitCritical(CORE_irqState_t irqState)

Exit a CRITICAL section.

void

Brief interrupt enable/disable sequence to allow handling of pending interrupts.

Enter a CRITICAL section.

void

Disable interrupts.

void

Enable interrupts.

void
CORE_ExitAtomic(CORE_irqState_t irqState)

Exit an ATOMIC section.

void

Brief interrupt enable/disable sequence to allow handling of pending interrupts.

Enter an ATOMIC section.

bool

Check whether the current CPU operation mode is handler mode.

bool

Check if interrupts are disabled.

void
CORE_EnterNvicMask(CORE_nvicMask_t *nvicState, const CORE_nvicMask_t *disable)

Enter a NVIC mask section.

void
CORE_NvicDisableMask(const CORE_nvicMask_t *disable)

Disable NVIC interrupts.

void
CORE_NvicEnableMask(const CORE_nvicMask_t *enable)

Set current NVIC interrupt enable mask.

void
CORE_YieldNvicMask(const CORE_nvicMask_t *enable)

Brief NVIC interrupt enable/disable sequence to allow handling of pending interrupts.

void
CORE_NvicMaskSetIRQ(IRQn_Type irqN, CORE_nvicMask_t *mask)

Utility function to set an IRQn bit in a NVIC enable/disable mask.

void
CORE_NvicMaskClearIRQ(IRQn_Type irqN, CORE_nvicMask_t *mask)

Utility function to clear an IRQn bit in a NVIC enable/disable mask.

bool
CORE_IrqIsBlocked(IRQn_Type irqN)

Check if a specific interrupt is disabled or blocked.

void
CORE_GetNvicEnabledMask(CORE_nvicMask_t *mask)

Get the current NVIC enable mask state.

bool
CORE_GetNvicMaskDisableState(const CORE_nvicMask_t *mask)

Get NVIC disable state for a given mask.

bool
CORE_NvicIRQDisabled(IRQn_Type irqN)

Check if an NVIC interrupt is disabled.

void *

Utility function to get the handler for a specific interrupt.

void
CORE_SetNvicRamTableHandler(IRQn_Type irqN, void *handler)

Utility function to set the handler for a specific interrupt.

void
CORE_InitNvicVectorTable(uint32_t *sourceTable, uint32_t sourceSize, uint32_t *targetTable, uint32_t targetSize, void *defaultHandler, bool overwriteActive)

Initialize an interrupt vector table by copying table entries from a source to a target table.

void
cycle_counter_start(dwt_cycle_counter_handle_t *handle)

Start a recording.

void
cycle_counter_stop(dwt_cycle_counter_handle_t *handle)

Stop a recording.

uint32_t

Returns the max time spent in critical section.

uint32_t

Returns the max time spent in atomic section.

void

Clears the max time spent in atomic section.

void

Clears the max time spent in atomic section.

Macros#

#define

Use PRIMASK register to disable interrupts in ATOMIC sections.

#define

Use BASEPRI register to disable interrupts in ATOMIC sections.

#define

The interrupt priority level disabled within ATOMIC regions.

#define
CORE_DECLARE_IRQ_STATE CORE_irqState_t irqState

Allocate storage for PRIMASK or BASEPRI value for use by CORE_ENTER/EXIT_ATOMIC() and CORE_ENTER/EXIT_CRITICAL() macros.

#define

CRITICAL style interrupt disable.

#define

CRITICAL style interrupt enable.

#define

Convenience macro for implementing a CRITICAL section.

#define

Enter CRITICAL section.

#define

Exit CRITICAL section.

#define

CRITICAL style yield.

#define

ATOMIC style interrupt disable.

#define

ATOMIC style interrupt enable.

#define

Convenience macro for implementing an ATOMIC section.

#define

Enter ATOMIC section.

#define

Exit ATOMIC section.

#define

ATOMIC style yield.

#define

Check if IRQ is disabled.

#define

Check if inside an IRQ handler.

#define

Placeholder for optional interrupt handler entry code.

#define

Placeholder for optional interrupt handler exit code.

#define
CORE_NVIC_REG_WORDS ((EXT_IRQ_COUNT + 31) / 32)

Number of words in a NVIC mask set.

#define

Number of entries in a default interrupt vector table.

#define

Highest priority for core interrupt.

#define

Default priority for core interrupt.

#define

Lowest priority for core interrupt.

#define
CORE_ATOMIC_METHOD_DEFAULT CORE_ATOMIC_METHOD_BASEPRI

Default method to disable interrupts in ATOMIC sections.

#define
CORE_ATOMIC_METHOD CORE_ATOMIC_METHOD_PRIMASK

Specify which method to use when implementing ATOMIC sections.

#define
CORE_DECLARE_NVIC_STATE CORE_nvicMask_t nvicState

Allocate storage for NVIC interrupt masks for use by CORE_ENTER/EXIT_NVIC() macros.

#define

Allocate storage for NVIC interrupt masks.

#define

Allocate storage for and zero initialize NVIC interrupt mask.

#define

NVIC mask style interrupt disable.

#define

NVIC mask style interrupt enable.

#define
CORE_NVIC_SECTION (mask, yourcode)

Convenience macro for implementing a NVIC mask section.

#define
CORE_ENTER_NVIC (disable)

Enter NVIC mask section.

#define

Exit NVIC mask section.

#define

NVIC maks style yield.

#define

Allocate storage for PRIMASK or BASEPRI value for use by CORE_ENTER/EXIT_ATOMIC() and CORE_ENTER/EXIT_CRITICAL() macros.

#define

CRITICAL style interrupt disable.

#define

CRITICAL style interrupt enable.

#define

Convenience macro for implementing a CRITICAL section.

#define

Enter CRITICAL section.

#define

Exit CRITICAL section.

#define

CRITICAL style yield.

#define

ATOMIC style interrupt disable.

#define

ATOMIC style interrupt enable.

#define

Convenience macro for implementing an ATOMIC section.

#define

Enter ATOMIC section.

#define

Exit ATOMIC section.

#define

ATOMIC style yield.

Typedef Documentation#

CORE_irqState_t#

typedef uint32_t CORE_irqState_t

Storage for PRIMASK or BASEPRI value.


CORE_irqState_t#

typedef uint32_t CORE_irqState_t

Storage for PRIMASK or BASEPRI value.


Function Documentation#

CORE_CriticalDisableIrq#

void CORE_CriticalDisableIrq (void )

Disable interrupts.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Disable all interrupts by setting PRIMASK. (Fault exception handlers will still be enabled).


CORE_CriticalEnableIrq#

void CORE_CriticalEnableIrq (void )

Enable interrupts.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Enable interrupts by clearing PRIMASK.


CORE_ExitCritical#

void CORE_ExitCritical (CORE_irqState_t irqState)

Exit a CRITICAL section.

Parameters
TypeDirectionArgument NameDescription
CORE_irqState_t[in]irqState

The interrupt priority blocking level to restore to PRIMASK when exiting the CRITICAL section. This value is usually the one returned by a prior call to CORE_EnterCritical().


CORE_YieldCritical#

void CORE_YieldCritical (void )

Brief interrupt enable/disable sequence to allow handling of pending interrupts.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • Usually used within a CRITICAL section.


CORE_EnterCritical#

CORE_irqState_t CORE_EnterCritical (void )

Enter a CRITICAL section.

Parameters
TypeDirectionArgument NameDescription
voidN/A

When a CRITICAL section is entered, all interrupts (except fault handlers) are disabled.

Returns

  • The value of PRIMASK register prior to the CRITICAL section entry.


CORE_AtomicDisableIrq#

void CORE_AtomicDisableIrq (void )

Disable interrupts.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Disable interrupts with a priority lower or equal to CORE_ATOMIC_BASE_PRIORITY_LEVEL. Sets core BASEPRI register to CORE_ATOMIC_BASE_PRIORITY_LEVEL.

Note


CORE_AtomicEnableIrq#

void CORE_AtomicEnableIrq (void )

Enable interrupts.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Enable interrupts by setting core BASEPRI register to 0.

Note


CORE_ExitAtomic#

void CORE_ExitAtomic (CORE_irqState_t irqState)

Exit an ATOMIC section.

Parameters
TypeDirectionArgument NameDescription
CORE_irqState_t[in]irqState

The interrupt priority blocking level to restore to BASEPRI when exiting the ATOMIC section. This value is usually the one returned by a prior call to CORE_EnterAtomic().

Note


CORE_YieldAtomic#

void CORE_YieldAtomic (void )

Brief interrupt enable/disable sequence to allow handling of pending interrupts.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note


CORE_EnterAtomic#

CORE_irqState_t CORE_EnterAtomic (void )

Enter an ATOMIC section.

Parameters
TypeDirectionArgument NameDescription
voidN/A

When an ATOMIC section is entered, interrupts with priority lower or equal to CORE_ATOMIC_BASE_PRIORITY_LEVEL are disabled.

Note

Returns

  • The value of BASEPRI register prior to ATOMIC section entry.


CORE_InIrqContext#

bool CORE_InIrqContext (void )

Check whether the current CPU operation mode is handler mode.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • True if the CPU is in handler mode (currently executing an interrupt handler).
    False if the CPU is in thread mode.


CORE_IrqIsDisabled#

bool CORE_IrqIsDisabled (void )

Check if interrupts are disabled.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • True if interrupts are disabled.


CORE_EnterNvicMask#

void CORE_EnterNvicMask (CORE_nvicMask_t * nvicState, const CORE_nvicMask_t * disable)

Enter a NVIC mask section.

Parameters
TypeDirectionArgument NameDescription
CORE_nvicMask_t *[out]nvicState

Return NVIC interrupts enable mask prior to section entry.

const CORE_nvicMask_t *[in]disable

A mask specifying which NVIC interrupts to disable within the section.

When a NVIC mask section is entered, specified NVIC interrupts are disabled.


CORE_NvicDisableMask#

void CORE_NvicDisableMask (const CORE_nvicMask_t * disable)

Disable NVIC interrupts.

Parameters
TypeDirectionArgument NameDescription
const CORE_nvicMask_t *[in]disable

A mask specifying which NVIC interrupts to disable.


CORE_NvicEnableMask#

void CORE_NvicEnableMask (const CORE_nvicMask_t * enable)

Set current NVIC interrupt enable mask.

Parameters
TypeDirectionArgument NameDescription
const CORE_nvicMask_t *[out]enable

A mask specifying which NVIC interrupts are currently enabled.


CORE_YieldNvicMask#

void CORE_YieldNvicMask (const CORE_nvicMask_t * enable)

Brief NVIC interrupt enable/disable sequence to allow handling of pending interrupts.

Parameters
TypeDirectionArgument NameDescription
const CORE_nvicMask_t *[in]enable

A mask specifying which NVIC interrupts to briefly enable.

Note

  • Usually used within an NVIC mask section.


CORE_NvicMaskSetIRQ#

void CORE_NvicMaskSetIRQ (IRQn_Type irqN, CORE_nvicMask_t * mask)

Utility function to set an IRQn bit in a NVIC enable/disable mask.

Parameters
TypeDirectionArgument NameDescription
IRQn_Type[in]irqN

The IRQn_Type enumerator for the interrupt.

CORE_nvicMask_t *[inout]mask

The mask to set the interrupt bit in.


CORE_NvicMaskClearIRQ#

void CORE_NvicMaskClearIRQ (IRQn_Type irqN, CORE_nvicMask_t * mask)

Utility function to clear an IRQn bit in a NVIC enable/disable mask.

Parameters
TypeDirectionArgument NameDescription
IRQn_Type[in]irqN

The IRQn_Type enumerator for the interrupt.

CORE_nvicMask_t *[inout]mask

The mask to clear the interrupt bit in.


CORE_IrqIsBlocked#

bool CORE_IrqIsBlocked (IRQn_Type irqN)

Check if a specific interrupt is disabled or blocked.

Parameters
TypeDirectionArgument NameDescription
IRQn_Type[in]irqN

The IRQn_Type enumerator for the interrupt to check.

Returns

  • True if the interrupt is disabled or blocked.


CORE_GetNvicEnabledMask#

void CORE_GetNvicEnabledMask (CORE_nvicMask_t * mask)

Get the current NVIC enable mask state.

Parameters
TypeDirectionArgument NameDescription
CORE_nvicMask_t *[out]mask

The current NVIC enable mask.


CORE_GetNvicMaskDisableState#

bool CORE_GetNvicMaskDisableState (const CORE_nvicMask_t * mask)

Get NVIC disable state for a given mask.

Parameters
TypeDirectionArgument NameDescription
const CORE_nvicMask_t *[in]mask

An NVIC mask to check.

Returns

  • True if all NVIC interrupt mask bits are clear.


CORE_NvicIRQDisabled#

bool CORE_NvicIRQDisabled (IRQn_Type irqN)

Check if an NVIC interrupt is disabled.

Parameters
TypeDirectionArgument NameDescription
IRQn_Type[in]irqN

The IRQn_Type enumerator for the interrupt to check.

Returns

  • True if the interrupt is disabled.


CORE_GetNvicRamTableHandler#

void * CORE_GetNvicRamTableHandler (IRQn_Type irqN)

Utility function to get the handler for a specific interrupt.

Parameters
TypeDirectionArgument NameDescription
IRQn_Type[in]irqN

The IRQn_Type enumerator for the interrupt.

Returns

  • The handler address.

Note

  • Uses the interrupt vector table defined by the current VTOR register value.


CORE_SetNvicRamTableHandler#

void CORE_SetNvicRamTableHandler (IRQn_Type irqN, void * handler)

Utility function to set the handler for a specific interrupt.

Parameters
TypeDirectionArgument NameDescription
IRQn_Type[in]irqN

The IRQn_Type enumerator for the interrupt.

void *[in]handler

The handler address.

Note

  • Uses the interrupt vector table defined by the current VTOR register value.


CORE_InitNvicVectorTable#

void CORE_InitNvicVectorTable (uint32_t * sourceTable, uint32_t sourceSize, uint32_t * targetTable, uint32_t targetSize, void * defaultHandler, bool overwriteActive)

Initialize an interrupt vector table by copying table entries from a source to a target table.

Parameters
TypeDirectionArgument NameDescription
uint32_t *[in]sourceTable

The address of the source vector table.

uint32_t[in]sourceSize

A number of entries in the source vector table.

uint32_t *[in]targetTable

The address of the target (new) vector table.

uint32_t[in]targetSize

A number of entries in the target vector table.

void *[in]defaultHandler

An address of the interrupt handler used for target entries for which where there is no corresponding source entry (i.e., the target table is larger than the source table).

bool[in]overwriteActive

When true, a target table entry is always overwritten with the corresponding source entry. If false, a target table entry is only overwritten if it is zero. This makes it possible for an application to partly initialize a target table before passing it to this function.

Note

  • This function will set a new VTOR register value.


cycle_counter_start#

static void cycle_counter_start (dwt_cycle_counter_handle_t * handle)

Start a recording.

Parameters
TypeDirectionArgument NameDescription
dwt_cycle_counter_handle_t *[in]handle

Pointer to initialized counter handle.

Note

  • SL_EMLIB_CORE_ENABLE_INTERRUPT_DISABLED_TIMING must be enabled.


cycle_counter_stop#

static void cycle_counter_stop (dwt_cycle_counter_handle_t * handle)

Stop a recording.

Parameters
TypeDirectionArgument NameDescription
dwt_cycle_counter_handle_t *[in]handle

Pointer to initialized counter handle.

Note

  • SL_EMLIB_CORE_ENABLE_INTERRUPT_DISABLED_TIMING must be enabled.


CORE_get_max_time_critical_section#

uint32_t CORE_get_max_time_critical_section (void )

Returns the max time spent in critical section.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • The max time spent in critical section.

Note

  • SL_EMLIB_CORE_ENABLE_INTERRUPT_DISABLED_TIMING must be enabled.


CORE_get_max_time_atomic_section#

uint32_t CORE_get_max_time_atomic_section (void )

Returns the max time spent in atomic section.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • The max time spent in atomic section.

Note

  • SL_EMLIB_CORE_ENABLE_INTERRUPT_DISABLED_TIMING must be enabled.


CORE_clear_max_time_critical_section#

void CORE_clear_max_time_critical_section (void )

Clears the max time spent in atomic section.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • SL_EMLIB_CORE_ENABLE_INTERRUPT_DISABLED_TIMING must be enabled.


CORE_clear_max_time_atomic_section#

void CORE_clear_max_time_atomic_section (void )

Clears the max time spent in atomic section.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • SL_EMLIB_CORE_ENABLE_INTERRUPT_DISABLED_TIMING must be enabled.


Macro Definition Documentation#

CORE_ATOMIC_METHOD_PRIMASK#

#define CORE_ATOMIC_METHOD_PRIMASK
Value:
0

Use PRIMASK register to disable interrupts in ATOMIC sections.


CORE_ATOMIC_METHOD_BASEPRI#

#define CORE_ATOMIC_METHOD_BASEPRI
Value:
1

Use BASEPRI register to disable interrupts in ATOMIC sections.


CORE_ATOMIC_BASE_PRIORITY_LEVEL#

#define CORE_ATOMIC_BASE_PRIORITY_LEVEL
Value:
3

The interrupt priority level disabled within ATOMIC regions.

Interrupts with priority level equal to or lower than this definition will be disabled within ATOMIC regions.


CORE_DECLARE_IRQ_STATE#

#define CORE_DECLARE_IRQ_STATE
Value:
CORE_irqState_t irqState

Allocate storage for PRIMASK or BASEPRI value for use by CORE_ENTER/EXIT_ATOMIC() and CORE_ENTER/EXIT_CRITICAL() macros.


CORE_CRITICAL_IRQ_DISABLE#

#define CORE_CRITICAL_IRQ_DISABLE
Value:
()

CRITICAL style interrupt disable.


CORE_CRITICAL_IRQ_ENABLE#

#define CORE_CRITICAL_IRQ_ENABLE
Value:
()

CRITICAL style interrupt enable.


CORE_CRITICAL_SECTION#

#define CORE_CRITICAL_SECTION
Value:
{ \
CORE_DECLARE_IRQ_STATE; \
CORE_ENTER_CRITICAL(); \
{ \
yourcode \
} \
CORE_EXIT_CRITICAL(); \
}

Convenience macro for implementing a CRITICAL section.


CORE_ENTER_CRITICAL#

#define CORE_ENTER_CRITICAL
Value:
()

Enter CRITICAL section.

Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.


CORE_EXIT_CRITICAL#

#define CORE_EXIT_CRITICAL
Value:
()

Exit CRITICAL section.

Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.


CORE_YIELD_CRITICAL#

#define CORE_YIELD_CRITICAL
Value:
()

CRITICAL style yield.


CORE_ATOMIC_IRQ_DISABLE#

#define CORE_ATOMIC_IRQ_DISABLE
Value:
()

ATOMIC style interrupt disable.


CORE_ATOMIC_IRQ_ENABLE#

#define CORE_ATOMIC_IRQ_ENABLE
Value:
()

ATOMIC style interrupt enable.


CORE_ATOMIC_SECTION#

#define CORE_ATOMIC_SECTION
Value:
{ \
CORE_DECLARE_IRQ_STATE; \
CORE_ENTER_ATOMIC(); \
{ \
yourcode \
} \
CORE_EXIT_ATOMIC(); \
}

Convenience macro for implementing an ATOMIC section.


CORE_ENTER_ATOMIC#

#define CORE_ENTER_ATOMIC
Value:
()

Enter ATOMIC section.

Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.


CORE_EXIT_ATOMIC#

#define CORE_EXIT_ATOMIC
Value:
()

Exit ATOMIC section.

Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.


CORE_YIELD_ATOMIC#

#define CORE_YIELD_ATOMIC
Value:
()

ATOMIC style yield.


CORE_IRQ_DISABLED#

#define CORE_IRQ_DISABLED
Value:
()

Check if IRQ is disabled.


CORE_IN_IRQ_CONTEXT#

#define CORE_IN_IRQ_CONTEXT
Value:
()

Check if inside an IRQ handler.


CORE_INTERRUPT_ENTRY#

#define CORE_INTERRUPT_ENTRY

Placeholder for optional interrupt handler entry code.

This might be needed when working with an RTOS.


CORE_INTERRUPT_EXIT#

#define CORE_INTERRUPT_EXIT

Placeholder for optional interrupt handler exit code.

This might be needed when working with an RTOS.


CORE_NVIC_REG_WORDS#

#define CORE_NVIC_REG_WORDS
Value:
((EXT_IRQ_COUNT + 31) / 32)

Number of words in a NVIC mask set.


CORE_DEFAULT_VECTOR_TABLE_ENTRIES#

#define CORE_DEFAULT_VECTOR_TABLE_ENTRIES
Value:
(EXT_IRQ_COUNT + 16)

Number of entries in a default interrupt vector table.


CORE_INTERRUPT_HIGHEST_PRIORITY#

#define CORE_INTERRUPT_HIGHEST_PRIORITY
Value:
0

Highest priority for core interrupt.


CORE_INTERRUPT_DEFAULT_PRIORITY#

#define CORE_INTERRUPT_DEFAULT_PRIORITY
Value:
5

Default priority for core interrupt.


CORE_INTERRUPT_LOWEST_PRIORITY#

#define CORE_INTERRUPT_LOWEST_PRIORITY
Value:
7

Lowest priority for core interrupt.


CORE_ATOMIC_METHOD_DEFAULT#

#define CORE_ATOMIC_METHOD_DEFAULT
Value:
CORE_ATOMIC_METHOD_BASEPRI

Default method to disable interrupts in ATOMIC sections.


CORE_ATOMIC_METHOD#

#define CORE_ATOMIC_METHOD
Value:
CORE_ATOMIC_METHOD_PRIMASK

Specify which method to use when implementing ATOMIC sections.

You can select between BASEPRI or PRIMASK method. Note

  • On Cortex-M0+ devices only PRIMASK can be used.


CORE_DECLARE_NVIC_STATE#

#define CORE_DECLARE_NVIC_STATE
Value:
CORE_nvicMask_t nvicState

Allocate storage for NVIC interrupt masks for use by CORE_ENTER/EXIT_NVIC() macros.


CORE_DECLARE_NVIC_MASK#

#define CORE_DECLARE_NVIC_MASK
Value:
(x)

Allocate storage for NVIC interrupt masks.


CORE_DECLARE_NVIC_ZEROMASK#

#define CORE_DECLARE_NVIC_ZEROMASK
Value:
(x)

Allocate storage for and zero initialize NVIC interrupt mask.


CORE_NVIC_DISABLE#

#define CORE_NVIC_DISABLE
Value:
(mask)

NVIC mask style interrupt disable.


CORE_NVIC_ENABLE#

#define CORE_NVIC_ENABLE
Value:
(mask)

NVIC mask style interrupt enable.


CORE_NVIC_SECTION#

#define CORE_NVIC_SECTION
Value:
{ \
CORE_DECLARE_NVIC_STATE; \
CORE_ENTER_NVIC(mask); \
{ \
yourcode \
} \
CORE_EXIT_NVIC(); \
}

Convenience macro for implementing a NVIC mask section.


CORE_ENTER_NVIC#

#define CORE_ENTER_NVIC
Value:
(disable)

Enter NVIC mask section.

Assumes that a CORE_DECLARE_NVIC_STATE exist in scope.


CORE_EXIT_NVIC#

#define CORE_EXIT_NVIC
Value:
()

Exit NVIC mask section.

Assumes that a CORE_DECLARE_NVIC_STATE exist in scope.


CORE_YIELD_NVIC#

#define CORE_YIELD_NVIC
Value:
(enable)

NVIC maks style yield.


CORE_DECLARE_IRQ_STATE#

#define CORE_DECLARE_IRQ_STATE

Allocate storage for PRIMASK or BASEPRI value for use by CORE_ENTER/EXIT_ATOMIC() and CORE_ENTER/EXIT_CRITICAL() macros.


CORE_CRITICAL_IRQ_DISABLE#

#define CORE_CRITICAL_IRQ_DISABLE

CRITICAL style interrupt disable.


CORE_CRITICAL_IRQ_ENABLE#

#define CORE_CRITICAL_IRQ_ENABLE

CRITICAL style interrupt enable.


CORE_CRITICAL_SECTION#

#define CORE_CRITICAL_SECTION
Value:
{ \
CORE_DECLARE_IRQ_STATE; \
CORE_ENTER_CRITICAL(); \
{ \
yourcode \
} \
CORE_EXIT_CRITICAL(); \
}

Convenience macro for implementing a CRITICAL section.


CORE_ENTER_CRITICAL#

#define CORE_ENTER_CRITICAL

Enter CRITICAL section.

Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.


CORE_EXIT_CRITICAL#

#define CORE_EXIT_CRITICAL

Exit CRITICAL section.

Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.


CORE_YIELD_CRITICAL#

#define CORE_YIELD_CRITICAL

CRITICAL style yield.


CORE_ATOMIC_IRQ_DISABLE#

#define CORE_ATOMIC_IRQ_DISABLE

ATOMIC style interrupt disable.


CORE_ATOMIC_IRQ_ENABLE#

#define CORE_ATOMIC_IRQ_ENABLE

ATOMIC style interrupt enable.


CORE_ATOMIC_SECTION#

#define CORE_ATOMIC_SECTION
Value:
{ \
CORE_DECLARE_IRQ_STATE; \
CORE_ENTER_ATOMIC(); \
{ \
yourcode \
} \
CORE_EXIT_ATOMIC(); \
}

Convenience macro for implementing an ATOMIC section.


CORE_ENTER_ATOMIC#

#define CORE_ENTER_ATOMIC

Enter ATOMIC section.

Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.


CORE_EXIT_ATOMIC#

#define CORE_EXIT_ATOMIC

Exit ATOMIC section.

Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.


CORE_YIELD_ATOMIC#

#define CORE_YIELD_ATOMIC

ATOMIC style yield.