ADC - Analog to Digital Converter#

Analog to Digital Converter (ADC) Peripheral API.

This module contains functions to control the ADC peripheral of Silicon Labs 32-bit MCUs and SoCs. The ADC is used to convert analog signals into a digital representation.

Modules#

ADC_Init_TypeDef

ADC_InitScanInput_TypeDef

ADC_InitScan_TypeDef

ADC_InitSingle_TypeDef

Enumerations#

enum
adcAcqTime1 = _ADC_SINGLECTRL_AT_1CYCLE
adcAcqTime2 = _ADC_SINGLECTRL_AT_2CYCLES
adcAcqTime4 = _ADC_SINGLECTRL_AT_4CYCLES
adcAcqTime8 = _ADC_SINGLECTRL_AT_8CYCLES
adcAcqTime16 = _ADC_SINGLECTRL_AT_16CYCLES
adcAcqTime32 = _ADC_SINGLECTRL_AT_32CYCLES
adcAcqTime64 = _ADC_SINGLECTRL_AT_64CYCLES
adcAcqTime128 = _ADC_SINGLECTRL_AT_128CYCLES
adcAcqTime256 = _ADC_SINGLECTRL_AT_256CYCLES
}

Acquisition time (in ADC clock cycles).

enum
adcOvsRateSel2 = _ADC_CTRL_OVSRSEL_X2
adcOvsRateSel4 = _ADC_CTRL_OVSRSEL_X4
adcOvsRateSel8 = _ADC_CTRL_OVSRSEL_X8
adcOvsRateSel16 = _ADC_CTRL_OVSRSEL_X16
adcOvsRateSel32 = _ADC_CTRL_OVSRSEL_X32
adcOvsRateSel64 = _ADC_CTRL_OVSRSEL_X64
adcOvsRateSel128 = _ADC_CTRL_OVSRSEL_X128
adcOvsRateSel256 = _ADC_CTRL_OVSRSEL_X256
adcOvsRateSel512 = _ADC_CTRL_OVSRSEL_X512
adcOvsRateSel1024 = _ADC_CTRL_OVSRSEL_X1024
adcOvsRateSel2048 = _ADC_CTRL_OVSRSEL_X2048
adcOvsRateSel4096 = _ADC_CTRL_OVSRSEL_X4096
}

Oversample rate select.

enum
adcPRSSELCh0 = _ADC_SINGLECTRLX_PRSSEL_PRSCH0
adcPRSSELCh1 = _ADC_SINGLECTRLX_PRSSEL_PRSCH1
adcPRSSELCh2 = _ADC_SINGLECTRLX_PRSSEL_PRSCH2
adcPRSSELCh3 = _ADC_SINGLECTRLX_PRSSEL_PRSCH3
adcPRSSELCh4 = _ADC_SINGLECTRLX_PRSSEL_PRSCH4
adcPRSSELCh5 = _ADC_SINGLECTRLX_PRSSEL_PRSCH5
adcPRSSELCh6 = _ADC_SINGLECTRLX_PRSSEL_PRSCH6
adcPRSSELCh7 = _ADC_SINGLECTRLX_PRSSEL_PRSCH7
adcPRSSELCh8 = _ADC_SINGLECTRLX_PRSSEL_PRSCH8
adcPRSSELCh9 = _ADC_SINGLECTRLX_PRSSEL_PRSCH9
adcPRSSELCh10 = _ADC_SINGLECTRLX_PRSSEL_PRSCH10
adcPRSSELCh11 = _ADC_SINGLECTRLX_PRSSEL_PRSCH11
adcPRSSELCh12 = _ADC_SINGLECTRLX_PRSSEL_PRSCH12
adcPRSSELCh13 = _ADC_SINGLECTRLX_PRSSEL_PRSCH13
adcPRSSELCh14 = _ADC_SINGLECTRLX_PRSSEL_PRSCH14
adcPRSSELCh15 = _ADC_SINGLECTRLX_PRSSEL_PRSCH15
}

Peripheral Reflex System signal used to trigger a single sample.

enum
adcRef1V25 = _ADC_SINGLECTRL_REF_1V25
adcRef2V5 = _ADC_SINGLECTRL_REF_2V5
adcRefVDD = _ADC_SINGLECTRL_REF_VDD
adcRef5V = _ADC_SINGLECTRL_REF_5V
adcRefExtSingle = _ADC_SINGLECTRL_REF_EXTSINGLE
adcRef2xExtDiff = _ADC_SINGLECTRL_REF_2XEXTDIFF
adcRef2xVDD = _ADC_SINGLECTRL_REF_2XVDD
adcRefVBGR = _ADC_SINGLECTRLX_VREFSEL_VBGR | ADC_CTRLX_VREFSEL_REG
adcRefVddxAtt = _ADC_SINGLECTRLX_VREFSEL_VDDXWATT | ADC_CTRLX_VREFSEL_REG
adcRefVPxAtt = _ADC_SINGLECTRLX_VREFSEL_VREFPWATT | ADC_CTRLX_VREFSEL_REG
adcRefP = _ADC_SINGLECTRLX_VREFSEL_VREFP | ADC_CTRLX_VREFSEL_REG
adcRefVEntropy = _ADC_SINGLECTRLX_VREFSEL_VENTROPY | ADC_CTRLX_VREFSEL_REG
adcRefVPNxAtt = _ADC_SINGLECTRLX_VREFSEL_VREFPNWATT | ADC_CTRLX_VREFSEL_REG
adcRefPN = _ADC_SINGLECTRLX_VREFSEL_VREFPN | ADC_CTRLX_VREFSEL_REG
}

ADC Reference.

enum
adcRes12Bit = _ADC_SINGLECTRL_RES_12BIT
adcRes8Bit = _ADC_SINGLECTRL_RES_8BIT
adcRes6Bit = _ADC_SINGLECTRL_RES_6BIT
adcResOVS = _ADC_SINGLECTRL_RES_OVS
}

Sample resolution.

enum
adcPosSelAPORT0XCH0 = _ADC_SINGLECTRL_POSSEL_APORT0XCH0
adcPosSelAPORT0XCH1 = _ADC_SINGLECTRL_POSSEL_APORT0XCH1
adcPosSelAPORT0XCH2 = _ADC_SINGLECTRL_POSSEL_APORT0XCH2
adcPosSelAPORT0XCH3 = _ADC_SINGLECTRL_POSSEL_APORT0XCH3
adcPosSelAPORT0XCH4 = _ADC_SINGLECTRL_POSSEL_APORT0XCH4
adcPosSelAPORT0XCH5 = _ADC_SINGLECTRL_POSSEL_APORT0XCH5
adcPosSelAPORT0XCH6 = _ADC_SINGLECTRL_POSSEL_APORT0XCH6
adcPosSelAPORT0XCH7 = _ADC_SINGLECTRL_POSSEL_APORT0XCH7
adcPosSelAPORT0XCH8 = _ADC_SINGLECTRL_POSSEL_APORT0XCH8
adcPosSelAPORT0XCH9 = _ADC_SINGLECTRL_POSSEL_APORT0XCH9
adcPosSelAPORT0XCH10 = _ADC_SINGLECTRL_POSSEL_APORT0XCH10
adcPosSelAPORT0XCH11 = _ADC_SINGLECTRL_POSSEL_APORT0XCH11
adcPosSelAPORT0XCH12 = _ADC_SINGLECTRL_POSSEL_APORT0XCH12
adcPosSelAPORT0XCH13 = _ADC_SINGLECTRL_POSSEL_APORT0XCH13
adcPosSelAPORT0XCH14 = _ADC_SINGLECTRL_POSSEL_APORT0XCH14
adcPosSelAPORT0XCH15 = _ADC_SINGLECTRL_POSSEL_APORT0XCH15
adcPosSelAPORT0YCH0 = _ADC_SINGLECTRL_POSSEL_APORT0YCH0
adcPosSelAPORT0YCH1 = _ADC_SINGLECTRL_POSSEL_APORT0YCH1
adcPosSelAPORT0YCH2 = _ADC_SINGLECTRL_POSSEL_APORT0YCH2
adcPosSelAPORT0YCH3 = _ADC_SINGLECTRL_POSSEL_APORT0YCH3
adcPosSelAPORT0YCH4 = _ADC_SINGLECTRL_POSSEL_APORT0YCH4
adcPosSelAPORT0YCH5 = _ADC_SINGLECTRL_POSSEL_APORT0YCH5
adcPosSelAPORT0YCH6 = _ADC_SINGLECTRL_POSSEL_APORT0YCH6
adcPosSelAPORT0YCH7 = _ADC_SINGLECTRL_POSSEL_APORT0YCH7
adcPosSelAPORT0YCH8 = _ADC_SINGLECTRL_POSSEL_APORT0YCH8
adcPosSelAPORT0YCH9 = _ADC_SINGLECTRL_POSSEL_APORT0YCH9
adcPosSelAPORT0YCH10 = _ADC_SINGLECTRL_POSSEL_APORT0YCH10
adcPosSelAPORT0YCH11 = _ADC_SINGLECTRL_POSSEL_APORT0YCH11
adcPosSelAPORT0YCH12 = _ADC_SINGLECTRL_POSSEL_APORT0YCH12
adcPosSelAPORT0YCH13 = _ADC_SINGLECTRL_POSSEL_APORT0YCH13
adcPosSelAPORT0YCH14 = _ADC_SINGLECTRL_POSSEL_APORT0YCH14
adcPosSelAPORT0YCH15 = _ADC_SINGLECTRL_POSSEL_APORT0YCH15
adcPosSelAPORT1XCH0 = _ADC_SINGLECTRL_POSSEL_APORT1XCH0
adcPosSelAPORT1YCH1 = _ADC_SINGLECTRL_POSSEL_APORT1YCH1
adcPosSelAPORT1XCH2 = _ADC_SINGLECTRL_POSSEL_APORT1XCH2
adcPosSelAPORT1YCH3 = _ADC_SINGLECTRL_POSSEL_APORT1YCH3
adcPosSelAPORT1XCH4 = _ADC_SINGLECTRL_POSSEL_APORT1XCH4
adcPosSelAPORT1YCH5 = _ADC_SINGLECTRL_POSSEL_APORT1YCH5
adcPosSelAPORT1XCH6 = _ADC_SINGLECTRL_POSSEL_APORT1XCH6
adcPosSelAPORT1YCH7 = _ADC_SINGLECTRL_POSSEL_APORT1YCH7
adcPosSelAPORT1XCH8 = _ADC_SINGLECTRL_POSSEL_APORT1XCH8
adcPosSelAPORT1YCH9 = _ADC_SINGLECTRL_POSSEL_APORT1YCH9
adcPosSelAPORT1XCH10 = _ADC_SINGLECTRL_POSSEL_APORT1XCH10
adcPosSelAPORT1YCH11 = _ADC_SINGLECTRL_POSSEL_APORT1YCH11
adcPosSelAPORT1XCH12 = _ADC_SINGLECTRL_POSSEL_APORT1XCH12
adcPosSelAPORT1YCH13 = _ADC_SINGLECTRL_POSSEL_APORT1YCH13
adcPosSelAPORT1XCH14 = _ADC_SINGLECTRL_POSSEL_APORT1XCH14
adcPosSelAPORT1YCH15 = _ADC_SINGLECTRL_POSSEL_APORT1YCH15
adcPosSelAPORT1XCH16 = _ADC_SINGLECTRL_POSSEL_APORT1XCH16
adcPosSelAPORT1YCH17 = _ADC_SINGLECTRL_POSSEL_APORT1YCH17
adcPosSelAPORT1XCH18 = _ADC_SINGLECTRL_POSSEL_APORT1XCH18
adcPosSelAPORT1YCH19 = _ADC_SINGLECTRL_POSSEL_APORT1YCH19
adcPosSelAPORT1XCH20 = _ADC_SINGLECTRL_POSSEL_APORT1XCH20
adcPosSelAPORT1YCH21 = _ADC_SINGLECTRL_POSSEL_APORT1YCH21
adcPosSelAPORT1XCH22 = _ADC_SINGLECTRL_POSSEL_APORT1XCH22
adcPosSelAPORT1YCH23 = _ADC_SINGLECTRL_POSSEL_APORT1YCH23
adcPosSelAPORT1XCH24 = _ADC_SINGLECTRL_POSSEL_APORT1XCH24
adcPosSelAPORT1YCH25 = _ADC_SINGLECTRL_POSSEL_APORT1YCH25
adcPosSelAPORT1XCH26 = _ADC_SINGLECTRL_POSSEL_APORT1XCH26
adcPosSelAPORT1YCH27 = _ADC_SINGLECTRL_POSSEL_APORT1YCH27
adcPosSelAPORT1XCH28 = _ADC_SINGLECTRL_POSSEL_APORT1XCH28
adcPosSelAPORT1YCH29 = _ADC_SINGLECTRL_POSSEL_APORT1YCH29
adcPosSelAPORT1XCH30 = _ADC_SINGLECTRL_POSSEL_APORT1XCH30
adcPosSelAPORT1YCH31 = _ADC_SINGLECTRL_POSSEL_APORT1YCH31
adcPosSelAPORT2YCH0 = _ADC_SINGLECTRL_POSSEL_APORT2YCH0
adcPosSelAPORT2XCH1 = _ADC_SINGLECTRL_POSSEL_APORT2XCH1
adcPosSelAPORT2YCH2 = _ADC_SINGLECTRL_POSSEL_APORT2YCH2
adcPosSelAPORT2XCH3 = _ADC_SINGLECTRL_POSSEL_APORT2XCH3
adcPosSelAPORT2YCH4 = _ADC_SINGLECTRL_POSSEL_APORT2YCH4
adcPosSelAPORT2XCH5 = _ADC_SINGLECTRL_POSSEL_APORT2XCH5
adcPosSelAPORT2YCH6 = _ADC_SINGLECTRL_POSSEL_APORT2YCH6
adcPosSelAPORT2XCH7 = _ADC_SINGLECTRL_POSSEL_APORT2XCH7
adcPosSelAPORT2YCH8 = _ADC_SINGLECTRL_POSSEL_APORT2YCH8
adcPosSelAPORT2XCH9 = _ADC_SINGLECTRL_POSSEL_APORT2XCH9
adcPosSelAPORT2YCH10 = _ADC_SINGLECTRL_POSSEL_APORT2YCH10
adcPosSelAPORT2XCH11 = _ADC_SINGLECTRL_POSSEL_APORT2XCH11
adcPosSelAPORT2YCH12 = _ADC_SINGLECTRL_POSSEL_APORT2YCH12
adcPosSelAPORT2XCH13 = _ADC_SINGLECTRL_POSSEL_APORT2XCH13
adcPosSelAPORT2YCH14 = _ADC_SINGLECTRL_POSSEL_APORT2YCH14
adcPosSelAPORT2XCH15 = _ADC_SINGLECTRL_POSSEL_APORT2XCH15
adcPosSelAPORT2YCH16 = _ADC_SINGLECTRL_POSSEL_APORT2YCH16
adcPosSelAPORT2XCH17 = _ADC_SINGLECTRL_POSSEL_APORT2XCH17
adcPosSelAPORT2YCH18 = _ADC_SINGLECTRL_POSSEL_APORT2YCH18
adcPosSelAPORT2XCH19 = _ADC_SINGLECTRL_POSSEL_APORT2XCH19
adcPosSelAPORT2YCH20 = _ADC_SINGLECTRL_POSSEL_APORT2YCH20
adcPosSelAPORT2XCH21 = _ADC_SINGLECTRL_POSSEL_APORT2XCH21
adcPosSelAPORT2YCH22 = _ADC_SINGLECTRL_POSSEL_APORT2YCH22
adcPosSelAPORT2XCH23 = _ADC_SINGLECTRL_POSSEL_APORT2XCH23
adcPosSelAPORT2YCH24 = _ADC_SINGLECTRL_POSSEL_APORT2YCH24
adcPosSelAPORT2XCH25 = _ADC_SINGLECTRL_POSSEL_APORT2XCH25
adcPosSelAPORT2YCH26 = _ADC_SINGLECTRL_POSSEL_APORT2YCH26
adcPosSelAPORT2XCH27 = _ADC_SINGLECTRL_POSSEL_APORT2XCH27
adcPosSelAPORT2YCH28 = _ADC_SINGLECTRL_POSSEL_APORT2YCH28
adcPosSelAPORT2XCH29 = _ADC_SINGLECTRL_POSSEL_APORT2XCH29
adcPosSelAPORT2YCH30 = _ADC_SINGLECTRL_POSSEL_APORT2YCH30
adcPosSelAPORT2XCH31 = _ADC_SINGLECTRL_POSSEL_APORT2XCH31
adcPosSelAPORT3XCH0 = _ADC_SINGLECTRL_POSSEL_APORT3XCH0
adcPosSelAPORT3YCH1 = _ADC_SINGLECTRL_POSSEL_APORT3YCH1
adcPosSelAPORT3XCH2 = _ADC_SINGLECTRL_POSSEL_APORT3XCH2
adcPosSelAPORT3YCH3 = _ADC_SINGLECTRL_POSSEL_APORT3YCH3
adcPosSelAPORT3XCH4 = _ADC_SINGLECTRL_POSSEL_APORT3XCH4
adcPosSelAPORT3YCH5 = _ADC_SINGLECTRL_POSSEL_APORT3YCH5
adcPosSelAPORT3XCH6 = _ADC_SINGLECTRL_POSSEL_APORT3XCH6
adcPosSelAPORT3YCH7 = _ADC_SINGLECTRL_POSSEL_APORT3YCH7
adcPosSelAPORT3XCH8 = _ADC_SINGLECTRL_POSSEL_APORT3XCH8
adcPosSelAPORT3YCH9 = _ADC_SINGLECTRL_POSSEL_APORT3YCH9
adcPosSelAPORT3XCH10 = _ADC_SINGLECTRL_POSSEL_APORT3XCH10
adcPosSelAPORT3YCH11 = _ADC_SINGLECTRL_POSSEL_APORT3YCH11
adcPosSelAPORT3XCH12 = _ADC_SINGLECTRL_POSSEL_APORT3XCH12
adcPosSelAPORT3YCH13 = _ADC_SINGLECTRL_POSSEL_APORT3YCH13
adcPosSelAPORT3XCH14 = _ADC_SINGLECTRL_POSSEL_APORT3XCH14
adcPosSelAPORT3YCH15 = _ADC_SINGLECTRL_POSSEL_APORT3YCH15
adcPosSelAPORT3XCH16 = _ADC_SINGLECTRL_POSSEL_APORT3XCH16
adcPosSelAPORT3YCH17 = _ADC_SINGLECTRL_POSSEL_APORT3YCH17
adcPosSelAPORT3XCH18 = _ADC_SINGLECTRL_POSSEL_APORT3XCH18
adcPosSelAPORT3YCH19 = _ADC_SINGLECTRL_POSSEL_APORT3YCH19
adcPosSelAPORT3XCH20 = _ADC_SINGLECTRL_POSSEL_APORT3XCH20
adcPosSelAPORT3YCH21 = _ADC_SINGLECTRL_POSSEL_APORT3YCH21
adcPosSelAPORT3XCH22 = _ADC_SINGLECTRL_POSSEL_APORT3XCH22
adcPosSelAPORT3YCH23 = _ADC_SINGLECTRL_POSSEL_APORT3YCH23
adcPosSelAPORT3XCH24 = _ADC_SINGLECTRL_POSSEL_APORT3XCH24
adcPosSelAPORT3YCH25 = _ADC_SINGLECTRL_POSSEL_APORT3YCH25
adcPosSelAPORT3XCH26 = _ADC_SINGLECTRL_POSSEL_APORT3XCH26
adcPosSelAPORT3YCH27 = _ADC_SINGLECTRL_POSSEL_APORT3YCH27
adcPosSelAPORT3XCH28 = _ADC_SINGLECTRL_POSSEL_APORT3XCH28
adcPosSelAPORT3YCH29 = _ADC_SINGLECTRL_POSSEL_APORT3YCH29
adcPosSelAPORT3XCH30 = _ADC_SINGLECTRL_POSSEL_APORT3XCH30
adcPosSelAPORT3YCH31 = _ADC_SINGLECTRL_POSSEL_APORT3YCH31
adcPosSelAPORT4YCH0 = _ADC_SINGLECTRL_POSSEL_APORT4YCH0
adcPosSelAPORT4XCH1 = _ADC_SINGLECTRL_POSSEL_APORT4XCH1
adcPosSelAPORT4YCH2 = _ADC_SINGLECTRL_POSSEL_APORT4YCH2
adcPosSelAPORT4XCH3 = _ADC_SINGLECTRL_POSSEL_APORT4XCH3
adcPosSelAPORT4YCH4 = _ADC_SINGLECTRL_POSSEL_APORT4YCH4
adcPosSelAPORT4XCH5 = _ADC_SINGLECTRL_POSSEL_APORT4XCH5
adcPosSelAPORT4YCH6 = _ADC_SINGLECTRL_POSSEL_APORT4YCH6
adcPosSelAPORT4XCH7 = _ADC_SINGLECTRL_POSSEL_APORT4XCH7
adcPosSelAPORT4YCH8 = _ADC_SINGLECTRL_POSSEL_APORT4YCH8
adcPosSelAPORT4XCH9 = _ADC_SINGLECTRL_POSSEL_APORT4XCH9
adcPosSelAPORT4YCH10 = _ADC_SINGLECTRL_POSSEL_APORT4YCH10
adcPosSelAPORT4XCH11 = _ADC_SINGLECTRL_POSSEL_APORT4XCH11
adcPosSelAPORT4YCH12 = _ADC_SINGLECTRL_POSSEL_APORT4YCH12
adcPosSelAPORT4XCH13 = _ADC_SINGLECTRL_POSSEL_APORT4XCH13
adcPosSelAPORT4YCH14 = _ADC_SINGLECTRL_POSSEL_APORT4YCH14
adcPosSelAPORT4XCH15 = _ADC_SINGLECTRL_POSSEL_APORT4XCH15
adcPosSelAPORT4YCH16 = _ADC_SINGLECTRL_POSSEL_APORT4YCH16
adcPosSelAPORT4XCH17 = _ADC_SINGLECTRL_POSSEL_APORT4XCH17
adcPosSelAPORT4YCH18 = _ADC_SINGLECTRL_POSSEL_APORT4YCH18
adcPosSelAPORT4XCH19 = _ADC_SINGLECTRL_POSSEL_APORT4XCH19
adcPosSelAPORT4YCH20 = _ADC_SINGLECTRL_POSSEL_APORT4YCH20
adcPosSelAPORT4XCH21 = _ADC_SINGLECTRL_POSSEL_APORT4XCH21
adcPosSelAPORT4YCH22 = _ADC_SINGLECTRL_POSSEL_APORT4YCH22
adcPosSelAPORT4XCH23 = _ADC_SINGLECTRL_POSSEL_APORT4XCH23
adcPosSelAPORT4YCH24 = _ADC_SINGLECTRL_POSSEL_APORT4YCH24
adcPosSelAPORT4XCH25 = _ADC_SINGLECTRL_POSSEL_APORT4XCH25
adcPosSelAPORT4YCH26 = _ADC_SINGLECTRL_POSSEL_APORT4YCH26
adcPosSelAPORT4XCH27 = _ADC_SINGLECTRL_POSSEL_APORT4XCH27
adcPosSelAPORT4YCH28 = _ADC_SINGLECTRL_POSSEL_APORT4YCH28
adcPosSelAPORT4XCH29 = _ADC_SINGLECTRL_POSSEL_APORT4XCH29
adcPosSelAPORT4YCH30 = _ADC_SINGLECTRL_POSSEL_APORT4YCH30
adcPosSelAPORT4XCH31 = _ADC_SINGLECTRL_POSSEL_APORT4XCH31
adcPosSelAVDD = _ADC_SINGLECTRL_POSSEL_AVDD
adcPosSelBUVDD = _ADC_SINGLECTRL_POSSEL_BUVDD
adcPosSelDVDD = _ADC_SINGLECTRL_POSSEL_DVDD
adcPosSelPAVDD = _ADC_SINGLECTRL_POSSEL_PAVDD
adcPosSelDECOUPLE = _ADC_SINGLECTRL_POSSEL_DECOUPLE
adcPosSelIOVDD = _ADC_SINGLECTRL_POSSEL_IOVDD
adcPosSelIOVDD1 = _ADC_SINGLECTRL_POSSEL_IOVDD1
adcPosSelVSP = _ADC_SINGLECTRL_POSSEL_VSP
adcPosSelOPA2 = _ADC_SINGLECTRL_POSSEL_OPA2
adcPosSelTEMP = _ADC_SINGLECTRL_POSSEL_TEMP
adcPosSelDAC0OUT0 = _ADC_SINGLECTRL_POSSEL_DAC0OUT0
adcPosSelR5VOUT = _ADC_SINGLECTRL_POSSEL_R5VOUT
adcPosSelSP1 = _ADC_SINGLECTRL_POSSEL_SP1
adcPosSelSP2 = _ADC_SINGLECTRL_POSSEL_SP2
adcPosSelDAC0OUT1 = _ADC_SINGLECTRL_POSSEL_DAC0OUT1
adcPosSelSUBLSB = _ADC_SINGLECTRL_POSSEL_SUBLSB
adcPosSelOPA3 = _ADC_SINGLECTRL_POSSEL_OPA3
adcPosSelDEFAULT = _ADC_SINGLECTRL_POSSEL_DEFAULT
adcPosSelVSS = _ADC_SINGLECTRL_POSSEL_VSS
}

Positive input selection for single and scan conversion.

enum
adcNegSelAPORT0XCH0 = _ADC_SINGLECTRL_NEGSEL_APORT0XCH0
adcNegSelAPORT0XCH1 = _ADC_SINGLECTRL_NEGSEL_APORT0XCH1
adcNegSelAPORT0XCH2 = _ADC_SINGLECTRL_NEGSEL_APORT0XCH2
adcNegSelAPORT0XCH3 = _ADC_SINGLECTRL_NEGSEL_APORT0XCH3
adcNegSelAPORT0XCH4 = _ADC_SINGLECTRL_NEGSEL_APORT0XCH4
adcNegSelAPORT0XCH5 = _ADC_SINGLECTRL_NEGSEL_APORT0XCH5
adcNegSelAPORT0XCH6 = _ADC_SINGLECTRL_NEGSEL_APORT0XCH6
adcNegSelAPORT0XCH7 = _ADC_SINGLECTRL_NEGSEL_APORT0XCH7
adcNegSelAPORT0XCH8 = _ADC_SINGLECTRL_NEGSEL_APORT0XCH8
adcNegSelAPORT0XCH9 = _ADC_SINGLECTRL_NEGSEL_APORT0XCH9
adcNegSelAPORT0XCH10 = _ADC_SINGLECTRL_NEGSEL_APORT0XCH10
adcNegSelAPORT0XCH11 = _ADC_SINGLECTRL_NEGSEL_APORT0XCH11
adcNegSelAPORT0XCH12 = _ADC_SINGLECTRL_NEGSEL_APORT0XCH12
adcNegSelAPORT0XCH13 = _ADC_SINGLECTRL_NEGSEL_APORT0XCH13
adcNegSelAPORT0XCH14 = _ADC_SINGLECTRL_NEGSEL_APORT0XCH14
adcNegSelAPORT0XCH15 = _ADC_SINGLECTRL_NEGSEL_APORT0XCH15
adcNegSelAPORT0YCH0 = _ADC_SINGLECTRL_NEGSEL_APORT0YCH0
adcNegSelAPORT0YCH1 = _ADC_SINGLECTRL_NEGSEL_APORT0YCH1
adcNegSelAPORT0YCH2 = _ADC_SINGLECTRL_NEGSEL_APORT0YCH2
adcNegSelAPORT0YCH3 = _ADC_SINGLECTRL_NEGSEL_APORT0YCH3
adcNegSelAPORT0YCH4 = _ADC_SINGLECTRL_NEGSEL_APORT0YCH4
adcNegSelAPORT0YCH5 = _ADC_SINGLECTRL_NEGSEL_APORT0YCH5
adcNegSelAPORT0YCH6 = _ADC_SINGLECTRL_NEGSEL_APORT0YCH6
adcNegSelAPORT0YCH7 = _ADC_SINGLECTRL_NEGSEL_APORT0YCH7
adcNegSelAPORT0YCH8 = _ADC_SINGLECTRL_NEGSEL_APORT0YCH8
adcNegSelAPORT0YCH9 = _ADC_SINGLECTRL_NEGSEL_APORT0YCH9
adcNegSelAPORT0YCH10 = _ADC_SINGLECTRL_NEGSEL_APORT0YCH10
adcNegSelAPORT0YCH11 = _ADC_SINGLECTRL_NEGSEL_APORT0YCH11
adcNegSelAPORT0YCH12 = _ADC_SINGLECTRL_NEGSEL_APORT0YCH12
adcNegSelAPORT0YCH13 = _ADC_SINGLECTRL_NEGSEL_APORT0YCH13
adcNegSelAPORT0YCH14 = _ADC_SINGLECTRL_NEGSEL_APORT0YCH14
adcNegSelAPORT0YCH15 = _ADC_SINGLECTRL_NEGSEL_APORT0YCH15
adcNegSelAPORT1XCH0 = _ADC_SINGLECTRL_NEGSEL_APORT1XCH0
adcNegSelAPORT1YCH1 = _ADC_SINGLECTRL_NEGSEL_APORT1YCH1
adcNegSelAPORT1XCH2 = _ADC_SINGLECTRL_NEGSEL_APORT1XCH2
adcNegSelAPORT1YCH3 = _ADC_SINGLECTRL_NEGSEL_APORT1YCH3
adcNegSelAPORT1XCH4 = _ADC_SINGLECTRL_NEGSEL_APORT1XCH4
adcNegSelAPORT1YCH5 = _ADC_SINGLECTRL_NEGSEL_APORT1YCH5
adcNegSelAPORT1XCH6 = _ADC_SINGLECTRL_NEGSEL_APORT1XCH6
adcNegSelAPORT1YCH7 = _ADC_SINGLECTRL_NEGSEL_APORT1YCH7
adcNegSelAPORT1XCH8 = _ADC_SINGLECTRL_NEGSEL_APORT1XCH8
adcNegSelAPORT1YCH9 = _ADC_SINGLECTRL_NEGSEL_APORT1YCH9
adcNegSelAPORT1XCH10 = _ADC_SINGLECTRL_NEGSEL_APORT1XCH10
adcNegSelAPORT1YCH11 = _ADC_SINGLECTRL_NEGSEL_APORT1YCH11
adcNegSelAPORT1XCH12 = _ADC_SINGLECTRL_NEGSEL_APORT1XCH12
adcNegSelAPORT1YCH13 = _ADC_SINGLECTRL_NEGSEL_APORT1YCH13
adcNegSelAPORT1XCH14 = _ADC_SINGLECTRL_NEGSEL_APORT1XCH14
adcNegSelAPORT1YCH15 = _ADC_SINGLECTRL_NEGSEL_APORT1YCH15
adcNegSelAPORT1XCH16 = _ADC_SINGLECTRL_NEGSEL_APORT1XCH16
adcNegSelAPORT1YCH17 = _ADC_SINGLECTRL_NEGSEL_APORT1YCH17
adcNegSelAPORT1XCH18 = _ADC_SINGLECTRL_NEGSEL_APORT1XCH18
adcNegSelAPORT1YCH19 = _ADC_SINGLECTRL_NEGSEL_APORT1YCH19
adcNegSelAPORT1XCH20 = _ADC_SINGLECTRL_NEGSEL_APORT1XCH20
adcNegSelAPORT1YCH21 = _ADC_SINGLECTRL_NEGSEL_APORT1YCH21
adcNegSelAPORT1XCH22 = _ADC_SINGLECTRL_NEGSEL_APORT1XCH22
adcNegSelAPORT1YCH23 = _ADC_SINGLECTRL_NEGSEL_APORT1YCH23
adcNegSelAPORT1XCH24 = _ADC_SINGLECTRL_NEGSEL_APORT1XCH24
adcNegSelAPORT1YCH25 = _ADC_SINGLECTRL_NEGSEL_APORT1YCH25
adcNegSelAPORT1XCH26 = _ADC_SINGLECTRL_NEGSEL_APORT1XCH26
adcNegSelAPORT1YCH27 = _ADC_SINGLECTRL_NEGSEL_APORT1YCH27
adcNegSelAPORT1XCH28 = _ADC_SINGLECTRL_NEGSEL_APORT1XCH28
adcNegSelAPORT1YCH29 = _ADC_SINGLECTRL_NEGSEL_APORT1YCH29
adcNegSelAPORT1XCH30 = _ADC_SINGLECTRL_NEGSEL_APORT1XCH30
adcNegSelAPORT1YCH31 = _ADC_SINGLECTRL_NEGSEL_APORT1YCH31
adcNegSelAPORT2YCH0 = _ADC_SINGLECTRL_NEGSEL_APORT2YCH0
adcNegSelAPORT2XCH1 = _ADC_SINGLECTRL_NEGSEL_APORT2XCH1
adcNegSelAPORT2YCH2 = _ADC_SINGLECTRL_NEGSEL_APORT2YCH2
adcNegSelAPORT2XCH3 = _ADC_SINGLECTRL_NEGSEL_APORT2XCH3
adcNegSelAPORT2YCH4 = _ADC_SINGLECTRL_NEGSEL_APORT2YCH4
adcNegSelAPORT2XCH5 = _ADC_SINGLECTRL_NEGSEL_APORT2XCH5
adcNegSelAPORT2YCH6 = _ADC_SINGLECTRL_NEGSEL_APORT2YCH6
adcNegSelAPORT2XCH7 = _ADC_SINGLECTRL_NEGSEL_APORT2XCH7
adcNegSelAPORT2YCH8 = _ADC_SINGLECTRL_NEGSEL_APORT2YCH8
adcNegSelAPORT2XCH9 = _ADC_SINGLECTRL_NEGSEL_APORT2XCH9
adcNegSelAPORT2YCH10 = _ADC_SINGLECTRL_NEGSEL_APORT2YCH10
adcNegSelAPORT2XCH11 = _ADC_SINGLECTRL_NEGSEL_APORT2XCH11
adcNegSelAPORT2YCH12 = _ADC_SINGLECTRL_NEGSEL_APORT2YCH12
adcNegSelAPORT2XCH13 = _ADC_SINGLECTRL_NEGSEL_APORT2XCH13
adcNegSelAPORT2YCH14 = _ADC_SINGLECTRL_NEGSEL_APORT2YCH14
adcNegSelAPORT2XCH15 = _ADC_SINGLECTRL_NEGSEL_APORT2XCH15
adcNegSelAPORT2YCH16 = _ADC_SINGLECTRL_NEGSEL_APORT2YCH16
adcNegSelAPORT2XCH17 = _ADC_SINGLECTRL_NEGSEL_APORT2XCH17
adcNegSelAPORT2YCH18 = _ADC_SINGLECTRL_NEGSEL_APORT2YCH18
adcNegSelAPORT2XCH19 = _ADC_SINGLECTRL_NEGSEL_APORT2XCH19
adcNegSelAPORT2YCH20 = _ADC_SINGLECTRL_NEGSEL_APORT2YCH20
adcNegSelAPORT2XCH21 = _ADC_SINGLECTRL_NEGSEL_APORT2XCH21
adcNegSelAPORT2YCH22 = _ADC_SINGLECTRL_NEGSEL_APORT2YCH22
adcNegSelAPORT2XCH23 = _ADC_SINGLECTRL_NEGSEL_APORT2XCH23
adcNegSelAPORT2YCH24 = _ADC_SINGLECTRL_NEGSEL_APORT2YCH24
adcNegSelAPORT2XCH25 = _ADC_SINGLECTRL_NEGSEL_APORT2XCH25
adcNegSelAPORT2YCH26 = _ADC_SINGLECTRL_NEGSEL_APORT2YCH26
adcNegSelAPORT2XCH27 = _ADC_SINGLECTRL_NEGSEL_APORT2XCH27
adcNegSelAPORT2YCH28 = _ADC_SINGLECTRL_NEGSEL_APORT2YCH28
adcNegSelAPORT2XCH29 = _ADC_SINGLECTRL_NEGSEL_APORT2XCH29
adcNegSelAPORT2YCH30 = _ADC_SINGLECTRL_NEGSEL_APORT2YCH30
adcNegSelAPORT2XCH31 = _ADC_SINGLECTRL_NEGSEL_APORT2XCH31
adcNegSelAPORT3XCH0 = _ADC_SINGLECTRL_NEGSEL_APORT3XCH0
adcNegSelAPORT3YCH1 = _ADC_SINGLECTRL_NEGSEL_APORT3YCH1
adcNegSelAPORT3XCH2 = _ADC_SINGLECTRL_NEGSEL_APORT3XCH2
adcNegSelAPORT3YCH3 = _ADC_SINGLECTRL_NEGSEL_APORT3YCH3
adcNegSelAPORT3XCH4 = _ADC_SINGLECTRL_NEGSEL_APORT3XCH4
adcNegSelAPORT3YCH5 = _ADC_SINGLECTRL_NEGSEL_APORT3YCH5
adcNegSelAPORT3XCH6 = _ADC_SINGLECTRL_NEGSEL_APORT3XCH6
adcNegSelAPORT3YCH7 = _ADC_SINGLECTRL_NEGSEL_APORT3YCH7
adcNegSelAPORT3XCH8 = _ADC_SINGLECTRL_NEGSEL_APORT3XCH8
adcNegSelAPORT3YCH9 = _ADC_SINGLECTRL_NEGSEL_APORT3YCH9
adcNegSelAPORT3XCH10 = _ADC_SINGLECTRL_NEGSEL_APORT3XCH10
adcNegSelAPORT3YCH11 = _ADC_SINGLECTRL_NEGSEL_APORT3YCH11
adcNegSelAPORT3XCH12 = _ADC_SINGLECTRL_NEGSEL_APORT3XCH12
adcNegSelAPORT3YCH13 = _ADC_SINGLECTRL_NEGSEL_APORT3YCH13
adcNegSelAPORT3XCH14 = _ADC_SINGLECTRL_NEGSEL_APORT3XCH14
adcNegSelAPORT3YCH15 = _ADC_SINGLECTRL_NEGSEL_APORT3YCH15
adcNegSelAPORT3XCH16 = _ADC_SINGLECTRL_NEGSEL_APORT3XCH16
adcNegSelAPORT3YCH17 = _ADC_SINGLECTRL_NEGSEL_APORT3YCH17
adcNegSelAPORT3XCH18 = _ADC_SINGLECTRL_NEGSEL_APORT3XCH18
adcNegSelAPORT3YCH19 = _ADC_SINGLECTRL_NEGSEL_APORT3YCH19
adcNegSelAPORT3XCH20 = _ADC_SINGLECTRL_NEGSEL_APORT3XCH20
adcNegSelAPORT3YCH21 = _ADC_SINGLECTRL_NEGSEL_APORT3YCH21
adcNegSelAPORT3XCH22 = _ADC_SINGLECTRL_NEGSEL_APORT3XCH22
adcNegSelAPORT3YCH23 = _ADC_SINGLECTRL_NEGSEL_APORT3YCH23
adcNegSelAPORT3XCH24 = _ADC_SINGLECTRL_NEGSEL_APORT3XCH24
adcNegSelAPORT3YCH25 = _ADC_SINGLECTRL_NEGSEL_APORT3YCH25
adcNegSelAPORT3XCH26 = _ADC_SINGLECTRL_NEGSEL_APORT3XCH26
adcNegSelAPORT3YCH27 = _ADC_SINGLECTRL_NEGSEL_APORT3YCH27
adcNegSelAPORT3XCH28 = _ADC_SINGLECTRL_NEGSEL_APORT3XCH28
adcNegSelAPORT3YCH29 = _ADC_SINGLECTRL_NEGSEL_APORT3YCH29
adcNegSelAPORT3XCH30 = _ADC_SINGLECTRL_NEGSEL_APORT3XCH30
adcNegSelAPORT3YCH31 = _ADC_SINGLECTRL_NEGSEL_APORT3YCH31
adcNegSelAPORT4YCH0 = _ADC_SINGLECTRL_NEGSEL_APORT4YCH0
adcNegSelAPORT4XCH1 = _ADC_SINGLECTRL_NEGSEL_APORT4XCH1
adcNegSelAPORT4YCH2 = _ADC_SINGLECTRL_NEGSEL_APORT4YCH2
adcNegSelAPORT4XCH3 = _ADC_SINGLECTRL_NEGSEL_APORT4XCH3
adcNegSelAPORT4YCH4 = _ADC_SINGLECTRL_NEGSEL_APORT4YCH4
adcNegSelAPORT4XCH5 = _ADC_SINGLECTRL_NEGSEL_APORT4XCH5
adcNegSelAPORT4YCH6 = _ADC_SINGLECTRL_NEGSEL_APORT4YCH6
adcNegSelAPORT4XCH7 = _ADC_SINGLECTRL_NEGSEL_APORT4XCH7
adcNegSelAPORT4YCH8 = _ADC_SINGLECTRL_NEGSEL_APORT4YCH8
adcNegSelAPORT4XCH9 = _ADC_SINGLECTRL_NEGSEL_APORT4XCH9
adcNegSelAPORT4YCH10 = _ADC_SINGLECTRL_NEGSEL_APORT4YCH10
adcNegSelAPORT4XCH11 = _ADC_SINGLECTRL_NEGSEL_APORT4XCH11
adcNegSelAPORT4YCH12 = _ADC_SINGLECTRL_NEGSEL_APORT4YCH12
adcNegSelAPORT4XCH13 = _ADC_SINGLECTRL_NEGSEL_APORT4XCH13
adcNegSelAPORT4YCH14 = _ADC_SINGLECTRL_NEGSEL_APORT4YCH14
adcNegSelAPORT4XCH15 = _ADC_SINGLECTRL_NEGSEL_APORT4XCH15
adcNegSelAPORT4YCH16 = _ADC_SINGLECTRL_NEGSEL_APORT4YCH16
adcNegSelAPORT4XCH17 = _ADC_SINGLECTRL_NEGSEL_APORT4XCH17
adcNegSelAPORT4YCH18 = _ADC_SINGLECTRL_NEGSEL_APORT4YCH18
adcNegSelAPORT4XCH19 = _ADC_SINGLECTRL_NEGSEL_APORT4XCH19
adcNegSelAPORT4YCH20 = _ADC_SINGLECTRL_NEGSEL_APORT4YCH20
adcNegSelAPORT4XCH21 = _ADC_SINGLECTRL_NEGSEL_APORT4XCH21
adcNegSelAPORT4YCH22 = _ADC_SINGLECTRL_NEGSEL_APORT4YCH22
adcNegSelAPORT4XCH23 = _ADC_SINGLECTRL_NEGSEL_APORT4XCH23
adcNegSelAPORT4YCH24 = _ADC_SINGLECTRL_NEGSEL_APORT4YCH24
adcNegSelAPORT4XCH25 = _ADC_SINGLECTRL_NEGSEL_APORT4XCH25
adcNegSelAPORT4YCH26 = _ADC_SINGLECTRL_NEGSEL_APORT4YCH26
adcNegSelAPORT4XCH27 = _ADC_SINGLECTRL_NEGSEL_APORT4XCH27
adcNegSelAPORT4YCH28 = _ADC_SINGLECTRL_NEGSEL_APORT4YCH28
adcNegSelAPORT4XCH29 = _ADC_SINGLECTRL_NEGSEL_APORT4XCH29
adcNegSelAPORT4YCH30 = _ADC_SINGLECTRL_NEGSEL_APORT4YCH30
adcNegSelAPORT4XCH31 = _ADC_SINGLECTRL_NEGSEL_APORT4XCH31
adcNegSelTESTN = _ADC_SINGLECTRL_NEGSEL_TESTN
adcNegSelDEFAULT = _ADC_SINGLECTRL_NEGSEL_DEFAULT
adcNegSelVSS = _ADC_SINGLECTRL_NEGSEL_VSS
}

Negative input selection for single and scan conversion.

enum
adcScanInputGroup0 = 0
adcScanInputGroup1 = 1
adcScanInputGroup2 = 2
adcScanInputGroup3 = 3
}

ADC scan input groups.

enum
adcScanNegInput1 = 1
adcScanNegInput3 = 3
adcScanNegInput5 = 5
adcScanNegInput7 = 7
adcScanNegInput8 = 8
adcScanNegInput10 = 10
adcScanNegInput12 = 12
adcScanNegInput14 = 14
adcScanNegInputDefault = 0xFF
}

ADC scan alternative negative inputs.

enum
adcStartSingle = ADC_CMD_SINGLESTART
adcStartScan = ADC_CMD_SCANSTART
adcStartScanAndSingle = ADC_CMD_SCANSTART | ADC_CMD_SINGLESTART
}

ADC start command.

enum
adcWarmupNormal = _ADC_CTRL_WARMUPMODE_NORMAL
adcWarmupKeepInStandby = _ADC_CTRL_WARMUPMODE_KEEPINSTANDBY
adcWarmupKeepInSlowAcq = _ADC_CTRL_WARMUPMODE_KEEPINSLOWACC
adcWarmupKeepADCWarm = _ADC_CTRL_WARMUPMODE_KEEPADCWARM
}

Warm-up mode.

enum
adcEm2Disabled = 0
adcEm2ClockOnDemand = ADC_CTRL_ADCCLKMODE_ASYNC | ADC_CTRL_ASYNCCLKEN_ASNEEDED
adcEm2ClockAlwaysOn = ADC_CTRL_ADCCLKMODE_ASYNC | ADC_CTRL_ASYNCCLKEN_ALWAYSON
}

ADC EM2 clock configuration.

Functions#

void
ADC_Init(ADC_TypeDef *adc, const ADC_Init_TypeDef *init)

Initialize ADC.

void
ADC_ScanInputClear(ADC_InitScan_TypeDef *scanInit)

Clear ADC scan input configuration.

uint32_t
ADC_ScanSingleEndedInputAdd(ADC_InitScan_TypeDef *scanInit, ADC_ScanInputGroup_TypeDef inputGroup, ADC_PosSel_TypeDef singleEndedSel)

Initialize ADC scan single-ended input configuration.

uint32_t
ADC_ScanDifferentialInputAdd(ADC_InitScan_TypeDef *scanInit, ADC_ScanInputGroup_TypeDef inputGroup, ADC_PosSel_TypeDef posSel, ADC_ScanNegInput_TypeDef negInput)

Initialize the ADC scan differential input configuration.

void
ADC_InitScan(ADC_TypeDef *adc, const ADC_InitScan_TypeDef *init)

Initialize the ADC scan sequence.

void
ADC_InitSingle(ADC_TypeDef *adc, const ADC_InitSingle_TypeDef *init)

Initialize the single ADC sample conversion.

uint32_t
ADC_DataIdScanGet(ADC_TypeDef *adc, uint32_t *scanId)

Get a scan result and scan select ID.

uint8_t
ADC_PrescaleCalc(uint32_t adcFreq, uint32_t hfperFreq)

Calculate the prescaler value used to determine the ADC clock.

void
ADC_Reset(ADC_TypeDef *adc)

Reset ADC to a state that it was in after a hardware reset.

uint8_t
ADC_TimebaseCalc(uint32_t hfperFreq)

Calculate a timebase value to get a timebase providing at least 1 us.

uint32_t
ADC_DataSingleGet(ADC_TypeDef *adc)

Get a single conversion result.

uint32_t
ADC_DataSinglePeek(ADC_TypeDef *adc)

Peek single conversion result.

uint32_t
ADC_DataScanGet(ADC_TypeDef *adc)

Get a scan result.

uint32_t
ADC_DataScanPeek(ADC_TypeDef *adc)

Peek scan result.

void
ADC_IntClear(ADC_TypeDef *adc, uint32_t flags)

Clear one or more pending ADC interrupts.

void
ADC_IntDisable(ADC_TypeDef *adc, uint32_t flags)

Disable one or more ADC interrupts.

void
ADC_IntEnable(ADC_TypeDef *adc, uint32_t flags)

Enable one or more ADC interrupts.

uint32_t
ADC_IntGet(ADC_TypeDef *adc)

Get pending ADC interrupt flags.

uint32_t
ADC_IntGetEnabled(ADC_TypeDef *adc)

Get enabled and pending ADC interrupt flags.

void
ADC_IntSet(ADC_TypeDef *adc, uint32_t flags)

Set one or more pending ADC interrupts from software.

void
ADC_Start(ADC_TypeDef *adc, ADC_Start_TypeDef cmd)

Start scan sequence and/or single conversion.

Macros#

#define
ADC_CTRLX_VREFSEL_REG 0x80UL

Single and scan mode voltage references.

#define
ADC_SCANINPUTSEL_GROUP_NONE 0xFFU

Define none selected group for ADC_SCANINPUTSEL.

#define
ADC_SCANINPUTSEL_NONE undefined

Define none selected for ADC_SCANINPUTSEL.

#define
ADC_INIT_DEFAULT undefined

Default configuration for ADC initialization structure.

#define
ADC_INITSCAN_DEFAULT undefined

Default configuration for ADC scan initialization structure.

#define
ADC_INITSINGLE_DEFAULT undefined

Default configuration for ADC single conversion initialization structure.

Enumeration Documentation#

ADC_AcqTime_TypeDef#

ADC_AcqTime_TypeDef

Acquisition time (in ADC clock cycles).

Enumerator
adcAcqTime1

1 clock cycle.

adcAcqTime2

2 clock cycles.

adcAcqTime4

4 clock cycles.

adcAcqTime8

8 clock cycles.

adcAcqTime16

16 clock cycles.

adcAcqTime32

32 clock cycles.

adcAcqTime64

64 clock cycles.

adcAcqTime128

128 clock cycles.

adcAcqTime256

256 clock cycles.


Definition at line 53 of file platform/emlib/inc/em_adc.h

ADC_OvsRateSel_TypeDef#

ADC_OvsRateSel_TypeDef

Oversample rate select.

Enumerator
adcOvsRateSel2

2 samples per conversion result.

adcOvsRateSel4

4 samples per conversion result.

adcOvsRateSel8

8 samples per conversion result.

adcOvsRateSel16

16 samples per conversion result.

adcOvsRateSel32

32 samples per conversion result.

adcOvsRateSel64

64 samples per conversion result.

adcOvsRateSel128

128 samples per conversion result.

adcOvsRateSel256

256 samples per conversion result.

adcOvsRateSel512

512 samples per conversion result.

adcOvsRateSel1024

1024 samples per conversion result.

adcOvsRateSel2048

2048 samples per conversion result.

adcOvsRateSel4096

4096 samples per conversion result.


Definition at line 80 of file platform/emlib/inc/em_adc.h

ADC_PRSSEL_TypeDef#

ADC_PRSSEL_TypeDef

Peripheral Reflex System signal used to trigger a single sample.

Enumerator
adcPRSSELCh0

PRS channel 0.

adcPRSSELCh1

PRS channel 1.

adcPRSSELCh2

PRS channel 2.

adcPRSSELCh3

PRS channel 3.

adcPRSSELCh4

PRS channel 4.

adcPRSSELCh5

PRS channel 5.

adcPRSSELCh6

PRS channel 6.

adcPRSSELCh7

PRS channel 7.

adcPRSSELCh8

PRS channel 8.

adcPRSSELCh9

PRS channel 9.

adcPRSSELCh10

PRS channel 10.

adcPRSSELCh11

PRS channel 11.

adcPRSSELCh12

PRS channel 12.

adcPRSSELCh13

PRS channel 13.

adcPRSSELCh14

PRS channel 14.

adcPRSSELCh15

PRS channel 15.


Definition at line 119 of file platform/emlib/inc/em_adc.h

ADC_Ref_TypeDef#

ADC_Ref_TypeDef

ADC Reference.

Enumerator
adcRef1V25

Internal 1.25 V reference.

adcRef2V5

Internal 2.5 V reference.

adcRefVDD

Buffered VDD.

adcRef5V

Internal 5 V reference.

adcRefExtSingle

Single-ended external reference from pin 6.

adcRef2xExtDiff

Differential external reference from pin 6 and 7.

adcRef2xVDD

Unbuffered 2xVDD.

adcRefVBGR

Custom VFS: Internal Bandgap reference.

adcRefVddxAtt

Custom VFS: Scaled AVDD: AVDD * VREFATT.

adcRefVPxAtt

Custom VFS: Scaled singled ended external reference from pin 6: VREFP * VREFATT.

adcRefP

Custom VFS: Raw single-ended external reference from pin 6.

adcRefVEntropy

Custom VFS: Special mode for entropy generation.

adcRefVPNxAtt

Custom VFS: Scaled differential external Vref from pin 6 and 7: (VREFP - VREFN) * VREFATT.

adcRefPN

Custom VFS: Raw differential external Vref from pin 6 and 7: VREFP - VREFN.


Definition at line 185 of file platform/emlib/inc/em_adc.h

ADC_Res_TypeDef#

ADC_Res_TypeDef

Sample resolution.

Enumerator
adcRes12Bit

12 bit sampling.

adcRes8Bit

8 bit sampling.

adcRes6Bit

6 bit sampling.

adcResOVS

Oversampling.


Definition at line 261 of file platform/emlib/inc/em_adc.h

ADC_PosSel_TypeDef#

ADC_PosSel_TypeDef

Positive input selection for single and scan conversion.

Enumerator
adcPosSelAPORT0XCH0
adcPosSelAPORT0XCH1
adcPosSelAPORT0XCH2
adcPosSelAPORT0XCH3
adcPosSelAPORT0XCH4
adcPosSelAPORT0XCH5
adcPosSelAPORT0XCH6
adcPosSelAPORT0XCH7
adcPosSelAPORT0XCH8
adcPosSelAPORT0XCH9
adcPosSelAPORT0XCH10
adcPosSelAPORT0XCH11
adcPosSelAPORT0XCH12
adcPosSelAPORT0XCH13
adcPosSelAPORT0XCH14
adcPosSelAPORT0XCH15
adcPosSelAPORT0YCH0
adcPosSelAPORT0YCH1
adcPosSelAPORT0YCH2
adcPosSelAPORT0YCH3
adcPosSelAPORT0YCH4
adcPosSelAPORT0YCH5
adcPosSelAPORT0YCH6
adcPosSelAPORT0YCH7
adcPosSelAPORT0YCH8
adcPosSelAPORT0YCH9
adcPosSelAPORT0YCH10
adcPosSelAPORT0YCH11
adcPosSelAPORT0YCH12
adcPosSelAPORT0YCH13
adcPosSelAPORT0YCH14
adcPosSelAPORT0YCH15
adcPosSelAPORT1XCH0
adcPosSelAPORT1YCH1
adcPosSelAPORT1XCH2
adcPosSelAPORT1YCH3
adcPosSelAPORT1XCH4
adcPosSelAPORT1YCH5
adcPosSelAPORT1XCH6
adcPosSelAPORT1YCH7
adcPosSelAPORT1XCH8
adcPosSelAPORT1YCH9
adcPosSelAPORT1XCH10
adcPosSelAPORT1YCH11
adcPosSelAPORT1XCH12
adcPosSelAPORT1YCH13
adcPosSelAPORT1XCH14
adcPosSelAPORT1YCH15
adcPosSelAPORT1XCH16
adcPosSelAPORT1YCH17
adcPosSelAPORT1XCH18
adcPosSelAPORT1YCH19
adcPosSelAPORT1XCH20
adcPosSelAPORT1YCH21
adcPosSelAPORT1XCH22
adcPosSelAPORT1YCH23
adcPosSelAPORT1XCH24
adcPosSelAPORT1YCH25
adcPosSelAPORT1XCH26
adcPosSelAPORT1YCH27
adcPosSelAPORT1XCH28
adcPosSelAPORT1YCH29
adcPosSelAPORT1XCH30
adcPosSelAPORT1YCH31
adcPosSelAPORT2YCH0
adcPosSelAPORT2XCH1
adcPosSelAPORT2YCH2
adcPosSelAPORT2XCH3
adcPosSelAPORT2YCH4
adcPosSelAPORT2XCH5
adcPosSelAPORT2YCH6
adcPosSelAPORT2XCH7
adcPosSelAPORT2YCH8
adcPosSelAPORT2XCH9
adcPosSelAPORT2YCH10
adcPosSelAPORT2XCH11
adcPosSelAPORT2YCH12
adcPosSelAPORT2XCH13
adcPosSelAPORT2YCH14
adcPosSelAPORT2XCH15
adcPosSelAPORT2YCH16
adcPosSelAPORT2XCH17
adcPosSelAPORT2YCH18
adcPosSelAPORT2XCH19
adcPosSelAPORT2YCH20
adcPosSelAPORT2XCH21
adcPosSelAPORT2YCH22
adcPosSelAPORT2XCH23
adcPosSelAPORT2YCH24
adcPosSelAPORT2XCH25
adcPosSelAPORT2YCH26
adcPosSelAPORT2XCH27
adcPosSelAPORT2YCH28
adcPosSelAPORT2XCH29
adcPosSelAPORT2YCH30
adcPosSelAPORT2XCH31
adcPosSelAPORT3XCH0
adcPosSelAPORT3YCH1
adcPosSelAPORT3XCH2
adcPosSelAPORT3YCH3
adcPosSelAPORT3XCH4
adcPosSelAPORT3YCH5
adcPosSelAPORT3XCH6
adcPosSelAPORT3YCH7
adcPosSelAPORT3XCH8
adcPosSelAPORT3YCH9
adcPosSelAPORT3XCH10
adcPosSelAPORT3YCH11
adcPosSelAPORT3XCH12
adcPosSelAPORT3YCH13
adcPosSelAPORT3XCH14
adcPosSelAPORT3YCH15
adcPosSelAPORT3XCH16
adcPosSelAPORT3YCH17
adcPosSelAPORT3XCH18
adcPosSelAPORT3YCH19
adcPosSelAPORT3XCH20
adcPosSelAPORT3YCH21
adcPosSelAPORT3XCH22
adcPosSelAPORT3YCH23
adcPosSelAPORT3XCH24
adcPosSelAPORT3YCH25
adcPosSelAPORT3XCH26
adcPosSelAPORT3YCH27
adcPosSelAPORT3XCH28
adcPosSelAPORT3YCH29
adcPosSelAPORT3XCH30
adcPosSelAPORT3YCH31
adcPosSelAPORT4YCH0
adcPosSelAPORT4XCH1
adcPosSelAPORT4YCH2
adcPosSelAPORT4XCH3
adcPosSelAPORT4YCH4
adcPosSelAPORT4XCH5
adcPosSelAPORT4YCH6
adcPosSelAPORT4XCH7
adcPosSelAPORT4YCH8
adcPosSelAPORT4XCH9
adcPosSelAPORT4YCH10
adcPosSelAPORT4XCH11
adcPosSelAPORT4YCH12
adcPosSelAPORT4XCH13
adcPosSelAPORT4YCH14
adcPosSelAPORT4XCH15
adcPosSelAPORT4YCH16
adcPosSelAPORT4XCH17
adcPosSelAPORT4YCH18
adcPosSelAPORT4XCH19
adcPosSelAPORT4YCH20
adcPosSelAPORT4XCH21
adcPosSelAPORT4YCH22
adcPosSelAPORT4XCH23
adcPosSelAPORT4YCH24
adcPosSelAPORT4XCH25
adcPosSelAPORT4YCH26
adcPosSelAPORT4XCH27
adcPosSelAPORT4YCH28
adcPosSelAPORT4XCH29
adcPosSelAPORT4YCH30
adcPosSelAPORT4XCH31
adcPosSelAVDD
adcPosSelBUVDD
adcPosSelDVDD
adcPosSelPAVDD
adcPosSelDECOUPLE
adcPosSelIOVDD
adcPosSelIOVDD1
adcPosSelVSP
adcPosSelOPA2
adcPosSelTEMP
adcPosSelDAC0OUT0
adcPosSelR5VOUT
adcPosSelSP1
adcPosSelSP2
adcPosSelDAC0OUT1
adcPosSelSUBLSB
adcPosSelOPA3
adcPosSelDEFAULT
adcPosSelVSS

Definition at line 325 of file platform/emlib/inc/em_adc.h

ADC_NegSel_TypeDef#

ADC_NegSel_TypeDef

Negative input selection for single and scan conversion.

Enumerator
adcNegSelAPORT0XCH0
adcNegSelAPORT0XCH1
adcNegSelAPORT0XCH2
adcNegSelAPORT0XCH3
adcNegSelAPORT0XCH4
adcNegSelAPORT0XCH5
adcNegSelAPORT0XCH6
adcNegSelAPORT0XCH7
adcNegSelAPORT0XCH8
adcNegSelAPORT0XCH9
adcNegSelAPORT0XCH10
adcNegSelAPORT0XCH11
adcNegSelAPORT0XCH12
adcNegSelAPORT0XCH13
adcNegSelAPORT0XCH14
adcNegSelAPORT0XCH15
adcNegSelAPORT0YCH0
adcNegSelAPORT0YCH1
adcNegSelAPORT0YCH2
adcNegSelAPORT0YCH3
adcNegSelAPORT0YCH4
adcNegSelAPORT0YCH5
adcNegSelAPORT0YCH6
adcNegSelAPORT0YCH7
adcNegSelAPORT0YCH8
adcNegSelAPORT0YCH9
adcNegSelAPORT0YCH10
adcNegSelAPORT0YCH11
adcNegSelAPORT0YCH12
adcNegSelAPORT0YCH13
adcNegSelAPORT0YCH14
adcNegSelAPORT0YCH15
adcNegSelAPORT1XCH0
adcNegSelAPORT1YCH1
adcNegSelAPORT1XCH2
adcNegSelAPORT1YCH3
adcNegSelAPORT1XCH4
adcNegSelAPORT1YCH5
adcNegSelAPORT1XCH6
adcNegSelAPORT1YCH7
adcNegSelAPORT1XCH8
adcNegSelAPORT1YCH9
adcNegSelAPORT1XCH10
adcNegSelAPORT1YCH11
adcNegSelAPORT1XCH12
adcNegSelAPORT1YCH13
adcNegSelAPORT1XCH14
adcNegSelAPORT1YCH15
adcNegSelAPORT1XCH16
adcNegSelAPORT1YCH17
adcNegSelAPORT1XCH18
adcNegSelAPORT1YCH19
adcNegSelAPORT1XCH20
adcNegSelAPORT1YCH21
adcNegSelAPORT1XCH22
adcNegSelAPORT1YCH23
adcNegSelAPORT1XCH24
adcNegSelAPORT1YCH25
adcNegSelAPORT1XCH26
adcNegSelAPORT1YCH27
adcNegSelAPORT1XCH28
adcNegSelAPORT1YCH29
adcNegSelAPORT1XCH30
adcNegSelAPORT1YCH31
adcNegSelAPORT2YCH0
adcNegSelAPORT2XCH1
adcNegSelAPORT2YCH2
adcNegSelAPORT2XCH3
adcNegSelAPORT2YCH4
adcNegSelAPORT2XCH5
adcNegSelAPORT2YCH6
adcNegSelAPORT2XCH7
adcNegSelAPORT2YCH8
adcNegSelAPORT2XCH9
adcNegSelAPORT2YCH10
adcNegSelAPORT2XCH11
adcNegSelAPORT2YCH12
adcNegSelAPORT2XCH13
adcNegSelAPORT2YCH14
adcNegSelAPORT2XCH15
adcNegSelAPORT2YCH16
adcNegSelAPORT2XCH17
adcNegSelAPORT2YCH18
adcNegSelAPORT2XCH19
adcNegSelAPORT2YCH20
adcNegSelAPORT2XCH21
adcNegSelAPORT2YCH22
adcNegSelAPORT2XCH23
adcNegSelAPORT2YCH24
adcNegSelAPORT2XCH25
adcNegSelAPORT2YCH26
adcNegSelAPORT2XCH27
adcNegSelAPORT2YCH28
adcNegSelAPORT2XCH29
adcNegSelAPORT2YCH30
adcNegSelAPORT2XCH31
adcNegSelAPORT3XCH0
adcNegSelAPORT3YCH1
adcNegSelAPORT3XCH2
adcNegSelAPORT3YCH3
adcNegSelAPORT3XCH4
adcNegSelAPORT3YCH5
adcNegSelAPORT3XCH6
adcNegSelAPORT3YCH7
adcNegSelAPORT3XCH8
adcNegSelAPORT3YCH9
adcNegSelAPORT3XCH10
adcNegSelAPORT3YCH11
adcNegSelAPORT3XCH12
adcNegSelAPORT3YCH13
adcNegSelAPORT3XCH14
adcNegSelAPORT3YCH15
adcNegSelAPORT3XCH16
adcNegSelAPORT3YCH17
adcNegSelAPORT3XCH18
adcNegSelAPORT3YCH19
adcNegSelAPORT3XCH20
adcNegSelAPORT3YCH21
adcNegSelAPORT3XCH22
adcNegSelAPORT3YCH23
adcNegSelAPORT3XCH24
adcNegSelAPORT3YCH25
adcNegSelAPORT3XCH26
adcNegSelAPORT3YCH27
adcNegSelAPORT3XCH28
adcNegSelAPORT3YCH29
adcNegSelAPORT3XCH30
adcNegSelAPORT3YCH31
adcNegSelAPORT4YCH0
adcNegSelAPORT4XCH1
adcNegSelAPORT4YCH2
adcNegSelAPORT4XCH3
adcNegSelAPORT4YCH4
adcNegSelAPORT4XCH5
adcNegSelAPORT4YCH6
adcNegSelAPORT4XCH7
adcNegSelAPORT4YCH8
adcNegSelAPORT4XCH9
adcNegSelAPORT4YCH10
adcNegSelAPORT4XCH11
adcNegSelAPORT4YCH12
adcNegSelAPORT4XCH13
adcNegSelAPORT4YCH14
adcNegSelAPORT4XCH15
adcNegSelAPORT4YCH16
adcNegSelAPORT4XCH17
adcNegSelAPORT4YCH18
adcNegSelAPORT4XCH19
adcNegSelAPORT4YCH20
adcNegSelAPORT4XCH21
adcNegSelAPORT4YCH22
adcNegSelAPORT4XCH23
adcNegSelAPORT4YCH24
adcNegSelAPORT4XCH25
adcNegSelAPORT4YCH26
adcNegSelAPORT4XCH27
adcNegSelAPORT4YCH28
adcNegSelAPORT4XCH29
adcNegSelAPORT4YCH30
adcNegSelAPORT4XCH31
adcNegSelTESTN
adcNegSelDEFAULT
adcNegSelVSS

Definition at line 518 of file platform/emlib/inc/em_adc.h

ADC_ScanInputGroup_TypeDef#

ADC_ScanInputGroup_TypeDef

ADC scan input groups.

Enumerator
adcScanInputGroup0
adcScanInputGroup1
adcScanInputGroup2
adcScanInputGroup3

Definition at line 687 of file platform/emlib/inc/em_adc.h

ADC_ScanNegInput_TypeDef#

ADC_ScanNegInput_TypeDef

ADC scan alternative negative inputs.

Enumerator
adcScanNegInput1
adcScanNegInput3
adcScanNegInput5
adcScanNegInput7
adcScanNegInput8
adcScanNegInput10
adcScanNegInput12
adcScanNegInput14
adcScanNegInputDefault

Definition at line 707 of file platform/emlib/inc/em_adc.h

ADC_Start_TypeDef#

ADC_Start_TypeDef

ADC start command.

Enumerator
adcStartSingle

Start a single conversion.

adcStartScan

Start a scan sequence.

adcStartScanAndSingle

Start a scan sequence and single conversion, typically used when tailgating a single conversion after a scan sequence.


Definition at line 721 of file platform/emlib/inc/em_adc.h

ADC_Warmup_TypeDef#

ADC_Warmup_TypeDef

Warm-up mode.

Enumerator
adcWarmupNormal

ADC shutdown after each conversion.

adcWarmupKeepInStandby

ADC is kept in standby mode between conversions.

adcWarmupKeepInSlowAcq

ADC is kept in slow acquisition mode between conversions.

adcWarmupKeepADCWarm

ADC and reference selected for scan mode kept at warmup allowing continuous conversion.


Definition at line 736 of file platform/emlib/inc/em_adc.h

ADC_EM2ClockConfig_TypeDef#

ADC_EM2ClockConfig_TypeDef

ADC EM2 clock configuration.

Enumerator
adcEm2Disabled
adcEm2ClockOnDemand
adcEm2ClockAlwaysOn

Definition at line 769 of file platform/emlib/inc/em_adc.h

Function Documentation#

ADC_Init#

void ADC_Init (ADC_TypeDef * adc, const ADC_Init_TypeDef * init)

Initialize ADC.

Parameters
[in]adc

A pointer to the ADC peripheral register block.

[in]init

A pointer to the ADC initialization structure.

Initializes common parts for both single conversion and scan sequence. In addition, single and/or scan control configuration must be done. See ADC_InitSingle() and ADC_InitScan() respectively. For ADC architectures with the ADCn->SCANINPUTSEL register, use ADC_ScanSingleEndedInputAdd() to configure single-ended scan inputs or ADC_ScanDifferentialInputAdd() to configure differential scan inputs. ADC_ScanInputClear() is also provided for applications that need to update the input configuration.

Note

  • This function will stop any ongoing conversion.


Definition at line 373 of file platform/emlib/src/em_adc.c

ADC_ScanInputClear#

void ADC_ScanInputClear (ADC_InitScan_TypeDef * scanInit)

Clear ADC scan input configuration.

Parameters
[in]scanInit

Structure to hold the scan configuration and input configuration.


Definition at line 471 of file platform/emlib/src/em_adc.c

ADC_ScanSingleEndedInputAdd#

uint32_t ADC_ScanSingleEndedInputAdd (ADC_InitScan_TypeDef * scanInit, ADC_ScanInputGroup_TypeDef inputGroup, ADC_PosSel_TypeDef singleEndedSel)

Initialize ADC scan single-ended input configuration.

Parameters
[in]scanInit

ADC scan initialization structure

[in]inputGroup

ADC scan input group. See section 25.3.4 in the reference manual for more information.

[in]singleEndedSel

APORT select.

Set a configuration for ADC scan conversion with single-ended inputs. The ADC_InitScan_TypeDef structure updated from this function will be passed to ADC_InitScan().

Returns

  • Scan ID of selected ADC input. See section 25.3.4 in the reference manual for more information. Note that the returned integer represents the bit position in ADCn_SCANMASK set by this function. The accumulated mask is stored in scanInit->scanInputConfig->scanInputEn.


Definition at line 508 of file platform/emlib/src/em_adc.c

ADC_ScanDifferentialInputAdd#

uint32_t ADC_ScanDifferentialInputAdd (ADC_InitScan_TypeDef * scanInit, ADC_ScanInputGroup_TypeDef inputGroup, ADC_PosSel_TypeDef posSel, ADC_ScanNegInput_TypeDef negInput)

Initialize the ADC scan differential input configuration.

Parameters
[in]scanInit

Structure to hold the scan and input configuration.

[in]inputGroup

ADC scan input group. See section 25.3.4 in the reference manual for more information.

[in]posSel

APORT bus pair select. The negative terminal is implicitly selected by the positive terminal.

[in]negInput

ADC scan alternative negative input. Set to adcScanNegInputDefault to select a default negative input (implicit from posSel).

Set a configuration for the ADC scan conversion with differential inputs. The ADC_InitScan_TypeDef structure updated by this function should be passed to ADC_InitScan().

Returns

  • Scan ID of the selected ADC input. See section 25.3.4 in the reference manual for more information. Note that the returned integer represents the bit position in ADCn_SCANMASK set by this function. The accumulated mask is stored in the scanInit->scanInputConfig->scanInputEn.


Definition at line 581 of file platform/emlib/src/em_adc.c

ADC_InitScan#

void ADC_InitScan (ADC_TypeDef * adc, const ADC_InitScan_TypeDef * init)

Initialize the ADC scan sequence.

Parameters
[in]adc

A pointer to the ADC peripheral register block.

[in]init

A pointer to the ADC initialization structure.

See ADC_Start() for starting a scan sequence.

When selecting an external reference, the gain and offset calibration must be set explicitly (CAL register). For other references, the calibration is updated with values defined during manufacturing. For ADC architectures with the ADCn->SCANINPUTSEL register, use ADC_ScanSingleEndedInputAdd() to configure single-ended scan inputs or ADC_ScanDifferentialInputAdd() to configure differential scan inputs. ADC_ScanInputClear() is also provided for applications that need to update the input configuration.

Note

  • This function will stop any ongoing scan sequence.


Definition at line 719 of file platform/emlib/src/em_adc.c

ADC_InitSingle#

void ADC_InitSingle (ADC_TypeDef * adc, const ADC_InitSingle_TypeDef * init)

Initialize the single ADC sample conversion.

Parameters
[in]adc

A pointer to the ADC peripheral register block.

[in]init

A pointer to the ADC initialization structure.

See ADC_Start() for starting a single conversion.

When selecting an external reference, the gain and offset calibration must be set explicitly (CAL register). For other references, the calibration is updated with values defined during manufacturing.

Note

  • This function will stop any ongoing single conversion.

  • This function will set the BIASPROG_GPBIASACC bit when selecting the internal temperature sensor and clear the bit otherwise. Any application that depends on the state of the BIASPROG_GPBIASACC bit should modify it after a call to this function.


Definition at line 856 of file platform/emlib/src/em_adc.c

ADC_DataIdScanGet#

uint32_t ADC_DataIdScanGet (ADC_TypeDef * adc, uint32_t * scanId)

Get a scan result and scan select ID.

Parameters
[in]adc

A pointer to the ADC peripheral register block.

[out]scanId

A scan select ID of the first data in the scan FIFO.

Note

  • Only use if scan data valid. This function does not check the DV flag. The return value is meant to be used as an index for the scan select ID.

Returns

  • The first scan data in the scan FIFO.


Definition at line 987 of file platform/emlib/src/em_adc.c

ADC_PrescaleCalc#

uint8_t ADC_PrescaleCalc (uint32_t adcFreq, uint32_t hfperFreq)

Calculate the prescaler value used to determine the ADC clock.

Parameters
[in]adcFreq

ADC frequency wanted. The frequency will automatically be adjusted to a valid range according to the reference manual.

[in]hfperFreq

Frequency in Hz of reference HFPER/HFPERC clock. Set to 0 to use currently defined HFPER/HFPERC clock setting.

The ADC clock is given by: (HFPERCLK or HFPERCCLK) / (prescale + 1).

Note

  • The return value is clamped to the maximum prescaler value that the hardware supports.

Returns

  • A prescaler value to use for ADC in order to achieve a clock value <= adcFreq.


Definition at line 1018 of file platform/emlib/src/em_adc.c

ADC_Reset#

void ADC_Reset (ADC_TypeDef * adc)

Reset ADC to a state that it was in after a hardware reset.

Parameters
[in]adc

A pointer to ADC peripheral register block.

Note

  • The ROUTE register is NOT reset by this function to allow a centralized setup of this feature.


Definition at line 1063 of file platform/emlib/src/em_adc.c

ADC_TimebaseCalc#

uint8_t ADC_TimebaseCalc (uint32_t hfperFreq)

Calculate a timebase value to get a timebase providing at least 1 us.

Parameters
[in]hfperFreq

Frequency in Hz of the reference HFPER/HFPERC clock. Set to 0 to use currently defined HFPER/HFPERC clock setting.

Returns

  • A timebase value to use for ADC to achieve at least 1 us.


Definition at line 1114 of file platform/emlib/src/em_adc.c

ADC_DataSingleGet#

uint32_t ADC_DataSingleGet (ADC_TypeDef * adc)

Get a single conversion result.

Parameters
[in]adc

A pointer to the ADC peripheral register block.

Note

  • Check data valid flag before calling this function.

Returns

  • Single conversion data.


Definition at line 1073 of file platform/emlib/inc/em_adc.h

ADC_DataSinglePeek#

uint32_t ADC_DataSinglePeek (ADC_TypeDef * adc)

Peek single conversion result.

Parameters
[in]adc

A pointer to the ADC peripheral register block.

Note

  • Check data valid flag before calling this function.

Returns

  • Single conversion data.


Definition at line 1091 of file platform/emlib/inc/em_adc.h

ADC_DataScanGet#

uint32_t ADC_DataScanGet (ADC_TypeDef * adc)

Get a scan result.

Parameters
[in]adc

A pointer to the ADC peripheral register block.

Note

  • Check data valid flag before calling this function.

Returns

  • Scan conversion data.


Definition at line 1109 of file platform/emlib/inc/em_adc.h

ADC_DataScanPeek#

uint32_t ADC_DataScanPeek (ADC_TypeDef * adc)

Peek scan result.

Parameters
[in]adc

A pointer to the ADC peripheral register block.

Note

  • Check data valid flag before calling this function.

Returns

  • Scan conversion data.


Definition at line 1127 of file platform/emlib/inc/em_adc.h

ADC_IntClear#

void ADC_IntClear (ADC_TypeDef * adc, uint32_t flags)

Clear one or more pending ADC interrupts.

Parameters
[in]adc

A pointer to the ADC peripheral register block.

[in]flags

Pending ADC interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the ADC module (ADC_IF_nnn).


Definition at line 1166 of file platform/emlib/inc/em_adc.h

ADC_IntDisable#

void ADC_IntDisable (ADC_TypeDef * adc, uint32_t flags)

Disable one or more ADC interrupts.

Parameters
[in]adc

A pointer to the ADC peripheral register block.

[in]flags

ADC interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the ADC module (ADC_IF_nnn).


Definition at line 1182 of file platform/emlib/inc/em_adc.h

ADC_IntEnable#

void ADC_IntEnable (ADC_TypeDef * adc, uint32_t flags)

Enable one or more ADC interrupts.

Parameters
[in]adc

A pointer to the ADC peripheral register block.

[in]flags

ADC interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the ADC module (ADC_IF_nnn).

Note

  • Depending on use, a pending interrupt may already be set prior to enabling the interrupt. Consider using ADC_IntClear() prior to enabling if the pending interrupt should be ignored.


Definition at line 1203 of file platform/emlib/inc/em_adc.h

ADC_IntGet#

uint32_t ADC_IntGet (ADC_TypeDef * adc)

Get pending ADC interrupt flags.

Parameters
[in]adc

A pointer to the ADC peripheral register block.

Note

  • This function does not clear event bits.

Returns

  • ADC interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for the ADC module (ADC_IF_nnn).


Definition at line 1222 of file platform/emlib/inc/em_adc.h

ADC_IntGetEnabled#

uint32_t ADC_IntGetEnabled (ADC_TypeDef * adc)

Get enabled and pending ADC interrupt flags.

Parameters
[in]adc

A pointer to the ADC peripheral register block.

Useful for handling more interrupt sources in the same interrupt handler.

Note

  • This function does not clear interrupt flags.

Returns

  • Pending and enabled ADC interrupt sources. The return value is the bitwise AND combination of

    • the OR combination of enabled interrupt sources in ADCx_IEN_nnn register (ADCx_IEN_nnn) and

    • the OR combination of valid interrupt flags of the ADC module (ADCx_IF_nnn).


Definition at line 1246 of file platform/emlib/inc/em_adc.h

ADC_IntSet#

void ADC_IntSet (ADC_TypeDef * adc, uint32_t flags)

Set one or more pending ADC interrupts from software.

Parameters
[in]adc

A pointer to the ADC peripheral register block.

[in]flags

ADC interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the ADC module (ADC_IF_nnn).


Definition at line 1269 of file platform/emlib/inc/em_adc.h

ADC_Start#

void ADC_Start (ADC_TypeDef * adc, ADC_Start_TypeDef cmd)

Start scan sequence and/or single conversion.

Parameters
[in]adc

A pointer to the ADC peripheral register block.

[in]cmd

A command indicating which type of sampling to start.


Definition at line 1284 of file platform/emlib/inc/em_adc.h