ACMP initialization structure.

Public Attributes#

bool

Full-bias current.

bool

Half-bias current.

uint32_t

Bias current.

bool

Enable setting the interrupt flag on the falling edge.

bool

Enable setting the interrupt flag on the rising edge.

Warmup time, which is measured in HFPERCLK / HFPERCCLK cycles and should be about 10 us in wall clock time.

bool

Inactive value emitted by ACMP during warmup.

bool

Low power reference enabled.

uint32_t

VDD reference value.

bool

If true, ACMP is enabled after configuration.

Public Attribute Documentation#

fullBias#

bool ACMP_Init_TypeDef::fullBias

Full-bias current.

See the ACMP chapter about bias and response time in the reference manual for details.


Definition at line 753 of file platform/emlib/inc/em_acmp.h

halfBias#

bool ACMP_Init_TypeDef::halfBias

Half-bias current.

See the ACMP chapter about bias and response time in the reference manual for details.


Definition at line 759 of file platform/emlib/inc/em_acmp.h

biasProg#

uint32_t ACMP_Init_TypeDef::biasProg

Bias current.

See the ACMP chapter about bias and response time in the reference manual for details. Valid values are in the range 0-7.


Definition at line 764 of file platform/emlib/inc/em_acmp.h

interruptOnFallingEdge#

bool ACMP_Init_TypeDef::interruptOnFallingEdge

Enable setting the interrupt flag on the falling edge.


Definition at line 768 of file platform/emlib/inc/em_acmp.h

interruptOnRisingEdge#

bool ACMP_Init_TypeDef::interruptOnRisingEdge

Enable setting the interrupt flag on the rising edge.


Definition at line 772 of file platform/emlib/inc/em_acmp.h

warmTime#

ACMP_WarmTime_TypeDef ACMP_Init_TypeDef::warmTime

Warmup time, which is measured in HFPERCLK / HFPERCCLK cycles and should be about 10 us in wall clock time.


Definition at line 798 of file platform/emlib/inc/em_acmp.h

hysteresisLevel#

ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel

Hysteresis level.


Definition at line 804 of file platform/emlib/inc/em_acmp.h

inactiveValue#

bool ACMP_Init_TypeDef::inactiveValue

Inactive value emitted by ACMP during warmup.


Definition at line 820 of file platform/emlib/inc/em_acmp.h

lowPowerReferenceEnabled#

bool ACMP_Init_TypeDef::lowPowerReferenceEnabled

Low power reference enabled.

This setting, if enabled, reduces the power used by the VDD and bandgap references.


Definition at line 825 of file platform/emlib/inc/em_acmp.h

vddLevel#

uint32_t ACMP_Init_TypeDef::vddLevel

VDD reference value.

VDD_SCALED = VDD * VDDLEVEL * 50 mV/3.8 V. Valid values are in the 0-63 range.


Definition at line 835 of file platform/emlib/inc/em_acmp.h

enable#

bool ACMP_Init_TypeDef::enable

If true, ACMP is enabled after configuration.


Definition at line 839 of file platform/emlib/inc/em_acmp.h