A struct containing all of the function pointers needed to implement cipher operations using secure elements.

PSA Crypto API implementations should populate instances of the table as appropriate upon startup or at build time.

If one of the functions is not implemented (such as psa_drv_se_cipher_ecb_t), it should be set to NULL.

Public Functions#

size_t
MBEDTLS_PRIVATE(context_size)

The size in bytes of the hardware-specific secure element cipher context structure.

Function that performs a cipher setup operation.

MBEDTLS_PRIVATE(p_set_iv)

Function that sets a cipher IV (if necessary)

MBEDTLS_PRIVATE(p_update)

Function that performs a cipher update operation.

MBEDTLS_PRIVATE(p_finish)

Function that completes a cipher operation.

Function that aborts a cipher operation.

Function that performs ECB mode for a cipher operation (Danger: ECB mode should not be used directly by clients of the PSA Crypto Client API)

Public Function Documentation#

MBEDTLS_PRIVATE#

size_t psa_drv_se_cipher_t::MBEDTLS_PRIVATE (context_size )

The size in bytes of the hardware-specific secure element cipher context structure.

Parameters
N/A

Definition at line 514 of file util/third_party/mbedtls/include/psa/crypto_se_driver.h

MBEDTLS_PRIVATE#

psa_drv_se_cipher_setup_t psa_drv_se_cipher_t::MBEDTLS_PRIVATE (p_setup )

Function that performs a cipher setup operation.

Parameters
N/A

Definition at line 516 of file util/third_party/mbedtls/include/psa/crypto_se_driver.h

MBEDTLS_PRIVATE#

psa_drv_se_cipher_set_iv_t psa_drv_se_cipher_t::MBEDTLS_PRIVATE (p_set_iv )

Function that sets a cipher IV (if necessary)

Parameters
N/A

Definition at line 518 of file util/third_party/mbedtls/include/psa/crypto_se_driver.h

MBEDTLS_PRIVATE#

psa_drv_se_cipher_update_t psa_drv_se_cipher_t::MBEDTLS_PRIVATE (p_update )

Function that performs a cipher update operation.

Parameters
N/A

Definition at line 520 of file util/third_party/mbedtls/include/psa/crypto_se_driver.h

MBEDTLS_PRIVATE#

psa_drv_se_cipher_finish_t psa_drv_se_cipher_t::MBEDTLS_PRIVATE (p_finish )

Function that completes a cipher operation.

Parameters
N/A

Definition at line 522 of file util/third_party/mbedtls/include/psa/crypto_se_driver.h

MBEDTLS_PRIVATE#

psa_drv_se_cipher_abort_t psa_drv_se_cipher_t::MBEDTLS_PRIVATE (p_abort )

Function that aborts a cipher operation.

Parameters
N/A

Definition at line 524 of file util/third_party/mbedtls/include/psa/crypto_se_driver.h

MBEDTLS_PRIVATE#

psa_drv_se_cipher_ecb_t psa_drv_se_cipher_t::MBEDTLS_PRIVATE (p_ecb )

Function that performs ECB mode for a cipher operation (Danger: ECB mode should not be used directly by clients of the PSA Crypto Client API)

Parameters
N/A

Definition at line 529 of file util/third_party/mbedtls/include/psa/crypto_se_driver.h