CPC#
Modules#
sl_cpc_endpoint_debug_counters_t
Enumerations#
Enumeration representing user endpoint.
Enumeration representing the possible endpoint state.
Enumeration representing the possible configurable options for an endpoint.
Typedefs#
Typedef for the user - supplied callback function which is called when CPC is done with the provided buffer.
Typedef for the user - supplied callback function which is called when CPC receive data on an endpoint.
Typedef for the user-supplied callback function which is called when CPC detects a fatal error on an endpoint.
Typedef for the user-supplied callback function which is called when CPC connection to a secondary completes, successfully or not.
Functions#
Global variable that contains the core debug information.
The bare metal process action function.
Set endpoint option.
Shutdown endpoint connection.
Terminate an endpoint, effectively dropping any pending TX and RX frame.
Free the memory associated to an endpoint so it can be reused.
Abort read; Allow unblocking task in blocked by a read.
Read data.
Write data.
Get endpoint state.
Get endpoint encryption state.
Free buffer returned by sl_cpc_read().
Get the maximum payload length that the remote can receive.
Macros#
sl cpc open endpoint flag none
sl cpc open endpoint flag disable encryption
Struct representing a core debug.
sl cpc user endpoint id end.
sl cpc flag no block.
sli cpc security tag length.
sli cpc ldma desciptor max size.
sli cpc header size.
sli cpc payload crc size.
sl cpc tx payload max length.
sl cpc tx payload max lenght with security.
sl cpc transmit window min size.
sl cpc transmit window max size.
Enumeration Documentation#
sl_cpc_user_endpoint_id_t#
sl_cpc_user_endpoint_id_t
Enumeration representing user endpoint.
| Enumerator | |
|---|---|
| SL_CPC_ENDPOINT_USER_ID_0 | User endpoint ID 0. |
| SL_CPC_ENDPOINT_USER_ID_1 | User endpoint ID 1. |
| SL_CPC_ENDPOINT_USER_ID_2 | User endpoint ID 2. |
| SL_CPC_ENDPOINT_USER_ID_3 | User endpoint ID 3. |
| SL_CPC_ENDPOINT_USER_ID_4 | User endpoint ID 4. |
| SL_CPC_ENDPOINT_USER_ID_5 | User endpoint ID 5. |
| SL_CPC_ENDPOINT_USER_ID_6 | User endpoint ID 6. |
| SL_CPC_ENDPOINT_USER_ID_7 | User endpoint ID 7. |
| SL_CPC_ENDPOINT_USER_ID_8 | User endpoint ID 8. |
| SL_CPC_ENDPOINT_USER_ID_9 | User endpoint ID 9. |
sl_cpc_endpoint_state_t#
sl_cpc_endpoint_state_t
Enumeration representing the possible endpoint state.
| Enumerator | |
|---|---|
| SL_CPC_STATE_FREED | State freed. |
| SL_CPC_STATE_OPEN | State open. |
| SL_CPC_STATE_CLOSED | State close. |
| SL_CPC_STATE_CLOSING | State closing. |
| SL_CPC_STATE_CONNECTING | Connecting to remote's endpoint. |
| SL_CPC_STATE_CONNECTED | Connected to remote's endpoint. |
| SL_CPC_STATE_SHUTTING_DOWN | Transmissions shutting down. |
| SL_CPC_STATE_SHUTDOWN | Transmissions shutdown. |
| SL_CPC_STATE_REMOTE_SHUTDOWN | Remote transmissions shutdown. |
| SL_CPC_STATE_DISCONNECTED | Connection terminated. |
| SL_CPC_STATE_ERROR_DESTINATION_UNREACHABLE | Error state, destination unreachable. |
| SL_CPC_STATE_ERROR_SECURITY_INCIDENT | Error state, security incident. |
| SL_CPC_STATE_ERROR_FAULT | Error state, fault. |
sl_cpc_endpoint_option_t#
sl_cpc_endpoint_option_t
Enumeration representing the possible configurable options for an endpoint.
| Enumerator | |
|---|---|
| SL_CPC_ENDPOINT_ON_IFRAME_RECEIVE | Set callback for iframe received notification. |
| SL_CPC_ENDPOINT_ON_IFRAME_RECEIVE_ARG | Set callback argument for iframe received notification. |
| SL_CPC_ENDPOINT_ON_IFRAME_WRITE_COMPLETED | Set callback for write complete notification. |
| SL_CPC_ENDPOINT_ON_ERROR | Set callback for error notification. |
| SL_CPC_ENDPOINT_ON_ERROR_ARG | Set callback argument for error notification. |
| SL_CPC_ENDPOINT_ON_CONNECT | Set callback when host/primary connects to endpoint. |
| SL_CPC_ENDPOINT_ON_CONNECT_ARG | Set callback argument for connect notification. |
| SL_CPC_ENDPOINT_SHUTDOWN_TIMEOUT | Set shutdown timeout, in ticks. |
| SL_CPC_ENDPOINT_WRITE_TIMEOUT | Set the timeout time for blocking write in ticks. |
| SL_CPC_ENDPOINT_ON_UFRAME_RECEIVE | Set callback for uframe received notification. |
| SL_CPC_ENDPOINT_ON_UFRAME_RECEIVE_ARG | Set callback argument for uframe received notification. |
| SL_CPC_ENDPOINT_ON_UFRAME_WRITE_COMPLETED | Set callback for write complete notification. |
| SL_CPC_ENDPOINT_ON_POLL | Set callback for on poll notification. |
| SL_CPC_ENDPOINT_ON_POLL_ARG | Set callback argument for on poll notification. |
| SL_CPC_ENDPOINT_ON_FINAL | Set callback for on final notification. |
| SL_CPC_ENDPOINT_ON_FINAL_ARG | Set callback argument for on final notification. |
Typedef Documentation#
sl_cpc_on_write_completed_t#
typedef void(* sl_cpc_on_write_completed_t) (sl_cpc_user_endpoint_id_t endpoint_id, void *buffer, void *arg, sl_status_t status) )(sl_cpc_user_endpoint_id_t endpoint_id, void *buffer, void *arg, sl_status_t status)
Typedef for the user - supplied callback function which is called when CPC is done with the provided buffer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| N/A | endpoint_id | Endpoint ID | |
| N/A | buffer | Pointer to data buffer. | |
| N/A | arg | Transaction user's argument. | |
| N/A | status | Status indicating the transaction result: SL_STATUS_OK Remote should have receive the frame SL_STATUS_TRANSMIT_INCOMPLETE Remote has not received the frame. |
sl_cpc_on_data_reception_t#
typedef void(* sl_cpc_on_data_reception_t) (uint8_t endpoint_id, void *arg) )(uint8_t endpoint_id, void *arg)
Typedef for the user - supplied callback function which is called when CPC receive data on an endpoint.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| N/A | endpoint_id | Endpoint ID | |
| N/A | arg | User-specific argument . |
sl_cpc_on_error_callback_t#
typedef void(* sl_cpc_on_error_callback_t) (uint8_t endpoint_id, void *arg) )(uint8_t endpoint_id, void *arg)
Typedef for the user-supplied callback function which is called when CPC detects a fatal error on an endpoint.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| N/A | endpoint_id | Endpoint ID | |
| N/A | arg | User-specific argument . |
sl_cpc_on_connect_callback_t#
typedef void(* sl_cpc_on_connect_callback_t) (uint8_t endpoint_id, void *arg, sl_status_t status) )(uint8_t endpoint_id, void *arg, sl_status_t status)
Typedef for the user-supplied callback function which is called when CPC connection to a secondary completes, successfully or not.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| N/A | endpoint_id | Endpoint ID | |
| N/A | arg | User-specific argument. | |
| N/A | status | Indicate if the connection was successful or not: SL_STATUS_OK successfully connected SL_STATUS_TIMEOUT operation timed out SL_STATUS_NOT_READY secondary's endpoint is not ready |
Note
If several users connect to the same endpoint on the host side, this callback will only be called only when the first connection occurs.
Function Documentation#
sl_cpc_init#
sl_status_t sl_cpc_init (void )
Global variable that contains the core debug information.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Initialize CPC module.
sl_cpc_init_user_endpoint#
sl_status_t sl_cpc_init_user_endpoint (sl_cpc_endpoint_handle_t * endpoint_handle, sl_cpc_user_endpoint_id_t id, uint8_t flags)
The bare metal process action function.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [inout] | endpoint_handle | Endpoint handle. |
| sl_cpc_user_endpoint_id_t | [in] | id | Endpoint ID [90 to 99]. |
| uint8_t | [in] | flags | Initialization flags. Reserved for future used |
Initalize a user endpoint. Following the successful initialization of an endpoint, successive attempts to initialize an endpoint of the same ID will fail until the endpoint is freed.
sl_cpc_set_endpoint_option#
sl_status_t sl_cpc_set_endpoint_option (sl_cpc_endpoint_handle_t * endpoint_handle, sl_cpc_endpoint_option_t option, void * value)
Set endpoint option.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
| sl_cpc_endpoint_option_t | [in] | option | Endpoint Option. |
| void * | [in] | value | Pointer to the option value. |
Returns
Status code.
Return values
SL_STATUS_OK: Set endpoint option successfully.
Other: sl_status_t if error occurred.
Note
Public options are: SL_CPC_ENDPOINT_ON_CONNECT: Set a callback that will be called when connection is established with the remote.
SL_CPC_ENDPOINT_ON_CONNECT_ARG: Set an on connect argument.
SL_CPC_ENDPOINT_ON_IFRAME_RECEIVE: Set an on iframe receive callback. value is a sl_cpc_on_data_reception_t type.
SL_CPC_ENDPOINT_ON_IFRAME_RECEIVE_ARG: Set an on iframe receive argument.
SL_CPC_ENDPOINT_ON_IFRAME_WRITE_COMPLETED: Set an on iframe write completed callback. value is a sl_cpc_on_write_completed_t type.
SL_CPC_ENDPOINT_ON_ERROR: Set an on error callback. value is a sl_cpc_on_error_callback_t type.
SL_CPC_ENDPOINT_ON_ERROR_ARG: Set an on error callback argument.
SL_CPC_ENDPOINT_SHUTDOWN_TIMEOUT: (RTOS Only) Set shutdown handshake timeout, in ticks.
SL_CPC_ENDPOINT_WRITE_TIMEOUT: (RTOS Only) Set the timeout time for blocking write in ticks.
sl_cpc_shutdown_endpoint#
sl_status_t sl_cpc_shutdown_endpoint (sl_cpc_endpoint_handle_t * endpoint_handle, uint8_t flags)
Shutdown endpoint connection.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
| uint8_t | [in] | flags | Optional flags: SL_CPC_FLAG_NO_BLOCK Cause the function to return SL_STATUS_IN_PROGRESS immediately in RTOS data still pending TX. |
Any pending TX frame will attempt to be transmitted.
Note
In RTOS, this function is blocking by default. Use the SL_CPC_FLAG_NO_BLOCK flag to execute without blocking.
sl_cpc_terminate_endpoint#
sl_status_t sl_cpc_terminate_endpoint (sl_cpc_endpoint_handle_t * endpoint_handle, uint8_t flags)
Terminate an endpoint, effectively dropping any pending TX and RX frame.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
| uint8_t | [in] | flags | Termination flags. Reserved for future use |
In RTOS, this function will always block until all frames have been dropped.
Note
This function must be called before attempting to reconnect an endpoint to the remote.
sl_cpc_free_endpoint#
sl_status_t sl_cpc_free_endpoint (sl_cpc_endpoint_handle_t * endpoint_handle)
Free the memory associated to an endpoint so it can be reused.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
sl_cpc_abort_read#
sl_status_t sl_cpc_abort_read (sl_cpc_endpoint_handle_t * endpoint_handle)
Abort read; Allow unblocking task in blocked by a read.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
Note
This function can be called from an ISR.
sl_cpc_read#
sl_status_t sl_cpc_read (sl_cpc_endpoint_handle_t * endpoint_handle, void ** data, uint16_t * data_length, uint32_t timeout, uint8_t flags)
Read data.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
| void ** | [out] | data | Address of the variable that will receive the data pointer. |
| uint16_t * | [out] | data_length | Length of the data contained in the buffer. |
| uint32_t | [in] | timeout | Timeout in ticks for the read operation. (Requires RTOS). Note: No effect if SL_CPC_FLAG_NO_BLOCK is provided as a flag |
| uint8_t | [in] | flags | Optional flags: SL_CPC_FLAG_NO_BLOCK Cause the function to return SL_STATUS_EMPTY immediately in RTOS if no data available. |
sl_cpc_write#
sl_status_t sl_cpc_write (sl_cpc_endpoint_handle_t * endpoint_handle, void * data, uint16_t data_length, uint8_t flag, void * on_write_completed_arg)
Write data.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
| void * | [in] | data | Pointer to data buffer. |
| uint16_t | [in] | data_length | Length of the data contained in the buffer. |
| uint8_t | [in] | flag | Internal flag, do not use. |
| void * | [in] | on_write_completed_arg | Argument that will be passed to on_write_completed(). |
Note
This function cannot be called from an ISR.
When the write buffer is encrypted, the original content is lost and replaced by its encrypted counterpart.
sl_cpc_get_endpoint_state#
sl_cpc_endpoint_state_t sl_cpc_get_endpoint_state (sl_cpc_endpoint_handle_t * endpoint_handle)
Get endpoint state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
Returns
Endpoint state.
sl_cpc_get_endpoint_encryption#
bool sl_cpc_get_endpoint_encryption (sl_cpc_endpoint_handle_t * endpoint_handle)
Get endpoint encryption state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
Returns
Endpoint encryption state.
sl_cpc_free_rx_buffer#
sl_status_t sl_cpc_free_rx_buffer (void * data)
Free buffer returned by sl_cpc_read().
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void * | [in] | data | Pointer to data buffer to free. |
sl_cpc_get_tx_max_payload_length#
uint16_t sl_cpc_get_tx_max_payload_length (sl_cpc_endpoint_handle_t * endpoint_handle)
Get the maximum payload length that the remote can receive.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
Returns
the maximum tx payload length in function of whether the encryption is enabled on the endpoint or not