Configuration structure for alternate scatter-gather descriptor.
Public Attributes#
Pointer to location to transfer data from.
Pointer to location to transfer data to.
Destination increment size for each DMA transfer.
Source increment size for each DMA transfer.
DMA transfer unit size.
Arbitration rate, i.e., number of DMA transfers done before re-arbitration takes place.
Number of DMA transfers minus 1 to do.
HPROT signal state, refer to reference manual, DMA chapter for further details.
Specify if a memory or peripheral scatter-gather DMA cycle.
Public Attribute Documentation#
dstInc#
DMA_DataInc_TypeDef DMA_CfgDescrSGAlt_TypeDef::dstInc
Destination increment size for each DMA transfer.
srcInc#
DMA_DataInc_TypeDef DMA_CfgDescrSGAlt_TypeDef::srcInc
Source increment size for each DMA transfer.
arbRate#
DMA_ArbiterConfig_TypeDef DMA_CfgDescrSGAlt_TypeDef::arbRate
Arbitration rate, i.e., number of DMA transfers done before re-arbitration takes place.
nMinus1#
uint16_t DMA_CfgDescrSGAlt_TypeDef::nMinus1
Number of DMA transfers minus 1 to do.
Must be <= 1023.
hprot#
uint8_t DMA_CfgDescrSGAlt_TypeDef::hprot
HPROT signal state, refer to reference manual, DMA chapter for further details.
Normally set to 0 if protection is not an issue. The following bits are available:
- bit 0 - HPROT[1] control for source read accesses, privileged/non-privileged access. 
- bit 3 - HPROT[1] control for destination write accesses, privileged/non-privileged access. 
peripheral#
bool DMA_CfgDescrSGAlt_TypeDef::peripheral
Specify if a memory or peripheral scatter-gather DMA cycle.
Notice that this parameter should be the same for all alternate descriptors.
- true - this is a peripheral scatter-gather cycle. 
- false - this is a memory scatter-gather cycle.