Single conversion initialization structure.
Public Attributes#
Peripheral reflex system trigger selection.
Acquisition time (in ADC clock cycles).
Sample reference selection.
Sample resolution.
Sample input selection, use single-ended or differential input according to setting of diff. 
bool
Select if single-ended or differential input.
bool
Peripheral reflex system trigger enable.
bool
Select if left adjustment should be done.
bool
Select if continuous conversion until explicit stop.
Public Attribute Documentation#
prsSel#
ADC_PRSSEL_TypeDef ADC_InitSingle_TypeDef::prsSel
Peripheral reflex system trigger selection.
Only applicable if prsEnable is enabled. 
reference#
ADC_Ref_TypeDef ADC_InitSingle_TypeDef::reference
Sample reference selection.
Note that, for external references, the ADC calibration register must be set explicitly.
input#
ADC_SingleInput_TypeDef ADC_InitSingle_TypeDef::input
Sample input selection, use single-ended or differential input according to setting of diff.