LETIMER - Low Energy Timer#
Low Energy Timer (LETIMER) Peripheral API.
This module contains functions to control the LETIMER peripheral of Silicon Labs 32-bit MCUs and SoCs. The LETIMER is a down-counter that can keep track of time and output configurable waveforms.
Modules#
Enumerations#
Repeat mode.
Underflow action on output.
Functions#
Get the LETIMER compare register value.
Get LETIMER counter value.
Set LETIMER counter value.
Set the LETIMER compare register value.
Start/stop LETIMER.
Initialize LETIMER.
Get the LETIMER repeat register value.
Set the LETIMER repeat counter register value.
Reset LETIMER to the same state that it was in after a hardware reset.
Wait for the LETIMER to complete all synchronization of register changes and commands.
Set the LETIMER top value.
Get the current LETIMER top value.
Clear one or more pending LETIMER interrupts.
Disable one or more LETIMER interrupts.
Enable one or more LETIMER interrupts.
Get pending LETIMER interrupt flags.
Get enabled and pending LETIMER interrupt flags.
Set one or more pending LETIMER interrupts from SW.
Macros#
Default configuration for LETIMER initialization structure.
Enumeration Documentation#
LETIMER_RepeatMode_TypeDef#
LETIMER_RepeatMode_TypeDef
Repeat mode.
| Enumerator | |
|---|---|
| letimerRepeatFree | Count until stopped by SW. |
| letimerRepeatOneshot | Count REP0 times. |
| letimerRepeatBuffered | Count REP0 times, if REP1 has been written to, it is loaded into REP0 when REP0 is about to be decremented to 0. |
| letimerRepeatDouble | Run as long as both REP0 and REP1 are not 0. |
LETIMER_UFOA_TypeDef#
LETIMER_UFOA_TypeDef
Underflow action on output.
| Enumerator | |
|---|---|
| letimerUFOANone | No output action. |
| letimerUFOAToggle | Toggle output when counter underflows. |
| letimerUFOAPulse | Hold output one LETIMER clock cycle when counter underflows. |
| letimerUFOAPwm | Set output idle when counter underflows, and active when matching COMP1. |
Function Documentation#
LETIMER_CompareGet#
uint32_t LETIMER_CompareGet (LETIMER_TypeDef * letimer, unsigned int comp)
Get the LETIMER compare register value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | A pointer to the LETIMER peripheral register block. |
| unsigned int | [in] | comp | A compare register to get, either 0 or 1. |
Returns
A compare register value, 0 if invalid register selected.
LETIMER_CounterGet#
uint32_t LETIMER_CounterGet (LETIMER_TypeDef * letimer)
Get LETIMER counter value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
Returns
Current LETIMER counter value.
LETIMER_CounterSet#
void LETIMER_CounterSet (LETIMER_TypeDef * letimer, uint32_t value)
Set LETIMER counter value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
| uint32_t | [in] | value | New counter value. |
LETIMER_CompareSet#
void LETIMER_CompareSet (LETIMER_TypeDef * letimer, unsigned int comp, uint32_t value)
Set the LETIMER compare register value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | A pointer to the LETIMER peripheral register block. |
| unsigned int | [in] | comp | A compare register to set, either 0 or 1. |
| uint32_t | [in] | value | An initialization value (<= 0x0000ffff). |
Note
The setting of a compare register requires synchronization into the low frequency domain. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
LETIMER_Enable#
void LETIMER_Enable (LETIMER_TypeDef * letimer, bool enable)
Start/stop LETIMER.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | A pointer to the LETIMER peripheral register block. |
| bool | [in] | enable | True to enable counting, false to disable. |
Note
The enabling/disabling of the LETIMER modifies the LETIMER CMD register which requires synchronization into the low-frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
LETIMER_Init#
void LETIMER_Init (LETIMER_TypeDef * letimer, const LETIMER_Init_TypeDef * init)
Initialize LETIMER.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | A pointer to the LETIMER peripheral register block. |
| const LETIMER_Init_TypeDef * | [in] | init | A pointer to the LETIMER initialization structure. |
Note that the compare/repeat values must be set separately with LETIMER_CompareSet() and LETIMER_RepeatSet(). That should probably be done prior using this function if configuring the LETIMER to start when initialization is complete.
Note
The initialization of the LETIMER modifies the LETIMER CTRL/CMD registers which require synchronization into the low-frequency domain. If any of those registers are modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
LETIMER_RepeatGet#
uint32_t LETIMER_RepeatGet (LETIMER_TypeDef * letimer, unsigned int rep)
Get the LETIMER repeat register value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | A pointer to the LETIMER peripheral register block. |
| unsigned int | [in] | rep | Repeat register to get, either 0 or 1. |
Returns
Repeat register value, 0 if invalid register selected.
LETIMER_RepeatSet#
void LETIMER_RepeatSet (LETIMER_TypeDef * letimer, unsigned int rep, uint32_t value)
Set the LETIMER repeat counter register value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | A pointer to the LETIMER peripheral register block. |
| unsigned int | [in] | rep | Repeat counter register to set, either 0 or 1. |
| uint32_t | [in] | value | An initialization value (<= 0x0000ffff). |
Note
The setting of a repeat counter register requires synchronization into the low-frequency domain. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
LETIMER_Reset#
void LETIMER_Reset (LETIMER_TypeDef * letimer)
Reset LETIMER to the same state that it was in after a hardware reset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | A pointer to the LETIMER peripheral register block. |
Note
The ROUTE register is NOT reset by this function to allow for a centralized setup of this feature.
LETIMER_SyncWait#
void LETIMER_SyncWait (LETIMER_TypeDef * letimer)
Wait for the LETIMER to complete all synchronization of register changes and commands.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | A pointer to the LETIMER peripheral register block. |
LETIMER_TopSet#
void LETIMER_TopSet (LETIMER_TypeDef * letimer, uint32_t value)
Set the LETIMER top value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | A pointer to the LETIMER peripheral register block. |
| uint32_t | [in] | value | The top value. This can be a 16 bit value on series-0 and series-1 devices and a 24 bit value on series-2 devices. |
Note
The LETIMER is a down-counter, so when the counter reaches 0 then the top value will be loaded into the counter. This function can be used to set the top value.
If the LETIMER is not already configured to use a top value then this function will enable that functionality for the user.
LETIMER_TopGet#
uint32_t LETIMER_TopGet (LETIMER_TypeDef * letimer)
Get the current LETIMER top value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | A pointer to the LETIMER peripheral register block. |
Returns
The top value. This will be a 16 bit value on series-0 and series-1 devices and a 24 bit value on series-2 devices.
LETIMER_IntClear#
void LETIMER_IntClear (LETIMER_TypeDef * letimer, uint32_t flags)
Clear one or more pending LETIMER interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to LETIMER peripheral register block. |
| uint32_t | [in] | flags | Pending LETIMER interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn). |
LETIMER_IntDisable#
void LETIMER_IntDisable (LETIMER_TypeDef * letimer, uint32_t flags)
Disable one or more LETIMER interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to LETIMER peripheral register block. |
| uint32_t | [in] | flags | LETIMER interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn). |
LETIMER_IntEnable#
void LETIMER_IntEnable (LETIMER_TypeDef * letimer, uint32_t flags)
Enable one or more LETIMER interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to the LETIMER peripheral register block. |
| uint32_t | [in] | flags | LETIMER interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn). |
Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using LETIMER_IntClear() prior to enabling the interrupt.
LETIMER_IntGet#
uint32_t LETIMER_IntGet (LETIMER_TypeDef * letimer)
Get pending LETIMER interrupt flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to LETIMER peripheral register block. |
Note
Event bits are not cleared by the use of this function.
Returns
LETIMER interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).
LETIMER_IntGetEnabled#
uint32_t LETIMER_IntGetEnabled (LETIMER_TypeDef * letimer)
Get enabled and pending LETIMER interrupt flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to LETIMER peripheral register block. |
Useful for handling more interrupt sources in the same interrupt handler.
Note
Event bits are not cleared by the use of this function.
Returns
Pending and enabled LETIMER interrupt sources. Return value is the bitwise AND combination of
the OR combination of enabled interrupt sources in LETIMER_IEN_nnn register (LETIMER_IEN_nnn) and
the OR combination of valid interrupt flags of the LETIMER module (LETIMER_IF_nnn).
LETIMER_IntSet#
void LETIMER_IntSet (LETIMER_TypeDef * letimer, uint32_t flags)
Set one or more pending LETIMER interrupts from SW.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LETIMER_TypeDef * | [in] | letimer | Pointer to LETIMER peripheral register block. |
| uint32_t | [in] | flags | LETIMER interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn). |