USB Endpoint Descriptor.
Public Attributes#
uint8_t
Size of this descriptor in bytes
uint8_t
Constant ENDPOINT Descriptor Type
uint8_t
The address of the endpoint
uint8_t
This field describes the endpoint attributes
uint16_t
Maximum packet size for the endpoint
uint8_t
Interval for polling EP for data transfers
Public Attribute Documentation#
bDescriptorType#
uint8_t USB_EndpointDescriptor_TypeDef::bDescriptorType
Constant ENDPOINT Descriptor Type
bEndpointAddress#
uint8_t USB_EndpointDescriptor_TypeDef::bEndpointAddress
The address of the endpoint
bmAttributes#
uint8_t USB_EndpointDescriptor_TypeDef::bmAttributes
This field describes the endpoint attributes
wMaxPacketSize#
uint16_t USB_EndpointDescriptor_TypeDef::wMaxPacketSize
Maximum packet size for the endpoint
bInterval#
uint8_t USB_EndpointDescriptor_TypeDef::bInterval
Interval for polling EP for data transfers