CPC#
Modules#
sl_cpc_endpoint_debug_counters_t
Enumerations#
Enumeration representing user endpoint.
Enumeration representing the possible endpoint state.
Enumeration representing the possible configurable options for an endpoint.
Typedefs#
Typedef for the user - supplied callback function which is called when CPC is done with the provided buffer.
Typedef for the user - supplied callback function which is called when CPC receive data on an endpoint.
Typedef for the user-supplied callback function which is called when CPC detects a fatal error on an endpoint.
Typedef for the user-supplied callback function which is called when CPC connection to a secondary completes, successfully or not.
Functions#
Initialize CPC module.
The bare metal process action function.
Dynamically allocate and initialize a user endpoint.
Connect endpoint to remote.
Dynamically allocate and open a user endpoint.
Put an endpoint in listening mode, waiting for the remote to connect to it.
Close endpoint.
Set endpoint option.
Shutdown endpoint connection.
Terminate an endpoint, effectively dropping any pending TX and RX frame.
Free the memory associated to an endpoint so it can be reused.
Abort read; Allow unblocking task in blocked by a read.
Read data.
Write data.
Get endpoint state.
Get endpoint encryption state.
Free buffer returned by sl_cpc_read().
Get the maximum payload length that the remote can receive.
Called when secondary app version is requested.
Called when primary app version is requested.
Callback implemented by the user to verify if the secondary application version is compatible with this primary version.
Fetch the next firmware update image chunk from the user.
Macros#
sl cpc open endpoint flag none
sl cpc open endpoint flag disable encryption
Struct representing a core debug.
sl cpc user endpoint id end.
maximum simultaneous user endpoint.
sl cpc flag no block.
sli cpc security tag length.
sli cpc ldma desciptor max size.
sli cpc header size.
sli cpc payload crc size.
sl cpc tx payload max length.
sl cpc tx payload max lenght with security.
sl cpc transmit window min size.
sl cpc transmit window max size.
Enumeration Documentation#
sl_cpc_user_endpoint_id_t#
sl_cpc_user_endpoint_id_t
Enumeration representing user endpoint.
| Enumerator | |
|---|---|
| SL_CPC_ENDPOINT_USER_ID_0 | User endpoint ID 0. |
| SL_CPC_ENDPOINT_USER_ID_1 | User endpoint ID 1. |
| SL_CPC_ENDPOINT_USER_ID_2 | User endpoint ID 2. |
| SL_CPC_ENDPOINT_USER_ID_3 | User endpoint ID 3. |
| SL_CPC_ENDPOINT_USER_ID_4 | User endpoint ID 4. |
| SL_CPC_ENDPOINT_USER_ID_5 | User endpoint ID 5. |
| SL_CPC_ENDPOINT_USER_ID_6 | User endpoint ID 6. |
| SL_CPC_ENDPOINT_USER_ID_7 | User endpoint ID 7. |
| SL_CPC_ENDPOINT_USER_ID_8 | User endpoint ID 8. |
| SL_CPC_ENDPOINT_USER_ID_9 | User endpoint ID 9. |
sl_cpc_endpoint_state_t#
sl_cpc_endpoint_state_t
Enumeration representing the possible endpoint state.
| Enumerator | |
|---|---|
| SL_CPC_STATE_FREED | State freed. |
| SL_CPC_STATE_OPEN | State open. |
| SL_CPC_STATE_CLOSED | State close. |
| SL_CPC_STATE_CLOSING | State closing. |
| SL_CPC_STATE_CONNECTING | Connecting to remote's endpoint. |
| SL_CPC_STATE_CONNECTED | Connected to remote's endpoint. |
| SL_CPC_STATE_SHUTTING_DOWN | Transmissions shutting down. |
| SL_CPC_STATE_SHUTDOWN | Transmissions shutdown. |
| SL_CPC_STATE_REMOTE_SHUTDOWN | Remote transmissions shutdown. |
| SL_CPC_STATE_DISCONNECTED | Connection terminated. |
| SL_CPC_STATE_ERROR_DESTINATION_UNREACHABLE | Error state, destination unreachable. |
| SL_CPC_STATE_ERROR_SECURITY_INCIDENT | Error state, security incident. |
| SL_CPC_STATE_ERROR_FAULT | Error state, fault. |
sl_cpc_endpoint_option_t#
sl_cpc_endpoint_option_t
Enumeration representing the possible configurable options for an endpoint.
| Enumerator | |
|---|---|
| SL_CPC_ENDPOINT_ON_IFRAME_RECEIVE | Set callback for iframe received notification. |
| SL_CPC_ENDPOINT_ON_IFRAME_RECEIVE_ARG | Set callback argument for iframe received notification. |
| SL_CPC_ENDPOINT_ON_IFRAME_WRITE_COMPLETED | Set callback for write complete notification. |
| SL_CPC_ENDPOINT_ON_ERROR | Set callback for error notification. |
| SL_CPC_ENDPOINT_ON_ERROR_ARG | Set callback argument for error notification. |
| SL_CPC_ENDPOINT_ON_CONNECT | Set callback when host/primary connects to endpoint. |
| SL_CPC_ENDPOINT_ON_CONNECT_ARG | Set callback argument for connect notification. |
| SL_CPC_ENDPOINT_SHUTDOWN_TIMEOUT | Set shutdown timeout, in ticks. |
| SL_CPC_ENDPOINT_WRITE_TIMEOUT | Set the timeout time for blocking write in ticks. |
| SL_CPC_ENDPOINT_ON_UFRAME_RECEIVE | Set callback for uframe received notification. |
| SL_CPC_ENDPOINT_ON_UFRAME_RECEIVE_ARG | Set callback argument for uframe received notification. |
| SL_CPC_ENDPOINT_ON_UFRAME_WRITE_COMPLETED | Set callback for write complete notification. |
| SL_CPC_ENDPOINT_ON_FINAL | Set callback for on final notification. |
| SL_CPC_ENDPOINT_ON_FINAL_ARG | Set callback argument for on final notification. |
Typedef Documentation#
sl_cpc_on_write_completed_t#
typedef void(* sl_cpc_on_write_completed_t) (sl_cpc_user_endpoint_id_t endpoint_id, void *buffer, void *arg, sl_status_t status) )(sl_cpc_user_endpoint_id_t endpoint_id, void *buffer, void *arg, sl_status_t status)
Typedef for the user - supplied callback function which is called when CPC is done with the provided buffer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| N/A | endpoint_id | Endpoint ID | |
| N/A | buffer | Pointer to data buffer. | |
| N/A | arg | Transaction user's argument. | |
| N/A | status | Status indicating the transaction result: SL_STATUS_OK Remote should have receive the frame SL_STATUS_TRANSMIT_INCOMPLETE Remote has not received the frame. |
sl_cpc_on_data_reception_t#
typedef void(* sl_cpc_on_data_reception_t) (uint8_t endpoint_id, void *arg) )(uint8_t endpoint_id, void *arg)
Typedef for the user - supplied callback function which is called when CPC receive data on an endpoint.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| N/A | endpoint_id | Endpoint ID | |
| N/A | arg | User-specific argument . |
sl_cpc_on_error_callback_t#
typedef void(* sl_cpc_on_error_callback_t) (uint8_t endpoint_id, void *arg) )(uint8_t endpoint_id, void *arg)
Typedef for the user-supplied callback function which is called when CPC detects a fatal error on an endpoint.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| N/A | endpoint_id | Endpoint ID | |
| N/A | arg | User-specific argument . |
sl_cpc_on_connect_callback_t#
typedef void(* sl_cpc_on_connect_callback_t) (uint8_t endpoint_id, void *arg, sl_status_t status) )(uint8_t endpoint_id, void *arg, sl_status_t status)
Typedef for the user-supplied callback function which is called when CPC connection to a secondary completes, successfully or not.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| N/A | endpoint_id | Endpoint ID | |
| N/A | arg | User-specific argument. | |
| N/A | status | Indicate if the connection was successful or not: SL_STATUS_OK successfully connected SL_STATUS_TIMEOUT operation timed out SL_STATUS_NOT_READY secondary's endpoint is not ready |
Note
If several users connect to the same endpoint on the host side, this callback will only be called only when the first connection occurs.
Function Documentation#
sl_cpc_init#
sl_status_t sl_cpc_init (void )
Initialize CPC module.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
sl_cpc_process_action#
void sl_cpc_process_action (void )
The bare metal process action function.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
sl_cpc_init_user_endpoint#
sl_status_t sl_cpc_init_user_endpoint (sl_cpc_endpoint_handle_t * endpoint_handle, sl_cpc_user_endpoint_id_t id, uint8_t flags)
Dynamically allocate and initialize a user endpoint.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [inout] | endpoint_handle | Endpoint handle. |
| sl_cpc_user_endpoint_id_t | [in] | id | Endpoint ID [90 to 99]. |
| uint8_t | [in] | flags | Initialization flags. Reserved for future used |
Following the successful initialization of an endpoint, successive attempts to initialize an endpoint of the same ID will fail until the endpoint is freed.
sl_cpc_connect_endpoint#
sl_status_t sl_cpc_connect_endpoint (sl_cpc_endpoint_handle_t * endpoint_handle, uint8_t flags)
Connect endpoint to remote.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
| uint8_t | [in] | flags | Optional flags: SL_CPC_FLAG_NO_BLOCK Cause the function to return SL_STATUS_IN_PROGRESS immediately in RTOS. |
(CPC Primary only) Ths function will always block until the remote connects if no flag is specified.
sl_cpc_open_user_endpoint#
sl_status_t sl_cpc_open_user_endpoint (sl_cpc_endpoint_handle_t * endpoint_handle, sl_cpc_user_endpoint_id_t id, uint8_t flags, uint8_t tx_window_size)
Dynamically allocate and open a user endpoint.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
| sl_cpc_user_endpoint_id_t | [in] | id | Endpoint ID [90 to 99]. |
| uint8_t | [in] | flags | Endpoint type flags. SL_CPC_OPEN_ENDPOINT_FLAG_NONE Default behaviors SL_CPC_OPEN_ENDPOINT_FLAG_DISABLE_ENCRYPTION Disable encryption on the endpoint |
| uint8_t | [in] | tx_window_size | The maximum number of packets that can be sent before waiting for an acknowledge from the primary. Currently, only a value of 1 is supported. |
Note
This function will be deprecated in the future. Use
sl_cpc_init_user_endpoint()andsl_cpc_listen_endpoint()instead.
sl_cpc_listen_endpoint#
sl_status_t sl_cpc_listen_endpoint (sl_cpc_endpoint_handle_t * endpoint_handle, uint8_t flags)
Put an endpoint in listening mode, waiting for the remote to connect to it.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
| uint8_t | [in] | flags | Optional flags: SL_CPC_FLAG_NO_BLOCK Cause the function to return SL_STATUS_IN_PROGRESS immediately in RTOS. |
This function will always block until the remote connects if no flag is specified.
sl_cpc_close_endpoint#
sl_status_t sl_cpc_close_endpoint (sl_cpc_endpoint_handle_t * endpoint_handle)
Close endpoint.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
Note
This function will be deprecated in the future. Use
sl_cpc_terminate_endpoint()andsl_cpc_free_endpoint()instead.
sl_cpc_set_endpoint_option#
sl_status_t sl_cpc_set_endpoint_option (sl_cpc_endpoint_handle_t * endpoint_handle, sl_cpc_endpoint_option_t option, void * value)
Set endpoint option.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
| sl_cpc_endpoint_option_t | [in] | option | Endpoint Option. |
| void * | [in] | value | Pointer to the option value. |
Returns
Status code.
Return values
SL_STATUS_OK: Set endpoint option successfully.
Other: sl_status_t if error occurred.
Note
Public options are: SL_CPC_ENDPOINT_ON_CONNECT: Set a callback that will be called when connection is established with the remote.
SL_CPC_ENDPOINT_ON_CONNECT_ARG: Set an on connect argument.
SL_CPC_ENDPOINT_ON_IFRAME_RECEIVE: Set an on iframe receive callback. value is a sl_cpc_on_data_reception_t type.
SL_CPC_ENDPOINT_ON_IFRAME_RECEIVE_ARG: Set an on iframe receive argument.
SL_CPC_ENDPOINT_ON_IFRAME_WRITE_COMPLETED: Set an on iframe write completed callback. value is a sl_cpc_on_write_completed_t type.
SL_CPC_ENDPOINT_ON_ERROR: Set an on error callback. value is a sl_cpc_on_error_callback_t type.
SL_CPC_ENDPOINT_ON_ERROR_ARG: Set an on error callback argument.
SL_CPC_ENDPOINT_SHUTDOWN_TIMEOUT: (RTOS Only) Set shutdown handshake timeout, in ticks.
SL_CPC_ENDPOINT_WRITE_TIMEOUT: (RTOS Only) Set the timeout time for blocking write in ticks.
sl_cpc_shutdown_endpoint#
sl_status_t sl_cpc_shutdown_endpoint (sl_cpc_endpoint_handle_t * endpoint_handle, uint8_t flags)
Shutdown endpoint connection.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
| uint8_t | [in] | flags | Optional flags: SL_CPC_FLAG_NO_BLOCK Cause the function to return SL_STATUS_IN_PROGRESS immediately in RTOS data still pending TX. |
Any pending TX frame will attempt to be transmitted.
Note
In RTOS, this function is blocking by default. Use the SL_CPC_FLAG_NO_BLOCK flag to execute without blocking.
sl_cpc_terminate_endpoint#
sl_status_t sl_cpc_terminate_endpoint (sl_cpc_endpoint_handle_t * endpoint_handle, uint8_t flags)
Terminate an endpoint, effectively dropping any pending TX and RX frame.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
| uint8_t | [in] | flags | Termination flags. Reserved for future use |
In RTOS, this function will always block until all frames have been dropped.
Note
This function must be called before attempting to reconnect an endpoint to the remote.
sl_cpc_free_endpoint#
sl_status_t sl_cpc_free_endpoint (sl_cpc_endpoint_handle_t * endpoint_handle)
Free the memory associated to an endpoint so it can be reused.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
sl_cpc_abort_read#
sl_status_t sl_cpc_abort_read (sl_cpc_endpoint_handle_t * endpoint_handle)
Abort read; Allow unblocking task in blocked by a read.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
Note
This function can be called from an ISR.
sl_cpc_read#
sl_status_t sl_cpc_read (sl_cpc_endpoint_handle_t * endpoint_handle, void ** data, uint16_t * data_length, uint32_t timeout, uint8_t flags)
Read data.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
| void ** | [out] | data | Address of the variable that will receive the data pointer. |
| uint16_t * | [out] | data_length | Length of the data contained in the buffer. |
| uint32_t | [in] | timeout | Timeout in ticks for the read operation. (Requires RTOS). Note: No effect if SL_CPC_FLAG_NO_BLOCK is provided as a flag |
| uint8_t | [in] | flags | Optional flags: SL_CPC_FLAG_NO_BLOCK Cause the function to return SL_STATUS_EMPTY immediately in RTOS if no data available. |
sl_cpc_write#
sl_status_t sl_cpc_write (sl_cpc_endpoint_handle_t * endpoint_handle, void * data, uint16_t data_length, uint8_t flags, void * on_write_completed_arg)
Write data.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
| void * | [in] | data | Pointer to data buffer. |
| uint16_t | [in] | data_length | Length of the data contained in the buffer. |
| uint8_t | [in] | flags | Optional flags: SL_CPC_FLAG_NO_BLOCK Cause the function to return SL_STATUS_NO_MORE_RESOURCE immediately in RTOS when out of resources. |
| void * | [in] | on_write_completed_arg | Argument that will be passed to on_write_completed(). |
Note
This function cannot be called from an ISR.
When the write buffer is encrypted, the original content is lost and replaced by its encrypted counterpart.
sl_cpc_get_endpoint_state#
sl_cpc_endpoint_state_t sl_cpc_get_endpoint_state (sl_cpc_endpoint_handle_t * endpoint_handle)
Get endpoint state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
Returns
Endpoint state.
sl_cpc_get_endpoint_encryption#
bool sl_cpc_get_endpoint_encryption (sl_cpc_endpoint_handle_t * endpoint_handle)
Get endpoint encryption state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
Returns
Endpoint encryption state.
sl_cpc_free_rx_buffer#
sl_status_t sl_cpc_free_rx_buffer (void * data)
Free buffer returned by sl_cpc_read().
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void * | [in] | data | Pointer to data buffer to free. |
sl_cpc_get_tx_max_payload_length#
uint16_t sl_cpc_get_tx_max_payload_length (sl_cpc_endpoint_handle_t * endpoint_handle)
Get the maximum payload length that the remote can receive.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cpc_endpoint_handle_t * | [in] | endpoint_handle | Endpoint handle. |
Returns
the maximum tx payload length in function of whether the encryption is enabled on the endpoint or not
sl_cpc_is_ok_to_sleep#
bool sl_cpc_is_ok_to_sleep (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
sl_cpc_sleep_on_isr_exit#
sl_power_manager_on_isr_exit_t sl_cpc_sleep_on_isr_exit (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
sl_cpc_secondary_app_version#
const char * sl_cpc_secondary_app_version (void )
Called when secondary app version is requested.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
The format is up to the user. The string should be null terminated.
sl_cpc_primary_app_version#
const char * sl_cpc_primary_app_version (void )
Called when primary app version is requested.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
The format is up to the user. The string should be null terminated.
Note
: CPC source code contains a weak definition that default to returning "UNDEFINED". If the user provides a strong definition of this function, the user shall return a static string.
Returns
: String that represents the application version.
sl_cpc_user_is_ok_to_run#
bool sl_cpc_user_is_ok_to_run (const char * primary_app_version, const char * secondary_app_version)
Callback implemented by the user to verify if the secondary application version is compatible with this primary version.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const char * | N/A | primary_app_version | |
| const char * | N/A | secondary_app_version |
Note
: If this function is not implemented, then no version check will be performed and CPC API will always be available after the startup sequence.
: The function prototype is declared as weak. No default weak definition exist.
Returns
bool : true : CPC is authorized to start normally false : The user decided that the application versions are not compatible. CPC API will be blocked and only a firmware upgrade will be possible
sl_cpc_get_fwu_chunk#
sl_status_t sl_cpc_get_fwu_chunk (uint8_t *const chunk_buffer, const size_t index, const size_t chunk_size, size_t * size, bool * last)
Fetch the next firmware update image chunk from the user.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t *const | [in] | chunk_buffer | : 128 bytes buffer into which the user must copy the chunk |
| const size_t | [in] | index | : The byte index of the chunk being requested. When the FWU starts, the index starts at 0 and will increment by 128 (chunk size) after each time the user submits a chunk. |
| const size_t | [in] | chunk_size | : This will always be 128 (chunk size) and is the number of bytes the user must copy into the chunk_buffer. The only exception is for the last chunk; if the last chunk is less than 128 bytes, then the user must copy the the remaining bytes and return the size of the last chunk in the 'size' out parameter. |
| size_t * | [out] | size | : This is the number of bytes the user has copied into the chunk buffer. For all chunks except the last one, this value is expected to be 128 bytes, and some value between 1-128 for the last chunk. |
| bool * | [out] | last | : false if the chunk is not the last chunk. The firmware update state machine will continue fetching chunks from the user as long as the user does not return true on the last chunk. |
Note
: The prototype is declared as weak and no weak definition exist in CPC code. Not providing an implementation by the user is valid, although if the user asks to perform a firmware upgrade, sl_firmware_upgrade_start() will return SL_STATUS_NOT_AVAILABLE
Returns
sl_status_t : Whether or not the user has written a valid chunk. In the case where the user does not have the requested chunk in hand when this function is called and does not want to block (for example, fetching is from a serial link or an external storage), SL_STATUS_NOT_READY would be returned. The firmware update state machine will retry later to ask the user for the chunk. The index will remain the same at the next call. When a value of SL_STATUS_OK is returned, the state machine will go ahead and send the chunk to the secondary.
Macro Definition Documentation#
SL_CPC_ENDPOINT_FLAG_DISABLE_ENCRYPTION#
#define SL_CPC_ENDPOINT_FLAG_DISABLE_ENCRYPTIONValue:
(0x01 << 3)
sl cpc open endpoint flag disable encryption
SL_CPC_OPEN_ENDPOINT_FLAG_NONE#
#define SL_CPC_OPEN_ENDPOINT_FLAG_NONEValue:
SL_CPC_ENDPOINT_FLAG_NONE
SL_CPC_OPEN_ENDPOINT_FLAG_DISABLE_ENCRYPTION#
#define SL_CPC_OPEN_ENDPOINT_FLAG_DISABLE_ENCRYPTIONValue:
SL_CPC_ENDPOINT_FLAG_DISABLE_ENCRYPTION
SL_CPC_USER_ENDPOINT_ID_START#
#define SL_CPC_USER_ENDPOINT_ID_STARTValue:
((uint8_t)SL_CPC_ENDPOINT_USER_ID_0)
Struct representing a core debug.
sl cpc endpoint id start.
SL_CPC_USER_ENDPOINT_ID_END#
#define SL_CPC_USER_ENDPOINT_ID_ENDValue:
((uint8_t)SL_CPC_ENDPOINT_USER_ID_9)
sl cpc user endpoint id end.
SL_CPC_USER_ENDPOINT_MAX_COUNT#
#define SL_CPC_USER_ENDPOINT_MAX_COUNTValue:
(SL_CPC_USER_ENDPOINT_ID_END - SL_CPC_USER_ENDPOINT_ID_START + 1)
maximum simultaneous user endpoint.
SLI_CPC_LDMA_DESCRIPTOR_MAX_SIZE#
#define SLI_CPC_LDMA_DESCRIPTOR_MAX_SIZEValue:
2048
sli cpc ldma desciptor max size.
SL_CPC_TX_PAYLOAD_MAX_LENGTH#
#define SL_CPC_TX_PAYLOAD_MAX_LENGTHValue:
((2 * SLI_CPC_LDMA_DESCRIPTOR_MAX_SIZE) - SLI_CPC_HEADER_SIZE - SLI_CPC_PAYLOAD_CRC_SIZE)
sl cpc tx payload max length.
SL_CPC_TX_PAYLOAD_MAX_LENGTH_WITH_SECURITY#
#define SL_CPC_TX_PAYLOAD_MAX_LENGTH_WITH_SECURITYValue:
(SL_CPC_TX_PAYLOAD_MAX_LENGTH - SLI_CPC_SECURITY_TAG_LENGTH)
sl cpc tx payload max lenght with security.
SL_CPC_TRANSMIT_WINDOW_MIN_SIZE#
#define SL_CPC_TRANSMIT_WINDOW_MIN_SIZEValue:
1
sl cpc transmit window min size.
SL_CPC_TRANSMIT_WINDOW_MAX_SIZE#
#define SL_CPC_TRANSMIT_WINDOW_MAX_SIZEValue:
1
sl cpc transmit window max size.