Deprecated Functions#
Deprecated Functions.
Functions#
SE_readPubkey(uint32_t key_type, void *pubkey, uint32_t numBytes, bool signature)
Function Documentation#
SE_readPubkey#
SE_Response_t SE_readPubkey (uint32_t key_type, void * pubkey, uint32_t numBytes, bool signature)
Parameters
[in] | key_type | ID of key type to read. |
[out] | pubkey | Pointer to a buffer to contain the returned public key. Must be word aligned and have a length of 64 bytes. |
[in] | numBytes | Length of pubkey buffer (64 bytes). |
[in] | signature | If true, the function will return the signature programmed for the specified public key instead of the public key itself. |
Read pubkey or pubkey signature.
Read out a public key stored in the SE, or its signature. The command can be used to read:
SE_KEY_TYPE_BOOT
SE_KEY_TYPE_AUTH
Returns
One of the SE_RESPONSE return codes.
Definition at line
807
of file platform/emlib/src/em_se.c